LTspice: Integrating Noise Over a Bandwidth

Dec 19 2013

Figure 1

   

LTspice can perform .noise analysis of a circuit, where the noise voltage density (V/√Hz) for 1Hz bandwidth) can easily be plotted for the output noise, input noise or for any noisy component like a resistor, diode or transistor. However, you can also easily integrate noise over a selected bandwidth in a .noise analysis.

Figure 1. LTspice IV: Integrating Noise Over a Bandwidth.

To use this feature, Ctrl-click the data trace label, V(noise), in the waveform viewer—the total RMS noise based on the bandwidth specified in the .noise directive is displayed.

If you prefer to calculate the total noise over a limited bandwidth rather than the bandwidth specified in the .noise directive you can modify the left (low) and right (high) frequency limits of the waveform viewer by clicking on the horizontal axis. Once you have your waveform displaying the bandwidth of interest, Ctrl-click the data trace label to display the total RMS noise based in the bandwidth of interest.

Alternately, you can add a .measure statement to your schematic that will calculate the total noise over a particular bandwidth, and view your results in the LTspice error log (Ctrl + L) after each simulation. (More information on using .measure statement can be found in LTspice Help (F1).

Figure 2. LTspice IV: Integrating Noise Over a Bandwidth.

About the Authors

Gabino Alonso
Gabino Alonso is currently the director of strategic marketing for the Power by Linear™ Group. Prior to joining ADI, Gabino held various positions in marketing, engineering, operations, and education at Linear Technology,
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Resources


Video
Software and Simulation
Solutions Bulletin & Brochure
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project