MEMS Accelerometer Performance Comes Of Age

Apr 6 2018

Figure 1

   

In the June/July 2016 Uptime article, “Condition Monitoring and MEMS Accelerometers: What You Need to Know,” several attributes of micro- electromechanical system (MEMS) accelerometers were presented that make the technology compelling for condition monitoring applications. This article reviews data demonstrating the state of MEMS technology development and performance levels, by comparing it to a commercially available piezoelectric (PZT) condition monitoring accelerometer. 

Investment in MEMS process technology, coupled with design innovations, has greatly improved MEMS performance enough to make MEMS a viable option for a wider range of condition monitoring applications. Accelerometers with resonant frequencies up to 50 kHz, and noise density levels down to 25 μg √Hz are now possible with specialized MEMS structures and process technology. Careful design of signal conditioning electronics fully exploits the low Brownian motion noise of these new accelerometers.

Figure 1. The noise spectral density plot for a new, high frequency accelerometer.

Performance and Comparison Data

In order to assess whether the newest MEMS accelerometer would be suitable in a condition monitoring application, measurements were taken side by side with a commercially available PZT type condition monitoring accelerometer. To ensure both sensors had similar mass and were subject to the same stimulus, the MEMS sensor was adhered to the case of the PZT sensor. The single-supply analog output of the MEMS accelerometer was inputted directly into the analog input channel of the same data logger as the PZT sensor. A data acquisition instrument (DAQ) was used as the acquisition system for these experiments.

Motor Misalignment Simulation

A real-world scenario, such as the one described in vibration-based condition monitoring, was recreated on a vibration tester, in an effort to compare devices using a known stimulus. This example outlined the vibration levels for a gas turbine running at 5100 rpm (85 Hz) and a synchronous generator at 3000 rpm (50 Hz) running misaligned. The scenario describes the frequencies and amplitudes that the vibration system was programmed to produce using the random vibration test mode. Table 1 lists the amplitude measurements at the frequencies of interest for both devices.

Table 1. Motor Misalignment Simulation Set Point

Tone (#) Frequency (Hz) Level(s) g pk
1 50.00 0.400
2 85.00 0.400
3 100.00 0.250
4 170.00 0.250

Figure 2 shows resulting frequency spectrum measured for the MEMS accelerometer with 21 kHz resonant frequency, and the PZT sensor with 25 kHz resonance. The root mean square (rms) output of the MEMS accelerometer in the band from 1 kHz to 10 kHz, is higher than the PZT accelerometer by approximately 30 mg, or 1.7%.

Figure 2

Figure 2. Noise density spectrum for PZT accelerometer (top) and MEMS accelerometer (bottom); results are nearly identical up to 10 kHz, with a key difference in the low frequency response of the MEMS accelerometer.

Unlike the PZT device, the MEMS device has low frequency response with 1/f at 0.1 Hz, which is of interest for very low frequency machines, such as wind turbines (also enables a faster recovery from saturation). Since the frequency response of the vibration stimulus system rolled off at very low frequencies, the response for both devices were tested by “tapping” the test jig, and capturing the resulting responses. The recorded time domain measurement was then transformed to the frequency domain. The results are shown in Figure 3. Note that the MEMS accelerometer was able to record a response down to dc. 

Figure 3. A comparison of the response of both accelerometers when tapped.

Conclusion

The MEMS performance with the analog output driving the DAQ directly achieves good results comparable to the PZT sensor. This suggests that MEMS accelerometers are good candidates for rearchitected output channels of new condition monitoring products, in particular, enabling entirely new concepts based on semiconductor components that run on a single +5 V power supply, such as wireless smart sensors.

On the surface, the first generation accelerometer appeared attractive for this application, due to the high frequency resonance (22 kHz) and high full scale ranges (FSR) of ±70 g, ±250 g, and ±500 g. Unfortunately, the noise level is 4 mg√Hz, unacceptably high for most condition monitoring applications. For the second generation device used in the comparison, noise is reduced two orders of magnitude from the first generation, while power is reduced to 40%. Table 2 summarizes the performance comparison of both MEMS
accelerometers, highlighting the improvements in performance.

Table 2. Key Specifications Comparison of 1st and 2nd MEMS Accelerometer Generations for Condition Monitoring

  1st Generation Accelerometer 2nd Generation Accelerometer
FSR ±70 g to ±500 g ±50 g to ±100 g
F0 22 kHz 21 kHz
Supply Current 2.5 mA 1.0 mA
Self Test Yes Yes
emperature Range –40°C to +125°C –40°C to +125°C
Package 5 mm × 5 mm, 8-lead LCC 5 mm × 5 mm,
32-lead LFCSP
Noise Density 4 mg √Hz <30 μg √Hz

The convergence of electronic signal conditioning expertise and the development of high resolution MEMS accelerometers have enabled performance capable of serving condition monitoring applications. High frequency MEMS accelerometers with low levels of physical noise, coupled with high performance, low noise, and highly stable signal processing design techniques, address the fundamental limitations that have previously kept MEMS from offering performance comparable to contemporary PZT-based condition monitoring sensors.

About the Authors

Ed Spence
Ed Spence is the Marketing Manager for Analog Devices, Inc.’s Idustrial Sensors business unit, responsible for high performance accelerometers. Analog Devices designs and manufactures high performance inertial sensors
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project