Frequently Asked Question

What is Smart Wake Mode?

Smart Wake Mode allows the ADF7030-1 to wake up autonomously from sleep using the internal wake-up timer without intervention from the host processor. After wake-up, the ADF7030-1 can autonomously carrier sense, packet sniff, and receive packets while the host processor is in sleep, thereby reducing overall system current consumption. The smart wake mode can wake the host processor on an interrupt condition. These interrupt conditions can be configured to include the reception of valid preamble, sync word, CRC, or address match.