AN-1445: Upgrading from the ADF4355 to the ADF4356
Introduction
The ADF4356 is the improved, next generation of the ADF4355. Benefits of switching to the ADF4356 include the following:
- 4 dB improvement in both integer-N and fractional-N normalized phase noise floors figures of merit (FOMs)
- 5 dB improvement in 1/f flicker noise
- 5 dB to 10 dB improvement in spurs
This user guide details the hardware and software changes required.
Hardware Installation
- Remove the ADF4355BCPZ.
- Install the ADF4356BCPZ.
- Optional: remove RSET resistor (connected to Pin 22). The ADF4356 RSET can be left connected to NIC, Pin 22.
Write Sequences
The ADF4356 initialization sequence and the frequency update sequence are similar to the ADF4355 initialization sequence, with the addition of Register 13 to the ADF4356. See the ADF4356 data sheet for full details.
Registers
Table 1 and Table 2 list the differences in the register writes between the ADF4355 and the ADF4356. Refer to the ADF4355 and the ADF4356 data sheets for full details.
| Register(s) | Contents | Bit No. | Bit Description Changes |
| 0 to 5 | Not applicable | Not applicable | No changes to these bits. |
| 6 | 0x350180F6 | DB31 DB25 |
Reserved bit, set to 0. Reserved bit, set to 0. |
| 7 | 0x120000E7 | DB28 DB27 DB26 |
Reserved bit, set to 1. Reserved bit, set to 0. Reserved bit, set to 0. |
| 8 | 0x102D0428 | Not applicable | Not applicable. |
| 9 | 0x1A19FCC9 | Not applicable | VCO band division (Bits[DB31:DB24]) = ceiling (fPFD/2,400,000), where ceiling rounds up to the nearest integer. |
| 10 | Not applicable | Not applicable | No changes to these bits. |
| 11 | 0x0061300B | DB24 DB12 |
Reserved bit, set to 0. Reserved bit, set to 1. |
| 12 | 0x0001041C | [DB31:DB16] [DB15:DB11] [DB9:DB5] |
Resync clock bits. Reserved bits, set to 0. Reserved bits, set to 0. |
| 13 | Does not exist | Not applicable | Not applicable. |
| Register(s) | Contents | Bit No. | Bit Description Changes |
| 0 to 5 | Not applicable | Not applicable | No changes to these bits. |
| 6 | 0x350300F6 | DB31 DB25 |
Bleed polarity bit. For the ADF4356 new bleed current rule, see the ADF4356 data sheet. RF Output B select. |
| 7 | 0x060000E7 | DB28 DB27 DB26 |
Reserved bit, set to 0. LE SEL sync edge bit. Reserved bit, set to 1. |
| 8 | 0x15596568 | Not applicable | New default reserved value. |
| 9 | 0x2719FCC9 | Not applicable | VCO band division (Bits[DB31:DB24]) = ceiling (fPFD/1,600,000). |
| 10 | Not applicable | Not applicable | No changes to these bits. |
| 11 | 0x0061200B | DB24 DB12 |
VCO band hold bit. Reserved bit, set to 0. |
| 12 | 0x000015FC | [DB31:DB12] DB10 [DB8:DB5] |
Phase resync clock value bits. Reserved bit, set to 1. Reserved bits, set to 1. |
| 13 | Exists | Not applicable | Added MSB registers for FRAC2 and MOD2 values. See the ADF4356 data sheet. |