AN-1310: Flash Programming via MDIO—Protocol Type 8

Introduction

This application note describes a protocol proposed for fully integrated single package parts that incorporate high performance analog peripherals together with digital peripherals controlled by an ARM® Cortex™-M3 processor and integral flash for code and data.

The parts must include an MDIO interface capable of operating at up to 4 MHz and the capability to simultaneously execute from one flash block and to write/erase the other flash block making it ideal for 40 G to 100 G optical applications.

The nonerasable kernel code plus flags in user flash provide assistance to allow user code to robustly switch between the two blocks of user flash code and data spaces as required for MDIO.

For further details regarding the flags and other part specific details, consult the specific part hardware reference manual.

The purpose of this application note is to specify a flash procedure for initial programming of the user flash memory with only the power, GND, MDIO, and MDC pins accessible. The MDIO pin is in push-pull mode and does not require an external pull-up. The programming sequence can be initiated and controlled by a host.

For details about the MDIO protocol, refer to the MDIO specification IEEE 802.3 and the specific Analog Devices, Inc., device hardware reference manual. Protocol Type 8 only implements the minimum frame types necessary to perform downloads and relies entirely on the verify mechanism described in this application note to check that the download was successful. For in service reprogramming, one can devise and implement their own reprogramming strategy.

Entering Download

The device kernel enters download mode if P2.3 is low and both K2B0 and K2B1 are not zero. This is the case when the user code is blank or if the user has deliberately not written these keys as described in the hardware reference manual. This application note concentrates on describing the download protocol once the kernel has entered its downloader.

General Requirements

MDIO Frame Structure


As per the MDIO specification, each frame consists of a preamble, ST, OP, PHYADR, DEVADD, TA, and 16 bits of data.

Of the access types defined by OP, only Address, Write, and Read are used.

The value of PHYADR is 5.

The value of DEVADD is 1.


Commands in Address Frames


Address frames use pseudo addresses that contain command information and partial addresses, if appropriate. The top nibble of the address is interpreted as commands as shown in Table 1.

Table 1. Commands in Address Frames
Command Description
0 Reserved.
1
Download
Request download. Bit 0 to Bit 11 must be the last 3 nibbles of chip information.
2
SetAddress
Set flash address page to Bit 0 to Bit 11 of frame data.
3
PageErase
Set flash address page to Bit 0 to Bit 11 of frame data and then erase that page.
4
MassErase
Set flash address page to Bit 0 to Bit 11 of frame data and then erase entire user flash space.
5
Verify
Set flash address page to Bit 0 to Bit 11 of frame data and then verify that page.
6 Reserved.
7
Reset
Reset.
0x8 to 0xF Reserved.

After each command is received, it is executed and progress can be monitored with Read Frames.

Command 1 is required to enter download mode. If the chip information is incorrect, a subsequent read returns 0x0000. If any Erase, Write, or ReadInc frame is received before a correct Request Download, the part locks up until reset.


Write Frames


Write frames contain the data to be programmed to the part. Programming starts at the beginning of the flash page set by the last Command 2, Command 3 or Command 4. After each Write Frame, the data is saved. After every four Write Frames, the collected data is programmed into flash at the correct flash address. Thus, programming must be in multiples of four frames. A read back after a write frame returns the number of bytes processed for this page. This number is only updated after the frame is processed and is divisible by 8 when a location has been flashed.

If user flash protection is active (0x1FFF4 = 0x3A or 0x3FFF4 = 0x3A) writing fails and the read frame returns 0x8BAD.

Programming should always be in multiples of full pages.


Read Frams


After every frame, a reply is prepared to be returned by the next Read Frame (see Table 2).

Table 2. Reply Description
Response To Reply Description
Command 0 0x0BAD
Command 1 Chip information. See Table 3 for details.
Command 2 0x0002
Command 3 0 if erase not complete; 0x0003 if erase complete. 0x3BAD if error.
Command 4 0 if erase not complete; 0x0004 if erase complete.
Command 5 Verify data. See the description following Table 3.
Command 6 0x6BAD
Command 7 Undefined after reset.
Command 8 to Command 0xF 0x*BAD where * is replaced by the command number.
Write Frame Refer to the Write Frames section.
Read Frame Refer to the description following Table 3.

The chip information consists of three nibbles as shown in Table 3.

Table 3. Chip Information
Nibble Chip Information Description Defined Values
3 Unused 0
2 Category 0x3 for ADuCM
1 Family 0x2 for 32x
0 Family Member 0x0 for 320

Additional reads after the chip ID may contain further chip information. This information is implementation dependent. The first read back after Command 5 returns the sum of the last 4 half words of the page being verified. The second read back returns the low 16 bits of the CRC generated by the flash sign command.

The third read back returns the high 16 bits of the CRC generated by the flash sign command. Together, the three frames check all bytes of the page.

Typical Download Sequence

Table 4 shows a typical download sequence.

Table 4. Typical Download Sequence
Step Frame Type Description Framde Data Comment
0 Address Download 0x1320  
1 Read Chip information 0x0320 Check correct chip is accessed.
2 Address Erase 0x3000 + page number (Pages need not to be consecutive.)
3 Read Erase done? 0x0000 Repeat until 0x0003.
4 If desired, repeat Step 2 to Step 3.
5 Address Set address 0x2000 + page number (Pages need to be consecutive.)
6 Write Data Next 2 bytes to program Increment flash address by 2.
7 Write Data Next 2 bytes to program Increment flash address by 2.
8 Write Data Next 2 bytes to program Increment flash address by 2.
9 Write Data Next 2 bytes to program Increment flash address by 2.
10 Read Flashing done? Byte count Repeat until divisible by 8.
11 Repeat Step 5 to Step 10 another 255 times to complete flash page.
12 If desired, do a page verify as described in Step 14 to Step 18.
13 Repeat Step 5 to Step 12 until all pages are downloaded. Include Step 4 if next page not previously erased.
14 Address Verify 0x5000 + page number (Pages need not to be consecutive.)
15 Read Verify 4 × 16-bit sum 16 bit sum of last 4 half words
16 Read Verify CRC LSBs Lower 16 bits of FEESIG.
17 Read Verify CRC MSBs Upper 16 bits of FEESIG.
18 Check that verify values equal expected verify values.
19 Repeat Step 14 to Step 18 for all pages as final check of correct download. (Pages need not be consecutive.)
20 Address Reset 0x7000 Software reset restarts part.

The host can terminate a download with Command 7 if, for instance, it takes too long to get a suitable read back value or a bad reply is received.

References

IEEE 802.3 standard, Clause 45, is described online.

Author

Generic_Author_image

Eckart Hartmann