AN-1166: HDMI Sink Jitter Tolerance Issues for Devices that Use an HDMI Mux and HDMI Receiver

Introduction

A standard means to increase the overall number of HDMI inputs to a system is to use an HDMI mux with several inputs whose output feeds one of the inputs of an HDMI receiver. This results in two cascaded stages to handle the TMDS signals before they are digitally processed in the receiver (see Figure 1)

Each stage necessarily contributes some jitter, which degrades the quality of the signal. This can present a challenge for HDMI compliance tests especially when operating at higher data rates. An HDMI buffer (one input and one output) used inside an HDMI sink device faces the same performance issues as a mux.

Figure 1. An HDMI Mux/Buffer in Front of an HDMI Receiver

Synchronous vs. Asynchronous Muxes/Buffers

There are two categories of muxes/buffers to consider: synchronous and asynchronous. A synchronous buffer is a more complex part that performs a clock recovery operation and then retimes and reconstructs the output signal. This eliminates most of the jitter from the input signal and simplifies the task of the next stage in the chain.

On the other hand, an asynchronous mux/buffer has no retiming capability. It can attenuate some types of jitter from the input side, but for other types, it passes the jitter through and adds some of its own.

Analog Devices, Inc., makes both types of muxes/buffers for HDMI signals. A listing of available analog/HDMI/DVI interfaces can be found online.

The HDMI/DVI switches table lists the asynchronous devices and the HDMI transceiver table lists the synchronous devices.

A channel formed by a cable or circuit board trace has a lowpass characteristic that creates a type of data-dependent jitter (DDJ). This is also referred to as intersymbol interference (ISI) where the data pattern preceding a particular bit affects the timing and/or amplitude of the bit in question.

It is possible to design an equalizer (EQ) circuit with a highpass characteristic that is an approximate inverse of the channel. A properly designed EQ can remove significant amounts of ISI jitter that was present at the input.

HDMI Jitter Tolerance Compliance Test (JTOL)

The HDMI organization requires that systems be tested in accordance with the Compliant Test Specification (CTS) document. One test in particular, Test ID 8-7: TMDS Jitter Tolerance (JTOL), can be challenging for HDMI sinks to pass for 3 Gbps links. Such data rates support the latest HDMI resolution specifications, like 4 k × 2 k and 3D video among others. The unit interval (UI) for 3 Gbps data rates (333 ps) is shorter than for prior lower data rates and the jitter margin is restricted accordingly.

Note that this compliance test is only for a full HDMI sink device, such as a TV. There is no compliance test for the individual electronic components that form the signal path for the TV (or other sink) HDMI signal path. Therefore, it is not appropriate to make a claim about the compliance status of an individual circuit component. A valid test must be performed on a full system.

Performing the JTOL Test

The basic JTOL test uses standard HDMI signals and adds 0.3 UI of sinusoidal jitter in addition to timing skew to simulate the worst-case HDMI source. This set of test signals is then connected to the sink-under-test via two different self-equalized cable emulators (see Figure 2).

Figure 2. Block Diagram for HDMI Compliance JTOL Test ing (Test ID 8-7)

One cable emulator follows the attenuation profile of standard cable. The second cable emulator simulates a self-equalized cable and provide a high-pass network that creates a flatter frequency response.

An alternative is to use an arbitrary waveform generator (ARB) to create a set of test signals that is the equivalent of passing through such cable emulators. The HDMI sink device is required to make an error-free picture under either of these conditions to pass the test. It has been observed that the two different test platforms have subtle differences and might produce different results for a marginal system.

Figure 3. Eye Diagram for 3 Gbps Signal with 0.3 UI Sinusoidal Jitter at TP1

Signal Chain Considerations

A channel formed by a cable or circuit board trace has a lowpass characteristic that creates a type of data-dependent jitter (DDJ). This is also referred to as intersymbol interference (ISI) where the data pattern preceding a particular bit affects the timing and/or amplitude of the bit in question.

It is possible to design an equalizer (EQ) circuit with a highpass characteristic that is an approximate inverse of the channel.

A properly designed EQ can remove significant amounts of ISI jitter that was present at the input.

The HDMI buffer/mux usually has a cable at its input and provides input EQ at TP2 to enable the use of longer cables. Similarly, the HDMI receiver might also have inputs connected directly to a cable, and it also provides input EQ at TP4.

A problem can arise when testing with a self-equalized cable emulator between TP1 and TP2 and using an asynchronous buffer/mux between TP2 and TP3. Three cascaded stages provide an EQ function and create an over-equalized condition that has too much jitter for the HDMI receiver to reliably process and the test can fail.

On the other hand, an asynchronous mux/buffer in the center stage can remove most of the jitter it receives at TP2. A reconstructed data signal is presented to the HDMI Rx device, which has low jitter that is within the jitter budget limits of the receiver. This enables the system to pass the JTOL test.

Conclusion

Using an asynchronous HDMI mux/buffer in front of an HDMI receiver can present challenges in passing the 3 Gbps HDMI JTOL test in the CTS when using a self-equalized cable emulator. This is caused by an over-equalization condition which adds excessive jitter. A synchronous mux/buffer can perform better because by retiming the signal, it removes most of all types of jitter from its input and presents a clean signal to the HDMI receiver.

The CTS JTOL test presents a significant challenge at 3 Gbps. Therefore, it is highly recommended to conduct an early investigation of this aspect of system performance to see if the component selection and system design perform well enough to pass this test.

Author

Generic_Author_image

Peter Checkovich