ADI Logo

Integrated SoC Shrinks the Size of the 4-20 mA Smart Transmitter

Smart transmitters can normalize gain and offset, linearize the sensor by converting its analog signal to digital, process the signals with arithmetic algorithms resident in the microcontroller, convert back to analog, and transmit the result as a standard current along the loop. They also add the capability for digital communications, which share the twisted-pair line with the 4-20 mA signal. The resulting communication channel allows for transmission control and diagnostic signals along with the sensor data. The SoC that integrates AFE, microcontroller, HART®, and 4-20 mA transmitter technology allows for the small size of the 4-20 mA smart transmitter.

integrated soc shrinks the size of the 4 20 ma smart transmitter
Communication consent
© 1995 - 2026 Analog Devices, Inc. All Rights Reserved

About Analog Devices

Analog Devices, Inc. (NASDAQ: ADI) is a global semiconductor leader that bridges the physical and digital worlds to enable breakthroughs at the Intelligent Edge. ADI combines analog, digital, AI, and software technologies into solutions that help drive advancements in automation and robotics, mobility, energy and data centers, and healthcare, combat climate change, and reliably connect humans and the world. With revenue of more than $11 billion in FY25, ADI ensures today's innovators stay Ahead of What's Possible.