The EV1HMC8342LS6 evaluates the performance of the HMC8342 microwave integrated circuit (MMIC), active frequency multiplier.
Figure 1 in the user guide shows a photograph of the EV1HMC8342LS6. The EV1HMC8342LS6 contains the HMC8342 and two 2.92 mm K connectors. There is also a calibration path for use in calibrating out printed circuit board (PCB) trace delays at the RF input and RF output.
For full details on the HMC8342, see the HMC8342 data sheet. Consult this data sheet in conjunction with this user guide when using the EV1HMC8342LS6.
EQIUPMENT NEEDED
ONLINE RESOURCES
Pricing displayed is based on 1-piece.
Pricing displayed is based on 1-piece. The USA list pricing shown is for budgetary use only, shown in United States dollars (FOB USA per unit), and is subject to change. International prices may vary due to local duties, taxes, fees and exchange rates.