This user guide describes how to set up the provided hardware of the evaluation kit and establish the link type specific host connection and connect the evaluation board to an industrial Ethernet network.
The operation of the EV-RPG2 boards vary by Industrial Ethernet Protocol, and separate user guides are available for each protocol on the ADI Chronous Developer Portal.
The EV-RPG2 evaluation kits provide an end to end evaluation of the communication path from the host processor to the programmable logic controller (PLC) or PC-based tool.
The EV-RPG2 evaluation kits can completely verify the communication path between the host processor and a PLC before integrating the network interface into the end field device.
EVALUATION KIT OPTIONS
Pricing displayed is based on 1-piece.
Pricing displayed is based on 1-piece. The USA list pricing shown is for budgetary use only, shown in United States dollars (FOB USA per unit), and is subject to change. International prices may vary due to local duties, taxes, fees and exchange rates.