With decades of expertise at the interface between the physical and the digital, ADI is looking for the next generation of AI, robotics, and embedded software experts. Join us to transform industries from energy and transportation to wearables, healthcare, and more!
Learn about our team
97% Smaller, Just as Smart: Scaling Down Networks with Structured Pruning 97% Smaller, Just as Smart: Scaling Networks with Structured Pruning
By: Sheila Seidel, Principal Engineer, Machine Learning Edge AI
Oct 30, 2025
Why Smaller Models Matter
Shrinking AI models isn’t just a nice-to-have—it’s a necessity for bringing powerful, real-time intelligence to edge devices. Whether it’s smartphones, wearables, or embedded systems, these platforms operate with strict memory, compute, and battery constraints. Delivering AI experiences on-device means enabling ultralow latency and ultra low power consumption without sacrificing model accuracy or capability.
This is where model compression comes in. While unstructured pruning is a common starting point—removing individual low importance weights with minimal impact on architecture—it often results in irregular sparsity patterns and runtime inefficiencies due to mask overheads. That’s why our ADI team shifted focus to structured pruning, delivering true reductions in memory footprint and computational cost. Better yet, this approach produces models that are both smaller and more easily deployed on even the most resource-constrained edge devices.
Structured Pruning: A Better Path to Model Efficiency
Structured pruning offers a practical path to shrinking models for deployment on resource-constrained platforms. At its basic form, the technique removes entire units like channels, filters, or even entire layers. Better yet, unlike unstructured pruning, which requires tracking the locations of nonzero weights, structured pruning produces cleaner, smaller weight matrices that are easier to optimize and deploy.
However, pruning isn’t just about deleting parts of a model. Removing parameters in one layer can impact others, especially in tightly coupled architectures like RNNs. Managing these dependencies is key to keeping pruned models functional and effective.
Going Beyond Built-In Tools
While PyTorch provides basic pruning utilities via torch.nn.utils.prune, these tools are limited: they only apply masks without reducing actual model size or handling interlayer dependencies.
To solve this, we’ve been working with torch-pruning, an open-source library that physically removes redundant components from a model. Unlike PyTorch’s built-in utilities, torch-pruning builds a dependency graph of the network to determine how layers interact. This enables structured pruning that respects the model’s architecture.
Real-World Applications: Speech Denoising and Voice Activity Detection
We were recently tasked with work on a speech denoising project and tapped torch-pruning to help us compress a convolutional-GRU model. The Conv2D layers were straightforward to prune, yielding a 25% to 30% reduction in multiply-accumulate operations (MACs) without hurting performance.
But the GRU layers presented a challenge. PyTorch’s GRUs are implemented in C++ and don’t play well with torch-pruning’s dependency graph. Moreover, because GRUs feed their hidden state back into themselves, pruning these inputs wasn’t supported out of the box.
Our solution? Build a prunable GRU from scratch using standard PyTorch layers like nn.Linear and elementwise operations. We also introduced an identity adaptor layer to decouple the hidden state size from the GRU input, enabling safe pruning.
Here’s the workflow:
- Replace native GRUs with custom prunable GRUs, copying over existing weights.
- Apply structured pruning using torch-pruning.
- Convert prunable GRUs back into native GRUs.
- Fine-tune the model to recover accuracy.
- Deploy the now-smaller model.
This approach resulted in a 30% reduction in model parameters, in addition to the MAC savings from convolutional pruning.
In our voice activity detection (VAD) project, which uses a mostly convolutional architecture, we pruned an 80k-parameter model down to under 2k parameters while preserving state-of-the-art performance. Key to these changes: carefully pruning later layers while preserving rich early-layer features.
Open Source Contributions and What’s Next
Our custom GRU pruning solution is now part of an open pull request to the torch-pruning library: PR #515. This work opens the door to pruning other recurrent units like LSTMs and minimal RNN variants.
Looking ahead, we’re exploring agentic pruning workflows to make structured pruning even more accessible and adaptive for diverse model architectures.
Structured pruning isn’t just a research curiosity. It’s a practical tool to make powerful AI models run on everyday devices—more efficiently and more responsibly.