Analog Devices’ New Easy Drive™ SAR ADCs Simplify Design While Delivering Industry Leading Performance

May 3 2022 - Wilmington, MA
  • AD4630-24 Easy Drive SAR ADCs: Highest Performance SimplifiedAnalog Devices, Inc. (Nasdaq: ADI) today introduced a new portfolio of next-generation 16-to-24-bit, ultra-high precision successive approximation register (SAR) analog-to-digital converters (ADCs) that simplify the often complex process of designing ADCs into instrumentation, industrial and healthcare applications. The new high-performance SAR ADC family features ADI’s patented Easy Drive™ technology and versatile Flexi-SPI serial peripheral interface (SPI) that solve system design challenges and broaden the selection of directly compatible companion products.

    ADI’s Easy Drive technology maintains device performance while eliminating many traditional system-level design challenges such as strict layout guidelines, rigid digital interface timing requirements, and the complicated selection of companion products. The versatile Flexi-SPI digital interface eases host processor and ADC integration by providing easy-to-meet timing requirements. The combination of high performance with this reimagined digital interface provides a better overall design experience while also accelerating the system design cycle.

    First in the pin-compatible SAR ADC family of six, the 24-bit dual-channel, simultaneous sampling, two Megasamples (Msps) per second per channel AD4630-24 features an industry leading accuracy (INL) rating of 0.9 parts per million (ppm), which is a 4x improvement when compared to others. The AD4630-24 integrates a reference buffer and all critical decoupling components into a single chip, providing a 2x improvement in solution density when compared with others.

    “The combination of performance and speed will lead to more accurate and stable digital control loops that can settle to their final set point with lower latency,” said Ray Goggin, General Manager for ADI’s Electronic Test & Measurement Group. “ADI’s new family of ADCs is an intentional technology evolution that further simplifies the process of designing, evaluating and getting digitally controlled precision instrumentation products to market faster.”

    AD4630-24 SAR ADC Key Features:

    • Highest accuracy: Guaranteed accuracy rating of 0.9 ppm INL with typical performance of 0.1 ppm
    • Highest performance: Signal-to-noise ratio rating of 105.7 dB typical
    • Small solution size: Chip scale ball grid array (CSP-BGA) package integrates all the critical power supply and reference bypass capacitors to reduce footprint and system component count
    • Wide common mode input range: Ensures compatibility with both single-ended and differential input signal chains.

    The dual channel AD4630-24 and single channel AD4030-24 are available now and the additional four SAR ADCs will launch throughout this year.

    Part Number Resolution Channel Count Sample Rate Availability
    AD4630-24 24-bit Dual Channel 2 Msps Now
    AD4030-24 24-bit Single Channel 2 Msps Now
    AD4630-16 16-bit Dual Channel 2 Msps Coming Soon
    AD4632-24 24-bit Dual Channel 500 ksps Coming Soon
    AD4032-24 24-bit Single Channel 500 ksps Coming Soon
    AD4632-16 16-bit Dual Channel 500 ksps Coming Soon

    Pricing and Packaging

    Product Price Packaging
    AD4630-24 $30.95 in 1,000 Unit Quantities 64-ball 7mm x 7mm x 1.72mm CSP-BGA package
    EVAL-AD4630-24FMCZ Evaluation Kit $199.00 N/A


  • About Analog Devices
  • Analog Devices, Inc. (NASDAQ: ADI) operates at the center of the modern digital economy, converting real-world phenomena into actionable insight with its comprehensive suite of analog and mixed signal, power management, radio frequency (RF), and digital and sensor technologies. ADI serves 125,000 customers worldwide with more than 75,000 products in the industrial, communications, automotive, and consumer markets. ADI is headquartered in Wilmington, MA. Visit https://www.analog.com.

  • Editor's Contact Information
Stay Informed