LTC4218 12V/100A Hot Swap Design for Server Farms

2015-03-18

Figure 1

   

Cultivate reliability on the farm with a properly designed Hot Swap circuit.

Introduction

As data centers servicing the cloud grow in speed and capacity, backplane supplies are called on to deliver currents that push the performance boundaries of Hot Swap components. Hot Swap solutions allow boards to be inserted and removed from a live backplane without disturbing the power distributed to other boards. A typical Hot Swap solution uses a series MOSFET to manage the flow of power between the backplane and the board—preventing glitches and faults from disrupting power to the rest of the system.

The challenges of designing robust Hot Swap solutions multiply with increasing current demands. With load currents at 100A, simply determining power dissipation requirements is no longer sufficient. Designers must pay careful attention to the MOSFET safe operating area (SOA) and understand Kelvin current sensing techniques for multiple sense resistors. This article shows how to address these issues using the example of a 12V/100A solution based on the LTC4218 Hot Swap controller.

12V/100A Hot Swap Design

Figure 1 shows the LTC4218 Hot Swap controller managing power to a board that contains up to 1000μF of bypass capacitance, draws up to 100A of load current and is hot plugged into a 12V backplane supply.

Figure 1. 12V/100A Hot Swap solution

Figure 1. LTC4218 12V/100A Hot Swap Solution

Supporting the 100A load current without excessive power dissipation in the MOSFETs M1 and M2 requires that the PG (power good) signal disable the load until the output is fully powered. Typically, this is implemented by controlling the RESET signal of downstream circuitry with the Hot Swap controller’s PG signal. In the circuit of Figure 1, if the effective load resistance is greater than 10Ω during start-up (while PG is low), the output powers up normally. If the output resistance is low during start-up (such as might occur during an output short-circuit fault), the LTC4218 detects this condition and turns off the series MOSFET.

During start-up, the circuit’s current limit threshold is reduced by pulling the LTC4218’s ISET pin low through R4 until the PG signal transitions high. R4’s 3kΩ resistance lowers the current limit threshold to roughly 13% of the normal operating current limit. Any fault conditions that sink extra current beyond that level during start-up cause the TIMER to activate and shut off the MOSFET. (The relatively small components M3, M4, R6, R7, and C4 work together to effectively connect R4’s 3k resistance between ISET and ground when the PG pin is pulling low.)

The output ramp rate during start-up is set by the LTC4218’s 24μA pull-up current into C1 and the gates of MOSFETs M1 and M2. The result is an output ramp rate of 2V/ms. Because the load circuitry is disabled by the PG signal, the current at start-up is dedicated to charging the capacitance downstream of the Hot Swap circuit, represented by C6 in Figure 1. Ramping the 1000μF of capacitance at 2V/ms requires 1000μF • (2V/ms)=2A of current. This is far below the start-up current limit threshold set by R4 at 16A or 13% of the normal operating current limit. This allows plenty of margin for inaccuracies in the current sensing. Exceeding this current limit threshold for even a short time during start-up indicates a fault condition at the output, and the LTC4218 responds by turning off MOSFETs M1 and M2.

MOSFET Safe Operating Area

In this application, the entire SOA can be satisfied by M1 or M2 alone. It is unwise to assume that current and SOA share equally among MOSFETs during start-up or output overload faults that cause significant drain to source voltages across the MOSFETs. Either MOSFET should be able to support the entire SOA of the application.

On the other hand, when the MOSFET is fully enhanced during normal operation, its behavior is similar to a resistor and it is safe to assume that current shares more equally. In this application, two MOSFETs are used to reduce the power dissipation during normal operation, not to satisfy transient safe operation area requirements. At 100A, the power dissipated by a single 1mΩ MOSFET is I2R = (100A)2 • 1mΩ = 10W. If the current shares equally at 50A, the power in each MOSFET is a more reasonable I2R = (50A)2 • 1mΩ = 2.5W.

Proper Kelvin Sensing with Multiple Sense Resistors

At these current levels, properly monitoring the voltage across the sense resistance can be challenging. With the LTC4218’s 15mV current sense threshold, a 100A current limit requires less than 0.15mΩ of sense resistance, usually achieved using parallel resistors in a Kelvin sensing scheme.

When a single sense resistor is used in Hot Swap (or other current sense) applications, it is common practice to use separate low current Kelvin traces between the sense pins of the IC and the sense resistor. An example layout of Kelvin connections to a current sense resistor is shown in Figure 2. The low current Kelvin sense paths directly between the sense resistor and the LTC4218 SENSE+ and SENSE pins eliminate errors due to the voltage drops that occur when high currents pass through the resistive PCB copper.

Figure 2. Kelvin sensing with single sense resistor

Figure 2. Kelvin sensing with single sense resistor

In this 100A application, though, it is necessary to implement the sense resistance with multiple parallel sense resistors. Eight 1mΩ resistors in parallel is a reasonable choice, as it results in a typical current limit of 8 • (15mV/1mΩ) = 120A, providing a comfortable margin above the 100A delivered to the load.

Nevertheless, multiplying the number of sense resistors multiplies the layout challenges; the straightforward layout shown for a single resistor in Figure 2 no longer suffices. Current rarely shares equally among the sense resistors—it is not unusual to see a 50% difference in current between several low value sense resistors in high current applications. The resistors placed more closely to MOSFETs M1 and M2 conduct a greater proportion of the load current than the sense resistors placed farther away, due to the finite resistance of the PC board copper planes showing up in series with the sense resistors. If possible, the preferred layout is to place an equal number of sense resistors on the top and the bottom of the PC board. This minimizes the parasitic voltage drops caused by the lateral current flow through the copper planes required to reach the farthest sense resistor.

Even with an optimal PC board layout, it is necessary to use a resistor network to average the voltages sensed across the individual 1mΩ resistors. In this 12V/100A application, the SENSE+ and SENSE pins of the LTC4218 are joined to the eight 1mΩ sense resistors with an array of 1Ω resistors as shown in Figure 1. The resulting voltage between the SENSE+ and SENSE pins is the average of all of the voltages across the 1mΩ sense resistors, effectively Kelvin sensing the eight 1mΩ resistors. An example layout is shown in Figure 3.

Figure 3. Kelvin sensing layout for eight parallel resistors uses top and bottom of board

Figure 3. Kelvin sensing layout for eight parallel resistors uses top and bottom of board

Lab Results

Of course, calculations and circuit simulations are no substitute for benchtop testing, especially when working with high current Hot Swap solutions. Figure 4 shows an oscilloscope waveform of this design starting up into a 100Ω resistor followed by a 100A load step after the ENABLE/RESET signal transitions high. Note that the ENABLE/RESET in this setup drives the 4V ON signal of an electronic load box rather than the 12V level from M5 and R10 shown in Figure 1.

Figure 4. Normal start-up

Figure 4. Normal start-up

The waveform in Figure 4 is typical of proper operation when no faults are present. The 12V input supply ramps up first. Then, the LTC4218 charges the 1000μF output capacitor at 2V/ms. Finally, the 100A load turns on when the ENABLE/RESET output transitions high, signaling that the MOSFETs M1 and M2 are fully enhanced.

Figure 5 shows the LTC4218 turning off MOSFETs M1 and M2 when a short circuit occurs on the output. 100ms after the input voltage rises, the circuit begins to charge the output node. The LTC4218 limits the charging current to the 16A start-up current limit threshold and quickly detects the short-circuit. This solution responds properly and shuts off power to the load to avoid any disruption (and damage) to other components in the system.

Figure 5. Start-up into a short circuit

Figure 5. Start-up into a short circuit

Conclusion

Over the years, the designers of Hot Swap solutions have had to continually address fresh challenges posed by ever increasing supply currents. Some issues are not new, such as the power dissipation requirements that result from high current, but today’s current levels have pushed some new design issues to the fore, such as MOSFET safe operating area, and the Kelvin sensing techniques for multiple sense resistors. The 12V/100A LTC4218 Hot Swap controller solution shown here specifically addresses these design points.

关于作者

Dan Eddleman
Dan Eddleman是一名模拟工程师,在凌力尔特工作超过15年,曾担任过IC设计人员、新加坡IC设计中心经理和应用工程师。

他的职业生涯始于凌力尔特,设计了LTC2923和LTC2925电源跟踪控制器、LTC4355高压双通道理想二极管OR和LTC1546多协议收发器。他还是世界首款以太网供电控制器LTC4255的设计团队成员。他拥有两项与这些产品相关的专利。

随后
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

产品

产品分类

资源


LTspice
最新视频 21
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目