40nVP–P Noise, 0.05µV/°C Drift, Chopped FET Amplifier

2006-03-01

Figure 1

   

Figure 1’s circuit combines the 5V rail-to-rail performance of the LTC6241 with a pair of extremely low noise JFETs configured in a chopper based carrier modulation scheme to achieve extraordinarily low noise and DC drift. This circuit’s performance suits the demanding transducer signal conditioning situations such as high resolution scales and magnetic search coils.

Figure 1. 40nV noise chopper amplifier

The LTC1799’s output is divided down to form a 2-phase 925Hz square wave clock. This frequency, harmonically unrelated to 60Hz, provides excellent immunity to harmonic beating or mixing effects which could cause instabilities. S1 and S2 receive complementary drive, causing the A1-based stage to see a chopped version of the input voltage. A1’s square wave output is synchronously demodulated by S3 and S4. Because these switches are synchronously driven with the input chopper, proper amplitude and polarity information is presented to DC output amplifier A2. This stage integrates the square wave into a DC voltage, providing the output. The output is divided down (R2 and R1) and fed back to the input chopper where it serves as a zero signal reference. Gain, in this case 1000, is set by the R1-R2 ratio. Because the input stage is AC coupled, its DC errors do not affect overall circuit characteristics, resulting in the extremely low offset and drift noted.

Figure 2, noise measured over a 50 second interval, shows 40nV in a 0.1Hz to 10Hz bandwidth.This low noise is attributed to the input JFET’s die size and current density.

Figure 2. Noise measures 40nVP–P in 50s sample period

关于作者

Jim Williams
James M. Williams(1948年4月14日-2011年6月12日)是一名模拟电路设计人员兼技术文章作者,先后就职于麻省理工学院(1968–1979)、Philbrick、National Semiconductor (1979–1982)和凌力尔特公司(LTC) (1982–2011)。[1]他撰写了350多篇有关模拟电路设计的论文[2],包括5本书、21篇National Semiconductor应用笔记、62篇凌力尔特应...
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

最新视频 21
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目