Measuring 18 2-Wire RTDs with the LTC2983 High Accuracy Digital Temperature Measurement System

2016-08-01

Figure 1

   

The LTC2983 measures a wide variety of temperature sensors and digitally outputs the result, in °C or °F, with 0.1°C accuracy and 0.001°C resolution. It can measure the temperature of virtually all standard (type B, E, J, K, N, S, R, T) or custom thermocouples, automatically compensate for cold junction temperatures and linearize the results. The device can also measure temperature with standard 2-, 3-, or 4-wire RTDs, thermistors and diodes.

A single LTC2983 temperature measurement device can support up to 18 2-wire RTD probes, as shown in Figure 1. Each RTD measurement involves simultaneous sensing of two voltages developed across RSENSE and the RTD probe RTDx due to the current IS. Each voltage is sensed differentially, and given the LTC2983’s high common mode rejection ratio, the number of RTDs in the stack does not adversely affect the individual measurements.

Figure 1. LTC2983 with 18 RTD sensors.

The choice of the RTD probe depends on the system accuracy and sensitivity requirements. For example, given that 2-wire probes are used, the PT-1000 may prove more robust in the presence of wiring’s parasitic resistance.

Once the RTDs are selected, IS and RSENSE should be chosen so that voltage at the top of the resistor stack (V at the CH1 input) does not exceed the input common mode limit of the LTC2983 over the operating temperature range of the system. This requirement is expressed as:

Equation 1

Consider the system shown in Figure 1 and assume the following constraints: 5V supply rail, all RTD probes are PT-100, and the maximum expected temperature measurement is at 150°C. Table 1 shows the channel assignment word for each one of the PT-100 probes. Consult the “Channel Assignment Memory Map” in the LTC2983 data sheet. Note that in this example, CH3 senses the RTD1 probe, CH4 senses RTD2, etc

Table 1. CH2 through CH20 RTD channel assignment word
Function BIT Field Value Description
Sensor Type 31:27 01100 PT-100
Sense Resistor Channel Pointer 26:22 00010 CH2
Sensor Configuration 21:18 0001 2-Wire
Excitation Current 17:14 1000 1mA
RTD Curve 13:12 01 American Curve
Custom RTD Data Pointer Address 11:6 000000 NA
Length 5:0 000000 NA
The sense resistor, connected to CH2, is configured as shown in Table 2.
Table 2. Sense resistor channel assignment word
Function BIT Field Value Description
Sensor Type 31:27 11101 Sense Resistor (29)
Sense Resistor Value Integer 26:10 000000 1111101000 1kΩ
Fraction 9:0 0000000000

RTD Stack Settling Time

Once the excitation current source is enabled, it takes a finite amount of time for the R and C chain to settle, tS, where tS is dependent on the number and value of the individual resistors (RSENSE and RTDs) and capacitors at each input node. The upper bound on tS can be estimated by lumping the total RC, but that yields an overly pessimistic result. Another method to obtain tS is to simply simulate a circuit, as shown in Figure 2.

Figure 2. Delay line model of the RTD stack.

The results of simulation are shown in Figure 3. Here all capacitors are chosen to be 100nF, and RSENSE is 1k. Each line represents settling time tS to within 0.1% of the final value of the voltage across last RTD in the stack. For each graph, all RTDs are of the same type.

Figure 3. Simulated settling time of the RTD stack.

The LTC2983, by default, inserts a delay time tDELAY = 1ms between enabling the excitation source and the beginning of the ADC conversion. This, however, is insufficient for any more than two PT-100 probes in the RTD stack (see Figure 3).

The tDELAY may be increased by setting the value in the MUX configuration register, 0x0FF. By default the register is cleared. Each LSB added to the register value represents 100µs added to default tDELAY. Consult the “Supplemental Information” section in the data sheet for more detail on the MUX delay. For example, writing 0x10 into 0x0FF results in:

Equation 2

Note that the maximum value of programmable delay is 26.5ms, which is sufficient for settling of at most six PT-1000 devices, given the C = 100nF. See Figures 3 and 4.

The tDELAY is inserted prior to each individual ADC cycle. Each RTD measurement consists of two ADC cycles. Therefore the total conversion time of the stack of RTDs is approximately:

Equation 3

Where tDELAY is programmable by the user, tCONV is given in the “Complete System Electrical Characteristics” table in the data sheet, typically 164ms including the default MUX delay, and N is the number of RTDs to be measured.

Conclusion

The LTC2983 can interface to as many as 18 2-wire RTD probes, but be sure to take into account the settling delay incurred by RC systems. The issue may be exacerbated by the number and type of RTD probes used. The delay issues can be examined using the model and simulation presented here.

关于作者

Tom Domanski
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

产品

产品分类

最新视频 21

Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目