HFAN-09.0.4: NRZ Bandwidth - LF Cutoff and Baseline Wander

2002-11-26

Figure 1

   

摘要

A fundamental goal when designing physical-layer digital communication systems is transmission of the data signal through the system with minimum distortion. In order to accomplish this goal, it is imperative to match (as closely as possible) the system bandwidth to the bandwidth requirements of the data. The purpose of this application note is to explore the effects of limiting the low end of the system bandwidth.

添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章