摘要
At low data rates, the maximum number of transceivers and receivers on an RS-485 bus has a practical limit imposed by the voltage seen by receivers in relation to their input threshold voltage. The input impedance of an RS-485 receiver is not fixed in the standard and can vary between parts. This application note explains how to calculate the maximum number of receivers on a bus from data present in the data sheets for low and standard data rates.
Introduction
The TIA/EIA-485-A standard, commonly known as RS-485, has been a staple of industrial communication for many years. The RS-485 is a standard bi-directional half-duplex or full-duplex data transmission and allows multiple receivers and drivers on a shared bus. Figure 1 shows a simplified block diagram of a simple RS-485 bus.

Figure 1. Simplified RS-485 network diagram
The RS-485 standard does not definitely state a maximum number of nodes on a bus but does offer guidelines to determine and calculate the maximum bus size. At low data rates, the maximum number of transceivers and receivers on an RS-485 bus has a practical limit imposed by the voltage seen by receivers in relation to their input threshold voltage. Increasing the number of receivers on a bus leads to lower differential load impedance that the active driver sees-leading to lower differential voltage at the receivers due to the input impedance that each receiver has in addition to the cable impedance. The input impedance of an RS-485 receiver is not fixed in the RS-485 standard and varies strongly between part numbers. This application note explains how to calculate the maximum number of receivers on a bus from data present in the data sheets for low and standard data rates.
Start with the Unit Load
The RS-485 standard begins by defining a hypothetical term called the "unit load" (UL). The DC, or static, load of an RS-485 transceiver is defined by a fractional multiple of 1UL. Figure 2 shows the receiver single-ended input current-voltage mask that defines 1UL, as specified in the standard.

Figure 2. Single unit load current-voltage characteristics defined in the RS-485 standard.
The RS-485 receiver measurements are expected to fall within the mask over the entire −7V to +12V span. Typical receiver input current measurements for various Maxim RS-485 transceivers are shown in Figure 3. The mask has been superimposed in the figure to highlight that the input current characteristics are within the required limits over the entire −7V to +12V input voltage span required in the RS-485 standard.

Figure 3. Single unit load current-voltage characteristics for various Maxim RS-485 transceivers.
Every RS-485 transceiver or receiver can be specified with regards to the number of unit loads (nUL) that it represents on the bus.
The RS-485 standard does not explicitly declare a maximum number of nodes for an RS-485 bus and, instead, outlines the method to calculate the maximum value. Paraphrased, the calculation is as follows: the equivalent number of unit loads, nUL, that a receiver represents, is the ratio of the receiver's input current to the standard 1UL current. It is expected that the receiver input currents are usually highest at the −7V to +12V input voltages, and, as such, most manufacturers specify them at these extreme inputs. The input current ratios are calculated at these two inputs and the nUL is, then, the greater of the two ratios.
Calculate the Maximum UL (nMAX) on a Bus
The RS-485 standard limits the maximum driver current such that a standard bus can reliably support no more than 32UL. To calculate the maximum number of nodes on a bus, divide this value by the total sum of the fractional ULs: nMAX = 32UL / (nUL1 + nUL2 + … nULn)
Example 1: How Many MAX22506E Transceivers?
The following is an example calculation using Analog's MAX22506E 50Mbps half-duplex transceiver. The MAX22506E datasheet specifies the receiver inputs as shown in Table 1.
| Input Current (A and B) | IA,B | DE = GND, VCC = GND, +3.6V or +5.5V | VIN = +12V | +390 (max) | µA |
| VIN = −7V | -360 (min) |
Using this information, and the −7V to +12V current levels shown in Figure 2 (-0.8mA and +1mA, respectively), the fractional UL value at the −7V and +12V intercept points can be calculated as follows:
At the −7V intercept point: nULMAX22506E = -0.36mA/-0.8mA = 0.45UL
At the +12V intercept point: nULMAX22506E = +0.39mA/+1mA = 0.39UL
The larger of these two values, 0.45UL, is the fractional unit load of the MAX22506E.
Assuming a bus comprised of only MAX22506E simplifies the nMAX calculation to:
nMAX = 32UL/0.45UL
nMAX = 71 MAX22506E transceivers can comprise a single RS-485 bus.
Example 2: How Many Transceivers on a Mixed Bus?
The following is an example calculation using three different transceivers on a single RS-485 bus. This example uses Analog's MAX22506E, the MAX14783E, and the fault protected MAX14776E. All of these transceivers operate at 3.3V to 5V, with a maximum data rate of at least 20Mbps, and all are half-duplex. The receiver input characteristics for each of these is shown in Figure 3.
Table 2 shows the receiver input characteristics for the 3 devices, as taken from their respective datasheets.
| Input Voltage (A and B) |
Maximum Input Current (µA) | ||
| MAX22506E | MAX14783E | MAX14776E | |
| VIN = −7V | -360 | -800 | -200 |
| VIN = +12V | +390 | +1000 | +280 |
Using the information in this table, the fractional UL value at the −7V and +12V intercept points can be calculated as shown in Table 3.
| Input voltage (A and B) |
nUL Calculation for Transceivers | ||
| MAX22506E | MAX14783E | MAX14776E | |
| VIN = −7V | -0.36mA/-0.8mA = 0.45UL | -0.8mA/-0.8mA = 1UL | -0.20mA/-0.8mA = 0.25UL |
| VIN = +12V | 0.39mA/1mA = 0.39UL | +1.0mA/1mA = 1UL | +0.28mA/1mA = 0.28UL |
The larger of the two ratios, for each device, is the fractional UL. As shown in the table, this is 0.45UL for the MAX22506E, 1UL for the MAX14783E, and 0.28UL for the MAX14776E.
The maximum number of transceivers on the bus is calculated as follows:
nMAX = 32UL / (nUL1 + nUL2 + … nULn)
Using the calculated values, Table 4 shows some of the valid combinations (32 UL, max) of these transceivers that can be used on a single RS-485 bus.
|
MAX22506E |
MAX14783E |
MAX14776E |
Total UL |
|||
| Transceivers | UL | Transceivers | UL | Transceivers | UL | |
| 1 | 0.45 | 30 | 30 | 5 | 1.4 | 31.9 |
| 10 | 4.5 | 25 | 25 | 8 | 2.2 | 31.7 |
| 12 | 5.4 | 20 | 20 | 23 | 6.4 | 31.8 |
| 16 | 7.2 | 12 | 12 | 45 | 12.6 | 31.8 |
| 20 | 9 | 18 | 18 | 17 | 4.8 | 31.8 |
| 25 | 11.3 | 15 | 15 | 20 | 5.6 | 31.9 |
| 45 | 20.3 | 9 | 9 | 9 | 2.5 | 31.8 |
关联至此文章
产品
MAX14775E/MAX14776E评估套件
2.5kVRMS、完全隔离型RS-485/RS-422模块收发器 + 电源
高速3.3V/5V RS-485/RS-422收发器,具有±35kV HBM ESD保护
具有高EFT抗扰度的50Mbps半双工RS-485/RS-422收发器
用于长电缆的100Mbps半双工RS-485/RS-422收发器
2.5kVRMS、完全隔离型RS-485/RS-422模块收发器 + 电源
用于长电缆的100Mbps半双工RS-485/RS-422收发器
±65V故障保护500Kbps/20Mbps半双工RS-485/RS-422收发器
±65V故障保护500Kbps/20Mbps半双工RS-485/RS-422收发器