J-FET-Based DC/DC Converter Starts and Runs from 300mV Supply

2006-09-01

Figure 1

   

A J-FET’s self-biasing characteristic can be utilized to construct a DC/DC converter powered from as little as 300mV. Solar cells, thermopiles and single stage fuel cells, all with outputs below 600mV, are typical power sources for such a converter.

Figure 1, an N-channel J-FET I-V plot, shows drain-source conduction under zero bias (gate and source tied together) conditions. This property can be exploited to produce a self-starting DC/DC converter that runs from 0.3V to 1.6V inputs.

Figure 1. Zero volt biased JFET I-V curve shows 10mA conduction at 100mV, rising above 40mA at 500mV. Characteristic enables construction of DC/DC converter powered from 300mV supply.

Figure 2 shows the circuit. Q1 and T1 form an oscillator with T1’s secondary providing regenerative feedback to Q1’s gate. When power is applied, Q1’s gate is at zero volts and its drain conducts current via T1’s primary. T1’s phase inverting secondary responds by going negative at Q1’s gate, turning it off. T1’s primary current ceases, its secondary collapses and oscillation commences. T1’s primary action causes positive going “flyback” events at Q1’s drain, which are rectified and filtered. Q2’s approximately 2V turn-on potential isolates the load, aiding start-up. When Q2 turns on, circuit output heads towards 5V. C1, powered from Q2’s source, enforces output regulation by comparing a portion of the output with its internal voltage reference. C1’s switched output controls Q1’s on-time via Q3, forming a control loop.

Figure 2. J-FET based DC/DC converter runs from 300mV input. Q1-T1 oscillator output is rectified and filtered. Load is isolated until Q2 source arrives at approximately 2V, aiding startup. Comparator and Q3 close loop around oscillator, controlling Q1’s on-time to stabilize 5V output.

Waveforms for the circuit include the AC coupled output (Figure 3, trace A), C1’s output (trace B) and Q1’s drain flyback events (trace C). When the output drops below 5V, C1 goes low, turning on Q1. Q1’s resultant flyback events continue until the 5V output is restored. This pattern repeats, maintaining the output.

Figure 3. J-FET based DC/DC converter waveforms. When supply output (trace A) decays, C1 (trace B) switches, allowing Q1 to oscillate. Resultant flyback events at Q1 drain (trace C) restore supply output.

The 5V output can supply up to 2mA, sufficient to power circuitry or supply bias to a higher power switching regulator when more current is required. The circuit will start into loads of 300µA at 300mV input; 2mA loading requires a 475mV supply. Figure 4 plots minimum input voltage vs output current over a range of loads.

Figure 4. J-FET based DC/DC converter of Figure 2 starts and runs into 100µA load at VIN = 275mV. Regulation to 2mA is possible, although required VIN rises to 500mV. Quiescent current control circuitry of Figure 5 slightly increases input voltage required to support load at VIN < 500mV.

Q3’s shunt control of Q1 is simple and effective, but results in a 25mA quiescent current drain. Figure 5’s modifications reduce this figure to 1mA by series switching T1’s secondary. Here, Q3 switches series-connected Q4, more efficiently controlling Q1’s gate drive. Negative turn-off bias for Q4 is bootstrapped from T1’s secondary; the 6.8V zener holds off bias supply loading during initial power application, aiding start-up. Figure 4 shows minimal penalty imposed by the added quiescent current control circuitry.

Figure 5. Adding Q3, Q4 and bootstrapped negative bias generator reduces quiescent current. Comparator directed Q3 switches Q4, more efficiently controlling Q1’s gate drive. Q2 and zener diode isolate all loading during Q1 start-up.

关于作者

Jim Williams
James M. Williams(1948年4月14日-2011年6月12日)是一名模拟电路设计人员兼技术文章作者,先后就职于麻省理工学院(1968–1979)、Philbrick、National Semiconductor (1979–1982)和凌力尔特公司(LTC) (1982–2011)。[1]他撰写了350多篇有关模拟电路设计的论文[2],包括5本书、21篇National
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

产品分类
最新视频 25
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目