设计、搭建、测试
图示的电路板已装配完成且经过测试。

概览

设计资源

设计与集成文件

  • Schematic
  • PCB Layout
  • Bill of Materials
下载设计文件 2.49 M

描述

The MAX17595 is a peak-current-mode controller for designing wide input-voltage flyback regulators. The MAX17595 offers optimized input thresholds for universal input AC-DC converters and telecom DC-DC (36V to 72V input range) power supplies. It contains a built-in gate driver for an external n-channel MOSFET. The MAX17595 houses an internal error amplifier with 1% accurate reference, eliminating the need for an external reference. The switching frequency is programmable from 100kHz to 1MHz with an accuracy of 8%, allowing optimization of magnetic and filter components, resulting in compact and cost-effective power conversion. For EMI-sensitive applications, the MAX17595 incorporates a programmable frequency dithering scheme, enabling low-EMI spread-spectrum operation. Users can start the power supply precisely at the desired input voltage, implement input overvoltage protection, and program soft-start time. A programmable slope compensation scheme is provided to ensure stability of the peak current-mode control scheme. Hiccup-mode overcurrent protection and thermal shutdown are provided to minimize dissipation in overcurrent and overtemperature fault conditions.

优势和特点

  • Programmable Switching Frequency Allows Optimization of the Magnetic and Filter Components, Resulting in Compact, Cost-Effective, Efficient Isolated/ Nonisolated Power Supplies
  • 100kHz to 1MHz Programmable Switching Frequency with Optional Synchronization
  • Peak Current Mode Control Provides Excellent Transient Response—Offline (Universal Input AC) and Telecom (36V to 72V) Flyback Controller
  • Programmable Frequency Dithering Enables Low EMI Spread-Spectrum Operation
  • Integrated Protection Features Enhance System Reliability
  • Adjustable Current Limit with External Current Sense Resistor
  • Fast Cycle-By-Cycle Peak Current Limiting Hiccup-Mode Short-Circuit Protection
  • Overtemperature Protection
  • Programmable Soft-Start and Slope Compensation
  • Input Overvoltage Protection

详情

The MAX17595 is a peak-current-mode controller for designing wide input-voltage flyback regulators. The MAX17595 offers optimized input thresholds for universal input AC-DC converters and telecom DC-DC (36V to 72V input range) power supplies. It contains a built-in gate driver for an external n-channel MOSFET. The MAX17595 houses an internal error amplifier with 1% accurate reference, eliminating the need for an external reference. The switching frequency is programmable from 100kHz to 1MHz with an accuracy of 8%, allowing optimization of magnetic and filter components, resulting in compact and cost-effective power conversion. For EMI-sensitive applications, the MAX17595 incorporates a programmable frequency dithering scheme, enabling low-EMI spread-spectrum operation. Users can start the power supply precisely at the desired input voltage, implement input overvoltage protection, and program soft-start time. A programmable slope compensation scheme is provided to ensure stability of the peak current-mode control scheme. Hiccup-mode overcurrent protection and thermal shutdown are provided to minimize dissipation in overcurrent and overtemperature fault conditions.

  • Programmable Switching Frequency Allows Optimization of the Magnetic and Filter Components, Resulting in Compact, Cost-Effective, Efficient Isolated/ Nonisolated Power Supplies
  • 100kHz to 1MHz Programmable Switching Frequency with Optional Synchronization
  • Peak Current Mode Control Provides Excellent Transient Response—Offline (Universal Input AC) and Telecom (36V to 72V) Flyback Controller
  • Programmable Frequency Dithering Enables Low EMI Spread-Spectrum Operation
  • Integrated Protection Features Enhance System Reliability
  • Adjustable Current Limit with External Current Sense Resistor
  • Fast Cycle-By-Cycle Peak Current Limiting Hiccup-Mode Short-Circuit Protection
  • Overtemperature Protection
  • Programmable Soft-Start and Slope Compensation
  • Input Overvoltage Protection

An offline DCM flyback converter using the MAX17595 is demonstrated for a 3.3V DC output application. The power supply delivers up to 4.5A at 3.3V. Table 1 shows an overview of the design specification.

Table 1. Design Specification
PARAMETER SYMBOL MIN MAX
Input Voltage VIN 176V AC 284V AC
Frequency fSW 125kHz
Output Voltage VOUT 3.3V
Output Voltage Ripple ∆VOUT 1% of VOUT max
Output Current IOUT 0 4.5A
Output Power POUT 15W

This document describes the hardware shown in Figure 1. It provides a detailed systematic technical guide to designing an offline discontinuous conduction mode (DCM) flyback using Analog Devices MAX17595 current-mode controller. The power supply has been built and tested, details of which follow later in this document.

maxrefdes1190-hardware
Figure 1. MAXREFDES1190 hardware.

Figure 2 shows a generic isolated power-supply block diagram. It consists of a power stage, an isolation transformer, rectifier, secondary-side error amplifier, and opto-coupler to provide a feedback for the primary side control. Different isolated power supplies are different depending upon how the transformer is being used in them.

Figure 2. Generic isolated power supply.
Figure 2. Generic isolated power supply.

A transformer in a flyback configuration acts differently than its usual operation of transformation of energy from primary to secondary. During a transformer’s usual operation, both primary and secondary windings conduct together at the same time to make the transfer of energy possible from primary to secondary. In a flyback configuration the primary and secondary windings do not conduct at the same time and the transformer acts more like a coupled inductor. Note that in this document we have used the following notations for the transformer turns ratio:

MAXREFDES1190 Equation 1

This means capital K for primary turns/secondary turns and small k for secondary turns/primary turns.

Figure 3 shows a simple flyback topology that consists of a transformer whose primary winding is connected to the drain of a switching MOSFET. The source of the MOSFET is connected to ground. The secondary winding is connected to the output capacitor through a rectifier diode. In this flyback configuration the current flows into the primary winding during the on time of the switching period and flows into the secondary winding during the off time of the switching period.

Figure 3. Simple flyback topology.
Figure 3. Simple flyback topology.

During the on-time when the primary switch is closed, a current, IP, flows through the primary winding as shown in Figure 4. IP can be written as follows:

MAXREFDES1190 Equation 2

Figure 4. Flyback topology during on-time, tON.
Figure 4. Flyback topology during on-time, tON.

The peak magnitude of the primary current can be written as follows:

MAXREFDES1190 Equation 3

In the secondary winding, a negative voltage is induced due to the current flowing in to the primary. The rectifier diode is reverse-biased and no current is flowing in the secondary winding. The induced voltage in the primary can be written as:

MAXREFDES1190 Equation 4

During the off-time when the primary switch opens as shown in Figure 5, the magnetic field in the primary winding collapses and the voltage at the winding reverses, while current keeps flowing in the same direction until the field fades away.

Figure 5. Flyback topology during off-time, tOFF.
Figure 5. Flyback topology during off-time, tOFF.

The secondary current IS flows and the secondary and rectifier diode is forward-biased. Output voltage VOUT is now available across the secondary coil if we ignore the forward voltage drop of the rectifier diode. The secondary winding voltage is now flown away to primary side as K x VOUT. This voltage is present across the switch until the current in the secondary winding decays to zero. Total voltage available across the switch during the off-time can be written as:

VSW = VIN + K x VOUT

This voltage also causes the breakdown of the magnetic flux in the primary winding (no current is flowing in the primary winding after this reset). Here we can see that unlike a usual transformer action where current flows in both the winding at the same time, in a flyback transformer the current flows into the primary winding during the on-time and into the secondary winding during the off-time. This is why we use the term “coupled storage inductor” for transformers used in flyback operation. It should be noted though that mechanically these transformers are like any transformer. Use in flyback operations makes transformers act differently as coupled inductors. The required duty cycle for a given input voltage and output voltage can be calculated from:

MAXREFDES1190 Equation 5

where:

MAXREFDES1190 Equation 6

Figure 6 shows a typical CCM mode flyback primary and secondary winding current, and Figure 7 shows a typical DCM mode flyback waveform.

Figure 6. A typical CCM mode flyback primary and secondary winding current
Figure 6. A typical CCM mode flyback primary and secondary winding current
Figure 7. A typical DCM mode flyback topology waveform.
Figure 7. A typical DCM mode flyback topology waveform.

Design Procedure for Offline Flyback Using MAX17595

Now that the basic principle of the DCM flyback is understood, a practical design can be illustrated. The design parameters are obtained by using expressions given in Analog Devices Application Note 5504. This document is primarily concerned with the power stage and the feedback loop design, and is intended to complement the information contained in the MAX17595 data sheet.

Flyback converters can be operated in discontinuous conduction mode (DCM) or continuous conduction mode (CCM). The component choices, stress level in power devices, and controller design vary depending on the operating mode of the converter. The design discussed in this document is a DCM design and expressions for calculating component values and ratings are presented to achieve the design goals.

Step 1: Switching Frequency

For offline flyback operation, the selection of switching frequency is of prime importance. Thermal limits and junction temperature of the device limits the selected switching frequency to be less than 150kHz. For this design we have selected a switching frequency of 125kHz. The MAX17595 switching frequency is programmable between 100kHz and 1000kHz with a resistor RRT connected between RT and SGND. The RRT is calculated as follows:

MAXREFDES1190 Equation 7

A standard 80.6kΩ resistor is selected for RRT.

Step 2: Transformer Magnetizing Inductance and Turns Ratio

In a DCM flyback converter, the energy stored in the primary inductance of the flyback transformer is delivered entirely to the output. The maximum primary-inductance value for which the converter remains in DCM at all operating conditions can be calculated as:

MAXREFDES1190 Equation 8

where:

DMAX = 0.43V

VD = 0.1V is the forward voltage drop of the rectifier diode of the secondary winding. Here we are using synchronous rectification using the MAX17606 MOSFET driver at the secondary side.

In this offline application, the DC bus voltage varies from 248.9V DC to 401.6V DC. But the actual minimum input operating voltage depends on the 100Hz ripple present on the DC bus capacitor. In this application, the ripple is assumed to be 30V and hence the minimum DC input to the converter.

VINMIN = 176 × 1.414 − 30 = 218.9V

Substituting the above values in the expression of LMAG as follows:

MAXREFDES1190 Equation 9

The primary inductance for our design, LPRI is chosen as 1mH, LPRI = 1mH.

The leakage inductance of the transformer should be targeted as low as possible. For this design, we achieved a 1.5% leakage inductance of 15µH, LLKG = 15µH.

A customized transformer 750317627 from Würth Elektronik® is used in this design. This transformer also fulfills the specification of turns ratio, bias winding, and primary/secondary currents requirement of the design that is calculated step by step in this document. The transformer has dielectric isolation specification of 4200V AC.

Step 3: Maximum Duty Cycle Calculation with Selected LPRI

Use the following expressions to calculate the maximum duty cycle of the converter for the selected frequency and magnetizing inductance:

MAXREFDES1190 Equation 10

Calculate the required transformer turns ratio (k) using the expressions as follows:

MAXREFDES1190 Equation 11 

For the present design, k is chosen as 1:0.034.

Step 4: Calculation of Peak/RMS Current

Primary and secondary RMS and primary peak currents calculations are needed to design the transformer in switched-mode power supplies. Also, primary peak current is used in setting the current limit. Use the following expressions to calculate the primary and secondary peak and RMS currents.

MAXREFDES1190 Equation 12

Step 5: Current Limit Resistor Calculation

For current limit setting, the peak current can be calculated as follows:

ILIM = 1.2 x IPRIPEAK = 1.2 x 0.5477 = 0.657A 

The device includes a robust overcurrent protection scheme that protects the device under overload and short-circuit conditions. A current-sense resistor, connected between the source of the MOSFET and PGND, sets the peak current limit. The current-limit comparator has a voltage trip level (VCS-PEAK) of 300mV. Use the following equation to calculate the value of RCS:

MAXREFDES1190 Equation 13

where IMOSFET is the peak current flowing through the MOSFET. A typical 430mΩ current-sense resistor is selected, RCS = 430mΩ.

Step 6: MOSFET Selection

MOSFET selection criteria includes maximum drain voltage, peak/RMS current in the primary, and the maximum allowable power dissipation of the package without exceeding the junction temperature limits. The voltage seen by the MOSFET drain is the sum of the input voltage, the reflected secondary voltage on the transformer primary, and the leakage inductance spike. The MOSFET’s absolute maximum VDS rating must be higher than the worst-case drain voltage as follows:

MAXREFDES1190 Equation 14

For this application, the 800V 2.5A n-channel MOSFET IPD80R2K4P7 from Infineon® is selected as the primary MOSFET.

Step 7: Snubber Selection

RCD snubbers reduce the maximum voltage stress on the MOSFET by clamping the voltage level. However, they also dissipate power and reduce efficiency. They might not always be required, however it is always a good idea to leave place holders in the board for RCD and RC snubbers. Ideally, the external MOSFET experiences a drain-source voltage stress equal to the sum of the input voltage and reflected voltage across the primary winding during the off period of the MOSFET. In practice, parasitic inductors and capacitors in the circuit, such as leakage inductance of the flyback transformer, cause voltage overshoot and ringing in addition to the ideally expected voltage stress. Snubber circuits are used to limit the voltage overshoots to safe levels within the voltage rating of the external MOSFET. The snubber capacitor can be calculated using the following expression:

MAXREFDES1190 Equation 15

Considering the derating of the capacitor, we selected a capacitor of value 1200pF, CSNUB = 1200pF.

Figure 8. Bias winding configuration.
Figure 8. Bias winding configuration.

The power that must be dissipated in the snubber resistor is calculated using the following expressions:

PSNUB = 0.833 x LLKG x IPRIPEAK2 x fSW 
PSNUB = 0.833 x 15µ x 0.5472 x 125k = 468mW 

The snubber resistor is calculated based on the below expression:

MAXREFDES1190 Equation 16

A standard resistor of 120kΩ 1W is selected, RSNUB = 120kΩ.

The voltage rating of the snubber diode is:

MAXREFDES1190 Equation 17

An 800V, 1A diode S1KL from Taiwan Semiconductor is selected as the snubber diode for this design.

Step 8: Selection of Secondary MOSFET

The maximum operating drain-source rating of the secondary MOSFET must be higher than the sum of the output voltage and the reflected input voltage. We use the following expression to calculate the secondary diode voltage rating:

VSEC = 1.25 x (k x VINMAX + VOUT)
VSEC = 1.25 x (0.034en x 401.6 + 3.3) = 21.34V

For this application a 40V, 40A, MOSFET BSZ040N04LSG from Infineon is selected as a secondary MOSFET.

Step 9: Bias Winding Supply Configuration

The MAX17595 is implemented with a 20V VIN UVLO wake-up level with 13V hysteresis to optimize the size of bias capacitor. A simple RC circuit is used to start up the MAX17595. To sustain the operation of the circuit, the input supply to the IC is bootstrapped through diode D2 as shown in Figure 8.

Use VBIAS = 12V. Bias winding turns ratio kb can be calculated as follows:

MAXREFDES1190 Equation 18

In isolated applications where a bias winding configuration is used to power up the MAX17595, CSTART can be calculated as follows:

MAXREFDES1190 Equation 19

CSTART is the startup capacitor, CDRV is the cumulative capacitor used at the DRV pin, IIN is the MAX17595 quiescent current, tSS is the soft-start time, VOUT is the output voltage, COUT is the output capacitor used, and QG is the gate charge of the primary n-channel MOSFET.

Select:

MAXREFDES1190 Equation 20

It is recommended to consider the derating of the startup capacitor. A typical value of 4.7µF is selected as CSTART, CSTART = 4.7µF.

RSTART can be calculated as follows:

MAXREFDES1190 Equation 21

where CSTART is in µF.

MAXREFDES1190 Equation 22

RSTART is divided into three equal value resistors of value 610.8kΩ each. Standard 1206 resistor value of 619kΩ 250mW is selected for RIN1, RIN2, and RIN3, respectively.

RIN1 = RIN2 = RIN3 = 619kΩ

Step 10: Feedback Resistor Selection RU, RB

For all the applications that use a startup network to bias the VIN pin during the power-up sequence, calculate the feedback potential divider using the following formulas:

MAXREFDES1190 Equation 23

A standard resistor of 56Ω is selected, RB = 56Ω.

MAXREFDES1190 Equation 24

where VREF is the reference set by the secondary-side controller (VREF = 1.24V for TLV431 is used in this design).

MAXREFDES1190 Equation 25

A standard resistor of 0.0931kΩ is selected, RU = 0.0931kΩ.

Step 11: Soft-Start Capacitor

The soft-start period for the devices can be programmed by selecting the value of the capacitor CSS connected from the SS pin to SGND. Capacitor CSS can be calculated as:

CSS = 8.264 x tSS

where tSS is expressed in ms and the resultant value of CSS is in nF.

CSS = 8.264 x tSS = 8.264 x 12 = 99.17nF

A standard 100nF is selected as the soft-start capacitor, CSS = 100nF.

Step 12: Input Capacitor Selection

The MAX17595 is optimized to implement offline AC-DC applications. In such applications, the input capacitor must be selected based on either the ripple due to the rectified line voltage, or based on holdup-time requirements. Holdup time can be defined as the time period over which the power supply should regulate its output voltage from the instant the AC power fails.

For the flyback converter, the input capacitor supplies the input current when the diode rectifier is off. The voltage discharge on the input capacitor, due to the input average current, should be within the limits specified. Assuming 25% ripple present on input DC capacitor, the input capacitor can be calculated as follows:

MAXREFDES1190 Equation 26

where:

η = Target efficiency = 87%*

PLOAD = 3.3 × 4.5 = 15W

VINPK = Peak voltage at minimum AC voltage = 248.9V

MAXREFDES1190 Equation 27

*For low voltage, high current offline flybacks, the achieved efficiency is always less than the target efficiency.

Step 13: Output Capacitor Selection

X7R ceramic output capacitors are preferred in industrial applications due to their stability over temperature. The output capacitor is usually sized to support a step load of a certain percentage of the rated output current so that the output voltage deviation is contained to 3% of the rated output voltage. The output capacitance can be calculated by using the below expressions:

MAXREFDES1190 Equation 28

where ISTEP is the load step, tRESPONSE is the response time of the controller, ∆VOUT is the allowable output voltage deviation, and fC is the target closed-loop crossover frequency. In our application, we selected fC = 5kHz, typical bandwidth at nominal voltage for isolated applications to minimize noise and proportionally increase the gain.

MAXREFDES1190 Equation 29

Due to the DC-bias characteristics, 4 x 220µF 6.3V MLCC capacitors are selected as COUT for this design.

MLCC capacitor values change with temperature and applied voltage. Refer to the capacitor data sheets to select capacitors that guarantee the required output capacitance across the operating range. For design calculations, use the worst-case derated value of capacitance, based on temperature range and applied voltage. We have also used 3 x tantalum polymer capacitors with a value of 470µF in parallel with the MLCCs. The worstcase total value of all the capacitors is 1596µF.

For the flyback converter, the output capacitor supplies the load current when the main switch is on, and therefore the output voltage ripple is a function of load current and duty cycle. Use the following expression to estimate the output capacitor ripple:

MAXREFDES1190 Equation 30

Step 14: Loop Compensation

Optocoupler feedback is used in isolated flyback converter designs for precise control of isolated output voltage. Figure 9 shows the overall scheme of the optocoupler feedback.

Figure 9. A typical opto-coupler-based feedback compensation.
Figure 9. A typical opto-coupler-based feedback compensation.

Use RFB = 470Ω (typ), for an optocoupler transistor current of 1mA. Select R1 = 49.9kΩ and R2 = 22kΩ (typical values) to use the full range of available COMP voltage. U3 is a low-voltage adjustable shunt regulator with a 1.24V reference voltage. In this design a 1.24V, 0.5% shunt regulator TLV431BFTA from Diodes Inc. is selected.

Calculate RLED using expression below:

RLED = 400 x CTR x (VOUT - 2.7)
RLED = 400 x 1 x (3.3 - 2.7) = 0.240kΩ

A standard 0.240kΩ resistor is selected, RLED = 0.240kΩ.

The bandwidth of typical optocouplers limits the achievable closed-loop bandwidth of opto-isolated converters. Considering this limitation, the closed-loop crossover frequency can be chosen at the nominal input voltage by selecting fC = 5kHz. Closed-loop compensation values are designed based on the open-loop gain at the desired crossover frequency, fC. The open-loop at fC is calculated using the following expressions.

MAXREFDES1190 Equation 31

Three controller configurations are suggested in Application Note 5504 based on open-loop gain and the RLED value. For typical designs, the current transfer ratio (CTR) of the optocoupler designs can be assumed to be unity. It is known that the comparator and gate-driver delays associated with the input voltage variations affect the optocoupler CTR. Depending on the optocoupler selected, variations in CTR causes wide variations in bandwidth of the closed-loop system across the input-voltage operating range. It is recommended to select an optocoupler with less CTR variations across the operating range. Checking the condition as stated in Application Note 5504:

MAXREFDES1190 Equation 32

As 1.49 > 1.2, therefore, as stated in ApplicationNote5504, configuration 2 is selected. Figure 10 shows a typical schematic of configuration 2. The RM value can be calculated from the expression below:

MAXREFDES1190 Equation 33

Figure 10. Opto-coupler feedback compensation configuration 2 schematic.
Figure 10. Opto-coupler feedback compensation configuration 2 schematic.

A standard 100kΩ resistor is selected as RM, RM = 100kΩ. The CM value can be calculated from the expression below:

MAXREFDES1190 Equation 34

A standard 6.8nF capacitor is selected as CM, CM = 6.8nF. The CCF2 value can be calculated from the expression below:

MAXREFDES1190 Equation 35

A standard 82pF capacitor is selected as CCF2 = 82pF. The CCF1 value can be calculated from the expression below:

MAXREFDES1190 Equation 36

A standard 6.8µF capacitor is selected as CCF1 = 6.8µF.

Step 15: EN/UVLO and OVI Setting

The device’s EN/UVLO pin serves as an enable/disable input, as well as an accurate programmable input UVLO pin. The device does not commence startup operation unless the EN/UVLO pin voltage exceeds 1.21V. The device turns off if the EN/UVLO pin voltage falls below 1.15V. A resistor-divider from the input DC bus to ground can be used to divide down and apply a fraction of the input DC voltage (VDC) to the EN/UVLO pin. The values of the resistor-divider can be selected so the EN/UVLO pin voltage exceeds the 1.23V turn-on threshold at the desired input DC bus voltage. The same resistor-divider can be modified with an additional resistor (ROVI) to implement input overvoltage protection in addition to the EN/ UVLO functionality as shown in Figure 11.

Figure 11. Programming EN/UVLO and OVI.
Figure 11. Programming EN/UVLO and OVI.

When voltage at the OVI pin exceeds 1.21V the devices stop switching and resume switching operations only if voltage at the OVI pin falls below 1.15V. For given values of startup DC input voltage (VSTART) and input overvoltage-protection voltage (VOVI), the resistor values for the divider can be calculated as follows:

Select ROVI = 24.9kΩ.

MAXREFDES1190 Equation 37

where VOVI = maximum allowed overvoltage = 290 x 1.414 = 410.12V.

MAXREFDES1190 Equation 38

A standard 22kΩ resistor is selected, where REN = 22kΩ.

The same resistor-divider can be modified to implement input overvoltage protection. When the voltage at the OVI pin exceeds 1.215V (typ), the device stops switching. The device resumes switching operations only if the voltage at the OVI pin falls below 1.1V (typ).

MAXREFDES1190 Equation 39

In universal AC input applications, RSUM may need to be implemented as equal resistors in series (RDC1, RDC2, and RDC3) so that voltage across each resistor is limited to its maximum operation voltage.

MAXREFDES1190 Equation 40

A standard 2.8MΩ resistor is selected for RDC1, RDC2, and RDC3.

支持与培训

搜索我们的知识库,获取技术问题答案。我们专门的应用工程师团队也会随时为您解答技术问题。