设计、搭建、测试
图示的电路板已装配完成且经过测试。

概览

描述

Due to its simplicity and low cost, the flyback converter is the preferred choice for low-to-medium isolated DC-DC power-conversion applications. However, the use of an optocoupler or an auxiliary winding on the flyback transformer for voltage feedback across the isolation barrier increases the number of components and design complexity. The MAX17690 eliminates the need for an optocoupler or auxiliary transformer winding and achieves ±5% output voltage regulation over line, load, and temperature variations.

The MAX17690 implements an innovative algorithm to accurately determine the output voltage by sensing the reflected voltage across the primary winding during the flyback time interval. By sampling and regulating this reflected voltage when the secondary current is close to zero, the effects of secondary-side DC losses in the transformer winding, the PCB tracks, and the rectifying diode on output voltage regulation can be minimized.

The MAX17690 also compensates for the negative temperature coefficient of the rectifying diode.

优势和特点

  • 4.5V to 60V Input Voltage Range
  • Programmable Switching Frequency from 50kHz to 250kHz
  • Programmable Input Enable/UVLO Feature
  • Programmable Input Overvoltage Protection
  • Adjustable Soft-Start
  • 2A/4A Peak Source/Sink Gate Drive Capability
  • Hiccup Mode Short-Circuit Protection
  • Fast Cycle-by-Cycle Peak Current Limit
  • Thermal Shutdown Protection
  • Space-Saving, 16-Pin, 3mm x 3mm TQFN Package
  • -40°C to +125°C Operating Temperature Range

详情

Due to its simplicity and low cost, the flyback converter is the preferred choice for low-to-medium isolated DC-DC power-conversion applications. However, the use of an optocoupler or an auxiliary winding on the flyback transformer for voltage feedback across the isolation barrier increases the number of components and design complexity. The MAX17690 eliminates the need for an optocoupler or auxiliary transformer winding and achieves ±5% output voltage regulation over line, load, and temperature variations.

The MAX17690 implements an innovative algorithm to accurately determine the output voltage by sensing the reflected voltage across the primary winding during the flyback time interval. By sampling and regulating this reflected voltage when the secondary current is close to zero, the effects of secondary-side DC losses in the transformer winding, the PCB tracks, and the rectifying diode on output voltage regulation can be minimized.

The MAX17690 also compensates for the negative temperature coefficient of the rectifying diode.

Other features include the following:

  • 4.5V to 60V Input Voltage Range
  • Programmable Switching Frequency from 50kHz to 250kHz
  • Programmable Input Enable/UVLO Feature
  • Programmable Input Overvoltage Protection
  • Adjustable Soft-Start
  • 2A/4A Peak Source/Sink Gate Drive Capability
  • Hiccup Mode Short-Circuit Protection
  • Fast Cycle-by-Cycle Peak Current Limit
  • Thermal Shutdown Protection
  • Space-Saving, 16-Pin, 3mm x 3mm TQFN Package
  • -40°C to +125°C Operating Temperature Range

An isolated no-opto flyback DC-DC converter using the MAX17690 and MAX17606 is demonstrated for a 5V DC output application. The power supply delivers up to 2A at 5V. Table 1 shows an overview of the design specification.

Table 1. Design Specification
PARAMETER SYMBOL MIN MAX
Input Voltage VIN 18V 60V
Frequency fSW 143.5kHz
Peak Efficiency at Full
Load
ηMAX 90.4%
Efficiency at Minimum
Load
ηMIN 60%
Output Voltage VOU 5V
Output Voltage Ripple ΔVO 50mV
Maximum Output Current IOUT 2A
Maximum Output Power POUT 10W

This document describes the hardware shown in Figure 1. It provides a detailed systematic technical guide to designing an isolated no-opto flyback DC-DC converter using Maxim’s MAX17690 controller. The power supply has been built and tested.


Figure 1. MAXREFDES1105 hardware.

One of the drawbacks encountered in most isolated DC-DC converter topologies is that information relating to the output voltage on the isolated secondary side of the transformer must be communicated back to the primary side to maintain output voltage regulation. In a regular isolated flyback converter, this is normally achieved using an optocoupler feedback circuit or an additional auxiliary winding on the flyback transformer. Optocoupler feedback circuits reduce overall power-supply efficiency, and the extra components increase the cost and physical size of the power supply. In addition, optocoupler feedback circuits are difficult to design reliably due to their limited bandwidth, nonlinearity, high CTR variation, and aging effects. Feedback circuits employing auxiliary transformer windings also exhibit deficiencies. Using an extra winding adds to the flyback transformer’s complexity, physical size, and cost, while load regulation and dynamic response are often poor.

The MAX17690 is a peak current-mode controller designed specifically to eliminate the need for optocoupler or auxiliary transformer winding feedback in the traditional isolated flyback topology, therefore reducing size, cost, and design complexity. It derives information about the isolated output voltage by examining the voltage on the primary-side winding of the flyback transformer.

Other than this uniquely innovative method for regulating the output voltage, the no-opto isolated flyback converter using the MAX17690 follows the same general design process as a traditional flyback converter. To understand the operation and benefits of the no-opto flyback converter it is useful to review the schematic and typical waveforms of the traditional flyback converter (using the MAX17595), shown in Figure 2.


Figure 2. Isolated flyback converter topology with typical waveforms.

The simplified schematic in Figure 2 illustrates how information about the output voltage is obtained across the isolation barrier in traditional isolated flyback converters. The optocoupler feedback mechanism requires at least 10 components including an optocoupler and a shunt regulator, in addition to a primary-side bias voltage, VBIAS, to drive the photo-transistor. The error voltage FB2 connects to the FB pin of the flyback controller.

The transformer feedback method requires an additional winding on the primary side of the flyback transformer, a diode, a capacitor, and two resistors to generate a voltage proportional to the output voltage. This voltage is compared to an internal reference in a traditional flyback controller to generate the error voltage.

By including additional innovative features internally in the MAX17690 no-opto flyback controller, Maxim has enabled power-supply designers to eliminate the additional components, board area, complexity, and cost associated with both the optocoupler and transformer feedback methods. Figure 3 illustrates a simplified schematic and typical waveforms for an isolated no-opto flyback DC-DC converter using the MAX17690.


Figure 3. Isolated no-opto flyback converter topology with typical waveforms

By comparing Figure 3 with Figure 2, it is evident that there is no difference in the voltage and current waveforms in the traditional and no-opto flyback topologies. The difference is in the control method used to maintain VOUT at its target value over the required load, line, and temperature range. The MAX17690 achieves this with minimum components by forcing the voltage VFLYBACK during the conduction period of DFR to be precisely the voltage required to maintain a constant VOUT. When QP turns off, DFR conducts and the drain voltage of QP, rises to a voltage VFLYBACK above VIN. After initial ringing due to transformer leakage inductance and the junction capacitance of DFR and output capacitance of QP, the voltage VFLYBACK is given by:

MAXREFDES1105 Equation 1

where:

VFLYBACK is the QP drain voltage relative to primary ground

VDFR(T) is the forward voltage drop of DFR, which has a negative temperature coefficient

ILS(t) is the instantaneous secondary transformer current RS(T) is the total DC resistance of the secondary circuit, which has a positive temperature coefficient

nSP is the secondary to primary turns ratio of the flyback transformer.

The voltage of interest is (VFLYBACK - VIN) since this is a measure of VOUT. An internal voltage to current amplifier generates a current proportional to (VFLYBACK - VIN). This current then flows through RSET to generate a ground referenced voltage, VSET, proportional to (VFLYBACK - VIN). This requires that:

MAXREFDES1105 Equation 2

Combining this equation with the previous equation for VFLYBACK, we have:

MAXREFDES1105 Equation 3

We need to consider the effect of the temperature dependence of VDFR and the time dependence of ILS on the control system. If VFLYBACK is sampled at a time when ILS is very close to zero, then the term ILS(t) x RS(T) is negligible and can be assumed to be zero in the previous expression. This is the case when the flyback converter is operating in, or close to, discontinuous conduction mode. It is very important to sample the VFLYBACK voltage before the secondary current reaches zero since there is a very large oscillation on VFLYBACK due to the resonance between the primary magnetizing inductance of the flyback transformer and the output capacitance of QP as soon as the current reaches zero in the secondary, as shown in Figures 2 and 3. The time at which VFLYBACK is sampled is set by resistor RVCM.

The VDFR term has a significant negative temperature coefficient that must be compensated to ensure acceptable output voltage regulation over the required temperature range. This is achieved by internally connecting a positive temperature coefficient current source to the VSET pin. The current is set by resistor RTC connected to ground. The simplest way to understand the temperature compensation mechanism is to think about what needs to happen in the control system when temperature increases. In an uncompensated system, as the temperature increases, VDFR decreases due to its negative temperature coefficient. Since VDFR decreases, VOUT increases by the same amount, therefore VFLYBACKSET is proportional to VFLYBACK, VSET also remains unchanged. Since there is no change in VSET there is no change in duty cycle demand to bring VOUT back down to its target value. What needs to happen in the temperature compensated case is, when VOUT increases due to the negative temperature coefficient of VDFR, VSET needs to increase by an amount just sufficient to bring VOUT back to its target value. This is achieved by designing VSET with a positive temperature coefficient. Expressed mathematically as:

MAXREFDES1105 Equation 4

where:

δVDFR/δT is the diodes forward temperature coefficient

δVTC/δT = 1.85mV/°C

VTC = 0.55V is the voltage at the TC pin at +25°C

Rearranging the above expression gives:

MAXREFDES1105 Equation 5

The effect of adding the positive temperature coefficient current, ITC, to the current in RFB is equivalent to adding a positive temperature coefficient voltage in series with VDFR on the secondary side of value:

maxrefdes1105eq 6

Substituting from the previous expression, this becomes:

MAXREFDES1105 Equation 7

We can now substitute this expression into the expression for VOUT as follows:

MAXREFDES1105 Equation 8

and finally solve for RFB:


MAXREFDES1105 Equation 9

Values for RSET, VSET, and δVTC/δT can be obtained from the MAX17690 data sheet as follows:

RSET = 10KΩ
VSET = 1V
δVTC/δT = 1.85mV/°C

Values for VDFR and δVDFR/δT can be obtained from the output diode data sheet, and nSP is calculated when the flyback transformer is designed.

The value of RTC can then be calculated using the expression from earlier, restated below:

maxrefdes1105eq11

The calculated resistor values for RFB and RTC should always be verified experimentally and adjusted, if necessary, to achieve optimum performance over the required temperature range. Note that the reference design described in this document has only been verified at room temperature.

Finally, the internal temperature compensation circuitry requires a current proportional to VIN. RRIN should be chosen as approximately:


MAXREFDES1105 Equation 12

Setting the VFLYBACK Sampling Instant

The MAX17690 generates an internal voltage proportional to the on-time volt-second product. This enables the device to determine the correct sampling instant for VFLYBACK during the QP off-time. The RVCM resistor is used to scale this internal voltage to an acceptable internal voltage limit in the device.

Now that the principle difference between a traditional isolated flyback converter using optocoupler or auxiliary transformer winding feedback and the isolated no-opto flyback converter using the MAX17690 is understood, a practical design example can be illustrated. The converter design process can be divided into three parts: the power stage design, the setup of the MAX17690 no-opto flyback controller, and closing the control loop. This document is intended to complement the information contained in the MAX17690 data sheet.

The following design parameters are used throughout this document:

Set the closed-loop gain at fC equal to 1:
SYMBOL FUNCTION
VIN Input voltage
VUVLO Undervoltage turn-on threshold
VOVI Overvoltage turn-off threshold
tSS Soft-start time
VOUT Output voltage
ΔVO Steady-state output ripple voltage
IOUT Output current
POUT Output power
η(MAX) Target efficiency at maximum load
η(MIN) Target efficiency at minimum load
PIN Input power
fSW Switching frequency
D Duty cycle
nSP Secondary-primary turns ratio

 

Throughout the design procedure reference is made to the schematic. See the Design Resources section.

Part I: Designing the Power Components

Step 1: Calculate the Minimum Turns Ratio for the Flyback Transformer

The secondary-primary turns ratio, nSP, and the duty cycle, D, for the flyback converter are related by the flyback DC gain function as follows:

MAXREFDES1105 Equation 13

The converter’s absolute minimum input voltage is the undervoltage lockout threshold (VIN falling), which is programmed with a resistor-divider for the MAX17690. At this voltage and at maximum output power, D should be less than or equal to 66% (maximum duty cycle at which the MAX17690 can operate) to ensure reliable converter operation. For the current design, the undervoltage lockout threshold (VIN falling) occurs at 15.4V, so with D set at 66%, the absolute minimum turns ratio, nSP(MIN), for the flyback transformer is calculated as follows

nSP(MIN) = 0.17

This transformer turns ratio assumes that there are no DC voltage drops in the primary and/or secondary circuits. In practice, a larger transformer turns ratio must be chosen to account for these DC voltage drops. For the current design, a transformer turns ratio nSP = 0.25 was chosen.

Step 2: Estimate the Maximum and Minimum Duty Cycle Under Normal Operating Conditions

Normal input voltage operating conditions are defined as VIN(MIN) and VIN(MAX) on page 1. By using the flyback DC gain function again, the duty cycle is estimated as:


MAXREFDES1105 Equation 14

nSP and VOUT are fixed so clearly DMAX occurs when VIN is a minimum, i.e., at VIN(MIN). For the current design, VIN(MIN) = 18V, so:

DMAX = 0.53

The MAX17690 derives the current, ΔILP, in the primary magnetizing inductance by measuring the voltage, ΔVRCS, across the current-sense resistor (RCS) during the on-time of the primary-side MOSFET. So:

MAXREFDES1105 Equation 15

ΔILP is a maximum at DMAX and VIN(MIN) and a minimum at DMIN and VIN(MAX), so:

MAXREFDES1105 Equation 16

and

MAXREFDES1105 Equation 17

Solving these two equations:

MAXREFDES1105 Equation 18

where ΔVRCS(MIN) and ΔVRCS(MAX) correspond to the minimum current limit threshold (20mV) and the maximum current limit threshold (100mV) of the MAX17690, respectively. So, for VIN(MIN) = 18V, VIN(MAX) = 60V, and DMAX = 0.53, we have:

DMIN = 0.044

Step 3: Calculate the Maximum Allowable Switching Frequency

The isolated no-opto flyback topology requires the primary side MOSFET to constantly maintain switching, otherwise there is no way to sense the reflected secondary-side voltage at the drain of the primary-side MOSFET. The MAX17690 achieves this by having a critical minimum on-time, tON(CRIT), for which it drives the MOSFET. At a given switching frequency tON(MIN) corresponds to DMIN. From the MAX17690 data sheet, the critical minimum on-time tON(CRIT) for the NDRV pin is 235ns. We can therefore calculate the maximum allowable switching frequency to ensure that tON(MIN) > tON(CRIT) as follows:

MAXREFDES1105 Equation 19

Since DMIN is fixed by ΔVRCS(MIN), ΔVRCS(MAX), DMIN, VIN(MIN), and VIN(MAX), then tON(MIN) can be chosen arbitrarily larger than tON(CRIT) so that fSW is less than fSW(MAX). With tON(MIN) = 307ns the switching frequency as follows:

MAXREFDES1105 Equation 20

Note that the MAX17690 should always be operated in the 50kHz to 250kHz switching frequency range and tON(MIN) must be chosen accordingly to ensure that this constraint is met.

Step 4: Estimate the Primary Magnetizing Inductance

Maximum input power is given by:

MAXREFDES1105 Equation 21

For the discontinuous flyback converter all the energy stored in the primary magnetizing inductance, LP, during the MOSFET on-time is transferred to the output during the MOSFET off-time, i.e., the full power transfer occurs during one switching cycle. Therefore, because E = P x t, we have:

MAXREFDES1105 Equation 22

The maximum input energy must be stored in LP during the on-time of the MOSFET, so:

MAXREFDES1105 Equation 23

We also know that the peak current in LP, ΔILP(MAX) occurs at input voltage VIN(MIN) and MOSFET on-time tON(MAX), so:

MAXREFDES1105 Equation 24

and substituting:

MAXREFDES1105 Equation 25

Combining with the original P x t equation gives:

MAXREFDES1105 Equation 26

Finally, by rearranging we have an expression for the primary magnetizing inductance LP:

MAXREFDES1105 Equation 27

Estimating the power converter efficiency at 90% and with VIN(MIN) = 18V, DMAX = 0.53, VOUT = 5V, and fSW = 143.5kHz, then:

LP(MAX) ≈ 23.3μH

This inductance represents the maximum primary magnetizing inductance since it sets the current-limit threshold. Choosing a larger inductance sets the current-limit threshold at a lower value and could cause the converter to go into current limit at a value lower than IOUT, which would be undesirable. Assuming a ±10% tolerance for the primary magnetizing inductance gives:

LP ≈ 20μH ±10%

Step 5: Recalculate DMAX, DMIN, and tON(MIN) Based on the Selected Value for LP

Rearranging the LP equation in Step 4 gives an expression for DMAX as follows:

MAXREFDES1105 Equation 28

Referring to Step 2:

MAXREFDES1105 Equation 29

and:

MAXREFDES1105 Equation 30

Step 6: Calculate the Peak and RMS Currents in the Primary Winding of the Flyback Transformer

The peak primary winding current occurs at VIN(MIN) and DMAX according to the following equation:

MAXREFDES1105 Equation 31

The RMS primary winding current can be calculated from ΔILP(MAX) and DMAXas follows:

MAXREFDES1105 Equation 32

Step 7: Calculate the Peak and RMS Currents in the Secondary Winding of the Flyback Transformer

The peak current in the flyback transformer’s secondary-side winding can be established by considering that the entire energy transferred from the primary-side winding to the secondary-side winding is delivered to the load during one switching period. Again, since E = P x t:

MAXREFDES1105 Equation 33

Substituting:

MAXREFDES1105 Equation 34

And rearranging:

MAXREFDES1105 Equation 35

Current flows in the secondary-side winding of the flyback transformer during the time the secondary-side rectifying device is conducting. This conduction time, tON(SEC), is calculated using the inductor volt-second equation:

MAXREFDES1105 Equation 36

MAXREFDES1105 Equation 37

The maximum duty cycle of the secondary-side rectifying device, DS(MAX), can now be calculated:

MAXREFDES1105 Equation 38

Finally, the RMS secondary winding current can be calculated from ΔILS(MAX) and DS(MAX) as follows:

MAXREFDES1105 Equation 39

Step 8: Summarize the Flyback Transformer Specification

All the critical parameters for the flyback transformer have been calculated and are summarized below. Using these parameters, a suitable transformer can be designed.

PARAMETER SYMBOL VALUE
Primary Magnetizing Inductance LP 20μH ±10%
Primary Peak Current ΔILP(MAX) 2.78A
Primary RMS Current ILP(RMS) 1.07A
Turns Ratio (NS/NP) nSP 0.25
Secondary Peak Current ΔILS(MAX) 10.57A
Secondary RMS Current ILS(RMS) 4.83A

 

Step 9: Calculate Design Parameters for Secondary-Side Rectifying Device

Depending on the output voltage and current, a choice can be made for the secondary-side rectifying device. Generally, for output voltages above 12V at low currents (less than 1A), Schottky diodes are used, and for voltages less than 12V synchronous rectification (MOSFET) is used. The current design is a 5V/2A output converter, so we outline a procedure for selecting a suitable MOSFET for the synchronous switch.

Figure 4 shows a simplified schematic with the synchronous MOSFET, QS. The MAX17606 is a secondary-side synchronous driver and controller specifically designed for the isolated flyback topology operating in Discontinuous Conduction Mode (DCM) or Border Conduction Mode (BCM).

Figure 4. Simplified no-opto flyback schematic with synchronous rectification.

The important parameters to consider for the synchronous rectifying device are the same as those of a regular rectifying diode: peak instantaneous current, RMS current, voltage stress, and power losses. Since QS and LS are in series, they experience the same peak and RMS currents, so:

IQS(RMS) = ILS(RMS) = 4.83A

and

IQS(MAX) = ΔILS(MAX) = 10.57A

When QS is off, VIN reflected to the secondary side of the flyback transformer plus (VOUT +VQS(SAT)) is applied across the drain-source of QS, so:

VQS(MAX) = nSP x VIN(MAX) + VOUT + VQS(SAT)
= 0.25 x 60V + 5V + (4.83A x 6.1mΩ)
= 20V

QS has both conduction losses due to its RDS(ON) and switching losses. Allowing for reasonable design margin, we chose the BSZ040N04LSG from Infineon® for this design with the following specifications:

PARAMETER VALUE
Maximum Drain-Source Voltage 40V
Continuous Drain Current 40A
Drain-Source Resistance 6.1mΩ
Minimum VGS Threshold VGSTH 1.2V
Typical VGS Plateau VGSPL 3.0V
Maximum QG(T) 64nC
Typical QGD 4.9nC
Total Output Capacitance COSS 1100pF

 

The power losses in the QS can be approximated as follows:

PTOT = PCON + PCDS + PSW ≈ 189mW

where:

PCON is the loss due to IQS(RMS) flowing through the drain-source on resistance of QS:

PCON = I2QS(RMS) x RDS(ON) ≈ 142mW

PCDS is the loss due to the energy in the drain-source output capacitance being dissipated in QS at turn-on:

and PSW is the turn-on voltage-current transition loss that occurs as the drain-source voltage decreases and the drain current increases during the turn-on transition:

where IDRV is the maximum drive current capability of the MAX17606’s GATE output and IQS(t-ON) is the instantaneous current in QS at turn-on. IQS(t-ON) is equal to IQS(MAX).

Step 10: Calculate Design Parameters for Primary-Side MOSFET

The important parameters to consider for the primary-side MOSFET (QP) are peak instantaneous current, RMS current, voltage stress, and power losses. Because QP and LP are in series they experience the same peak and RMS currents, so from Step 6:

IQP(MAX) = ΔILP(MAX) ≈ 2.78A

and

IQP(RMS) = ILP(RMS) ≈ 1.07A

When QP turns off, VOUT reflected to the primary side of the flyback transformer plus VIN(MAX) is applied across the drain source of Q>sub>P. In addition, until QS starts to conduct, there is no path for the leakage inductance energy to flow through. This causes the drain-source voltage of QP to rise even further. The factor of (1.5) in the equation below represents this additional voltage rise; however, this factor can be higher or lower depending on the transformer and PCB leakage inductances:

Allowing for reasonable design margin, we chose the SIJ494DP from Vishay® was chosen for this design with the following specifications:

PARAMETER VALUE
Maximum Drain-Source Voltage 150V
Continuous Drain Current 34A
Drain-Source Resistance 27.2mΩ
Minimum VGS Threshold VGSTH 2.5V
Typical VGS Plateau VGSPL 5.2V
Maximum QG(T) 3.1nC
Typical QGD 6.7nC
Total Output Capacitance COSS 250pF

 

The power losses in the QP can be approximated as follows:

PTOT = PCON + PCDS + PSW ≈ 181mW

where:

PCON is the loss due to IQP(RMS) flowing through the drain-source on resistance of QP:

PCON = I2QP(RMS) x RDS(ON) ≈ 31mW

PCDS is the loss due to the energy in the drain-source output capacitance being dissipated in QP at turn-on:

MAXREFDES1105 Equation 40

And PSW is the turn-on voltage-current transition loss that occurs as the drain-source voltage decreases and the drain current increases during the turn-on transition:

MAXREFDES1105 Equation 41

where IDRV is the maximum drive current capability of the MAX17690’s NDRV output and IQP(t-ON) is the instantaneous current in QP at turn-on. Because the flyback converter is operating in DCM, IQP(t-ON) is zero and so is PSW.

Step 11: Select the RCD Snubber Components

Referring to Figure 5, when QP turns off, ILP charges the output capacitance, COSS, of QP. When the voltage across COSS exceeds the input voltage plus the reflected secondary to primary voltage, the secondary-side diode (or synchronous switch) turns on. Since the diode (or synchronous switch) is now on, the energy stored in the primary magnetizing inductance is transferred to the secondary; however, the energy stored in the leakage inductance will continue to charge COSS since there is nowhere else for it to go. Since the voltage across COSS is the same as the voltage across QP, if the energy stored in the leakage inductance charges COSS to a voltage level greater than the maximum allowable drain-source voltage of QP, the MOSFET fails.

Figure 5. RCD snubber circuit.

One way to avoid this situation arising is to add a suitable RCD snubber across the transformer’s primary winding. In Figure 5, the snubber is labeled RSN, CSN, and DSN. In this situation, when QP turns off, the voltage at Node A is:

VNODEA = VCSN + VIN

When the secondary-side diode (or synchronous switch)turns on, the voltage at Node B is:

MAXREFDES1105 Equation 45

So, the voltage across the leakage inductance is:

MAXREFDES1105 Equation 46

So:

MAXREFDES1105 Equation 47

The average power dissipated in the snubber network is:

MAXREFDES1105 Equation 48

Substituting ΔtSN into this expression we have:

MAXREFDES1105 Equation 49

The leakage inductance energy is dissipated in RSN, so from:

maxrefdes1105eq50

We can calculate the required RSN as follows:

maxrefdes1105eq51

Over one switching cycle we must have:

So, we can calculate the required CSN as follows:

Generally, ΔVCSN should be kept to approximately 10% to 30% of VCSN. Figure 6 illustrates VCSN, ΔISN, and ΔtSN. The voltage across the snubber capacitor, VCSN, should be selected so that:

VCSN < VDSMAX(QP) – VIN(MAX)

Choosing too large a value for VCSN causes the voltage on the QP drain to get too close to its maximum allowable drain-source voltage, while choosing too small a value results in higher power losses in the snubber resistor. A reasonable value should result in a maximum drain voltage on QPhat is approximately 75% of its maximum allowable value. The worst-case condition for the snubber circuit occurs at maximum output power when:

ΔISN = ΔILP(MAX)

Assuming the leakage inductance is 1.5% of the primary inductance, choosing VCSN = 52V and ΔVCSN = 5.2V, we get the following approximate values:

PSN = 275mW

RSN = 9.7kΩ

CSN = 7nF

Finally, we consider the snubber diode, DSN. This diode should have at least the same voltage rating as the MOSFET, QP. Although the average forward current is very low, it must have a peak repetitive current rating greater than ΔILP(MAX).

Figure 6. RCD snubber circuit waveforms.

Step 12: Calculate the Required Current-Sense Resistor

From Step 4 we have the maximum input power given by:

MAXREFDES1105 Equation 54

For the DCM flyback converter all the energy stored in the primary magnetizing inductance, LP, during the MOSFET on-time is transferred to the output during the MOSFET off-time, i.e., the full power transfer occurs during one switching cycle. Therefore, since E = P x t, we have:

MAXREFDES1105 Equation 55

The maximum input energy must be stored in LP during the primary-side MOSFET on-time, so:

MAXREFDES1105 Equation 56

Substituting the equations above:

MAXREFDES1105 Equation 57

and

MAXREFDES1105 Equation 58

From Step 2 we have:

MAXREFDES1105 Equation 59

so:

MAXREFDES1105 Equation 60

A standard 33mΩ resistor was chosen for RCS.

Step 13: Calculate and Select the Input Capacitors

Figure 7 shows a simplified schematic of the primary side of the flyback converter and the associated current waveforms. In steady-state operation, the converter draws a pulsed high-frequency current from the input capacitor, CIN. This current leads to a high-frequency ripple voltage across the capacitor according to the following expression:

 

Figure 7. Primary-side circuit and currents.

 

MAXREFDES1105 Equation 61

It is the ripple voltage arising from the amp second product through the input capacitor.

During the QP on-time interval from t0 to t1, the capacitor is supplying current to the primary inductance LP of the flyback transformer and its voltage is decreasing. During the QP off-time time interval from t1 to t2, no current is flowing in LP and current is being supplied to capacitor from the input voltage source. According to the charge balance law, the decrease in capacitor voltage during time t0 to t1 must equal the increase in capacitor voltage during time t1 to t2. So:

 

MAXREFDES1105 Equation 62

And finally, since:

MAXREFDES1105 Equation 63

we have:

MAXREFDES1105 Equation 64

For maximum high-frequency ripple voltage requirement ΔVCIN, we can now calculate the required minimum CIN.

There is high-frequency AC current flowing in CIN, as shown in the center waveform of Figure 7. The selected capacitor must be specified to tolerate the maximum RMS current, ICIN(RMS). From the simplified schematic:

ILP = IIN + ICIN

Therefore:

MAXREFDES1105 Equation 65

where:

MAXREFDES1105 Equation 66

and from Step 6:

MAXREFDES1105 Equation 67

so:

MAXREFDES1105 Equation 68

An additional high-frequency ripple voltage is present due to this RMS current flowing through the ESR of the capacitor. Ceramic capacitors are generally used for limiting high-frequency ripple due to their high AC current capability and low ESR.

In addition to using a ceramic capacitor for high-frequency input ripple-voltage control as described above, an electrolytic capacitor is sometimes inserted at the input of a flyback converter to limit the input voltage deviation when there is a rapid output load change. A 100% load change gives rise to an input current transient of:

MAXREFDES1105 Equation 69

 

During this transient, there is a voltage drop across any series stray inductance, LIN(STRAY), that exists between the input voltage source and the input capacitor of the power supply. So from:

MAXREFDES1105 Equation 70

we have:

MAXREFDES1105 Equation 71

We now have two values for CIN. One for input high-frequency ripple-voltage control:

MAXREFDES1105 Equation 72

and a second for transient input voltage control:

MAXREFDES1105 Equation 73

If CIN(ELE) > CIN(CER), both ceramic and electrolytic capacitors must be used at the input of the power supply and ΔVCIN should be limited to approximately 75mV to keep the AC current in the ESR of the electrolytic capacitor within acceptable limits. Otherwise, CIN(ELE) is not required. In this case, the value of CIN(CER) can be significantly reduced since there is no longer any requirement to limit ΔVCIN to less than 75mV. Based on the current design specification with LIN(STRAY) approximated at 50nH, we have:

CIN(CER) =32μF

and:

CIN(ELE) =4μF

Since CIN(ELE) < CIN(CER), an electrolytic capacitor is not required. We can now recalculate CIN(CER) based on a ΔVCIN = 600mV:

CIN(CER) ≈ 4μF

Allowing for a ±10% capacitor tolerance and a further reduction of capacitance of 75% due to the DC bias effect (operating an 80V ceramic capacitor at 50V), our final nominal value of input capacitance required is:

MAXREFDES1105 Equation 74

This is achieved by using four 4.7μF ceramic capacitor (GRM32ER71K475KE14 from Murata®). The AC current in the capacitor is:

ICIN(RMS) ≈ 0.21ARMS

which is well within specification for the selected capacitor.

This is achieved by using four 4.7μF ceramic capacitor (GRM32ER71K475KE14 from Murata®). The AC current in the capacitor is:

which is well within specification for the selected capacitor.

Step 14: Calculate and Select the Output Capacitor

High-frequency ripple voltage requirements are also used to determine the value of the output capacitor in a flyback converter. Figure 8 shows a simplified schematic of the secondary side of the flyback converter and the associated current waveforms.

In steady-state operation, the load draws a DC current from the secondary side of the flyback converter. By examining the secondary current waveforms, we see that CO is supplying the full output current IOUT to the load during the time interval from t2 to t3. During this time interval, the voltage across CO decreases. At time t3, QP has just turned off and the secondary rectifying diode DFR (or the secondary synchronous switch QS) starts to conduct supplying current to the load and to CO. The charging and discharging of CO leads to a high-frequency ripple voltage at the output according to the following expression:

MAXREFDES1105 Equation 75

Again, as with the input capacitor, this is the ripple voltage arising from the amp second product through the output capacitor.

By the capacitor charge balance law, the decrease in capacitor voltage during time t2 to t3 must equal the increase in capacitor voltage during time t1 to t2. When the capacitor is discharging, we have:

MAXREFDES1105 Equation 76

Finally, since:

MAXREFDES1105 Equation 77

We have:

MAXREFDES1105 Equation 79

For maximum high-frequency ripple voltage requirement ΔVCO, we can now calculate the required minimum CO.

CO ≈ 167.6μF

As with the input capacitor, an additional high-frequency ripple voltage occurs at the output due to the output capacitor’s ESR and can be minimized by choosing a capacitor with low ESR.

Also, as with the input capacitor, there is high-frequency AC current flowing in CO as shown in the center waveform of Figure 8. The selected capacitor must be specified to tolerate this maximum RMS current, ICO(RMS). From the simplified schematic:

ILS = IOUT + ICO

Therefore:

MAXREFDES1105 Equation 79

where:

IOUT(RMS) = IOUT

and from Step 7:

MAXREFDES1105 Equation 80

so:

MAXREFDES1105 Equation 81

If we allow for a ±20% capacitor tolerance and a further reduction of capacitance of 57% due to the DC bias effect (operating a 6.3V ceramic capacitor at 5V), our final nominal value is:

MAXREFDES1105 Equation 82

We can achieve this by placing five 100μF ceramic capacitors (GRM32ER60J107ME20 from Murata) in parallel. The minimum output capacitance using the above combination is 172μF. The AC current in each capacitor is:

MAXREFDES1105 Equation 83

which is well within specification for the selected capacitor.

Figure 8. Secondary-side circuit and currents.

Step 15: Summarize the Power Component Design

A first pass at calculating the power components in the no-opto flyback converter using MAX17690 has been completed. Referring to the schematic, a summary of the power components is listed below:

POWER
COMPONENT
QTY DESCRIPTION
Flyback
Transformer
1 PRI. INDUCTANCE = 20μH
SEC-PRI TURNS RATIO = 0.25
PEAK. PRI CURRENT = 2.78A
PRI. RMS CURRENT = 1.07A
PEAK SEC. CURRENT = 10.57A
SEC. RMS CURRENT = 4.83A
SWITCHING FREQ. = 143.5kHz
Input
Capacitor
4 CAPACITOR; SMT (1210);
CERAMIC CHIP
4.7μF; 80V; 10%; X7R
Murata GRM32ER71K475KE14
Output
Capacitors
5 CAPACITOR; SMT (1210);
CERAMIC CHIP
100μF; 6.3V; 20%; X5R
Murata GRM32ER60J107ME20
Primary
MOSFET
1 MOSFET; NCH; I-(36.8A); V-(150V)
Vishay SIJ494DP
Synchronous
MOSFET
1 MOSFET; NCH; I-(40A); V-(40V)
Vishay BSZ040N04LSG

 

Part II: Setting Up the MAX17690 No-Opto Flyback Controller

Step 16: Setting Up the Switching Frequency

The MAX17690 can operate at switching frequencies between 50kHz and 250kHz (subject to the considerations in Step 3). A lower switching frequency optimizes the design for efficiency, whereas increasing the switching frequency allows for smaller inductive and capacitive components sizes and costs. A switching frequency of 143.5kHz was chosen in Step 3. R9 sets the switching frequency according to the following expression:

MAXREFDES1105 Equation 84

where R9 is in kΩ and fSW is in Hz.

Step 17: Setting Up the Soft-Start Time

The capacitor C6 connected between the SS pin and SGND programs the soft-start time. A precision internal 5μA current source charges the soft-start capacitor C6. During the soft-start time, the voltage at the SS pin is used as a reference for the internal error amplifier during startup. The soft-start feature reduces inrush current during startup. Since the reference voltage for the internal error amplifier is ramping up linearly, so too is the output voltage during soft-start. The soft-start capacitor is chosen based on the required soft-start time (10ms) as follows:

C6 = 5 x tSS ≈ 50nF

where C6 is in nF and tSS is in ms. A standard 47nF capacitor was chosen.

Step 18: Setting Up the UVLO and OVI Resistors

A resistor-divider network of R1, R3, and R2 from VIN to SGND sets the input undervoltage lockout threshold and the output overvoltage inhibit threshold. The MAX17690 does not commence its startup operation until the voltage on the EN/UVLO pin (R3/R2 node) exceeds 1.215V (typ). When the voltage on the OVI pin (R1/R3 node) exceeds 1.215V (typ), the MAX17690 stops switching, thus inhibiting the output. Both pins have hysteresis built in to avoid unstable turn-on/turn-off at the UVLO/EN and OVI thresholds. After the device is enabled, if the voltage on the UVLO/EN pin drops below 1.1V (typ), the controller turns off; after the device is OVI inhibited, it turns back on when the voltage at the OVI pin drops below 1.1V (typ). Whenever the controller turns on, it goes through the soft-start sequence. For the current design R1 = 10kΩ, R2 = 464kΩ, and R3 = 25.5kΩ give rise to an UVLO/EN threshold of 17.1V and an OVI threshold of 60.7V.

Step 19: Placing Decoupling Capacitors on VIN and INTVCC Pins

As previously discussed, the MAX17690 no-opto flyback controller compares the voltage VFLYBACK to VIN. This voltage difference is converted to a proportional current that flows in R5. The voltage across R5 is sampled and compared to an internal reference by the error amplifier. The output of the error amplifier is used to regulate the output voltage. The VIN pin should be directly connected to the input voltage supply. For robust and accurate operation, a ceramic capacitor (C2 = 1μF) should be placed between VIN and SGND as close as possible to the IC.

VIN powers the MAX17690’s internal low dropout regulator. The LDO’s regulated output is connected to the INTVCC pin. A ceramic capacitor (C3 = 2.2μF min) should be connected between the INTVCC and PGND pins for the stable operation over the full temperature range. Place this capacitor as close as possible to the IC.

Step 20: Setting Up the Feedback Components

RSET (R5), RFB (R4, R18), RRIN (R8), RVCM (R6), and RTC (R7) are critically important to achieving optimum output voltage regulation across all specified line, load and temperature ranges.

RSET resistor (R5): This resistor value is optimized based on the IC’s internal voltage to current amplifier and should not be changed.

R5 = RSET = 10kΩ

RFB resistor (R4, R18): The feedback resistor is calculated according to the following equation:

MAXREFDES1105 Equation 85

Since we are using a synchronous MOSFET for rectification on the secondary side, we can assume that δVDFR/δT = 0, so:

MAXREFDES1105 Equation 86

From the MAX17690 data sheet, VSET = 1V. The two resistors R4 = 182kΩ and R18 = 20kΩ form RFB. Using one high value resistor and one low value resistor in series allows slight adjustment to the series resistance combination so that the output voltage can be fine-tuned to its required value, if necessary.

RRIN resistor (R8): The internal temperature compensation circuitry requires a current proportional to VIN. RRIN establishes this current and is calculated according to the following equation:

RRIN ≈ 0.6 x RFB

RVCM resistor (R6): The MAX17690 generates an internal voltage proportional to the on-time volt-second product. This enables the device to determine the correct sampling instant for VFLYBACK during the QP off-time. Resistor R6 is used to scale this internal voltage to an acceptable internal voltage limit in the device. To calculate the resistor, we must first calculate a scaling constant as follows:

MAXREFDES1105 Equation 87

After KC is calculated, the R6 value can be selected from the table below by choosing the resistance value that corresponds to the next largest KC.

KC R6
640
320 75kΩ
160 121kΩ
80 220Ω
40 Open

 

In the present case, R6 = 121kΩ.

RTC resistor (R7): The value of RTC can then be calculated using the previous expression, restated below:

MAXREFDES1105 Equation 88

Since we are using a synchronous MOSFET for secondary-side rectification, we can assume that the temperature coefficient δVDFR/δT is zero so RTC should be infinite (i.e., open circuit).

This completes the setup of the MAX17690 no-opto flyback controller.

Part III: Closing the Control Loop

Step 21: Determine the Required Bandwidth

The bandwidth of the control loop determines how quickly the converter can respond to changes at its input and output. If we have a step change in output current, the voltage across the output capacitor decreases as shown in Figure 9.

Figure 9. Output load step response.

The control loop detects this reduction in output voltage and increases the duty cycle of QP to supply more current to the output capacitor. The amount of time required by the control loop to increase the duty cycle from its minimum value to its maximum value is the response time, τRES, of the control loop. For the MAX17690 we have:

MAXREFDES1105 Equation 89

where fC is the bandwidth of the power converter. If we apply a switching load step of amplitude ΔISTEP, at a frequency of (1/τRES) and a 50% duty cycle then, to limit the output voltage deviation to ±ΔVOUT(STEP) we must have a minimum output capacitance of:

MAXREFDES1105 Equation 90

Combining the two previous equations, we have:

MAXREFDES1105 Equation 91

It is normal to specify ΔVOUT(STEP) for a load step from 50% to 100% of the maximum output current. We have already calculated CO(MIN) = 172μF in Step 14, fSW = 143.5kHz, so based on a 3% maximum ΔVOUT(STEP):

fC ≈ 7.5kHz

Step 22: Calculate the Loop Compensation

The MAX17690 uses peak current-mode control and an internal transconductance error amplifier to compensate the control loop. The control loop is modeled, as shown in Figure 10, by a power modulator transfer function GMOD(S) an output-voltage feedback transfer function GFB(S) and an error amplifier transfer function GEA(S).

Figure 10. Simplified model of control loop.

The power modulator has a pole located at fP(MOD) determined by the impedance of the output capacitor CO and the load impedance RL. It also has a zero at fZ(MOD) determined by the impedance of CO and the ESR of CO. The DC gain of the power modulator is determined by the peak primary current ΔILP and the current-sense resistor RCS. So:

MAXREFDES1105 Equation 92
MAXREFDES1105 Equation 93

and:

MAXREFDES1105 Equation 94

The output voltage feedback transfer function GFB(S) is independent of frequency and has a DC gain determined by VIN, VFLYBACK, and VSET as follows:

MAXREFDES1105 Equation 95

The MAX17690’s transconductance error amplifier should be set up in a configuration to compensate for the pole at fP(MOD) and the zero at fZ(MOD) of the modulator. This can be achieved by a Type II transconductance error amplifier compensation shown in Figure 11.

 

Figure 11. Type II compensation for OTA.

This compensation scheme type has a low frequency pole at fP-LF(EA) due to the very large output resistance RO (30MΩ to 50MΩ) of the operational transconductance amplifier (OTA). It has a zero at fZ(EA) determined by CZ and RZ of the compensation network, and it has an additional pole at fP(EA) determined by CP and RZ of the compensation network. So:

MAXREFDES1105 Equation 96

and

MAXREFDES1105 Equation 97

To achieve stable operation, we must ensure that:

MAXREFDES1105 Equation 97

Set the closed-loop gain at fC equal to 1:

GMOD(fC) x GFB(fC) x GEA(fC) = 1

Place the zero in the error amplifier network at the same frequency as the pole in the power modulator transfer function:

MAXREFDES1105 Equation 100

The frequency fZ(MOD) at which the zero occurs in the power modulator transfer function depends on the ESR of CO. If ceramic capacitors are used for CO, fZ(MOD) will be generally much higher than fC. However, if the ESR of CO is large, fZ(MOD)) could be lower than fC. This is a very important point since both the gain of the power modulator at fC, and the gain of the error amplifier at fCdepend on whether fZ(MOD) is greater than or less than fC. This is illustrated in Figure 12.

Figure 12. Simplified gain plot.

By examining the gain plots in Figure 12, we see that for fZ(MOD) > fC:

MAXREFDES1105 Equation 101

and for fZ(MOD) < fC:

MAXREFDES1105 Equation 102

For the current design, we have:

MAXREFDES1105 Equation 103

and

MAXREFDES1105 Equation 104

Since fZ(MOD) > fC:

MAXREFDES1105 Equation 105

and since GFB is independent of frequency, we have:

MAXREFDES1105 Equation 106

We can now set the closed-loop gain equal to 1 as follows:

MAXREFDES1105 Equation 107

Rearranging we can calculate:

MAXREFDES1105 Equation 108

Substituting ΔILP from Step 12:

MAXREFDES1105 Equation 109

Finally, we can calculate the remaining components, CZ and CP, in the error amplifier compensation network as follows:

MAXREFDES1105 Equation 110

支持与培训

搜索我们的知识库,获取技术问题答案。我们专门的应用工程师团队也会随时为您解答技术问题。