faqs
Frequently Asked Question
What is the host interface used for?
The host interface is used for configuration of the ADV202/212 and for transfering compressed data to/from the ADV202/212.
In Host Interface/Pixel Interface [HIPI] mode, it is also used for uncompressed pixel input/output.
Refer to AN-790 for more information on the function of the host interface.