Frequently Asked Question
What evaluation systems are available for the ADV202/212?
1. ADV202/212 ASD P160 EB is an ADV202/ADV212 daugther card designed for a Memec Xilinx Spartan 3SXLC motherboard.
Input: analog NTSC or PAL in CVBS or S-Video format
Output: analog NTSC or PAL in CVBS or S-Video format The boards can be used in a stand-alone application. In this case modes are controlled over DIP switches.
In PC control mode access to registers, parameter settings is possible. The board is controlled over a USB connection to a PC using the Hyperterminal interface.
In Developer Mode, access to source code is available.
Interface is Xilinx EDK and ISE over a JTAG connector.
2. The ADV202/212-HD-EB is a 32-bit PCI card.
Input : 1080i or 720p SDI video
Output: 1080i or 720p SDI video One card can be used for either encode or decode. Two cards can be used in the same PC for a encode-decode pass-thru demonstration.
The card is mainly intended for evaluation JPEG2000 compression of High Definition video.