faqs
Frequently Asked Question
Is the ADV202/212 output compatible with any JPEG2000 software codecs?
Yes. The ADV202/212 compressed output, if .j2c or jp2 format, is fully compatible to the ISO/IEC 15444-1 JPEG2000 standard.
Note, the ADV202/212 will insert a 16-byte header at the start of each codestream. This header has to be removed in order for other JPEG2000 codecs to recognize the codestream correctly.
Commonly used with the ADV202/212, Kakadu is a free of charge software codec from www.kakadusoftware.com