Abstract 
This application note describes the hardware and software differences between the Dallas Semiconductor DS21Q42 and the DS21Q41B quad port framer devices.  The DS21Q42 enhanced quad T1 framer offers a broader feature set while retaining the original features of the DS21Q41B.  As such, the designer must decide on what changes need to be made in software and hardware when migrating to the DS21Q42 from the DS21Q41B quad T1 framer.  Any designer who is thinking of upgrading an existing design to use the DS21Q42 should read this application note.  The application note contains detailed information for software migration such as: register location changes, how individual functions have changed from the DS21Q41B to the DS21Q42, and which new functions are available on the DS21Q42.  It also covers migration for the hardware interface and covers new functions that are available in the DS21Q42.  In the end, the designer should have enough information to easily migrate an existing design which uses the DS21Q41B to the DS21Q42 device.
                 
            Introduction
This application note highlights the differences between the DS21Q42 and the DS21Q41B Quad T1
Framers. The DS21Q42 is a superset of the DS21Q41B. The DS21Q42 is only offered in a 3.3 volt
version with 5 volt tolerant I/O. All of the original features of the DS21Q41B have been retained and software created for the DS21Q41B is transferable to the DS21Q42 with minimal effort.
Additional Functionality
    
        
            | New Features | Data Sheet Section | 
        
            | Framer Mode Select (FMS) hardware pin provides DS21Q41B emulation mode | 1 | 
        
            | 8.192 MHz clock synthesizer | 1 & 3 | 
        
            | CRC6 support for Japanese standard | 6 | 
        
            | Expanded receive and transmit elastic store reset functions | 6 | 
        
            | Device ID register | 6 | 
        
            | RCL, RLOS, RRA, and RAIS alarms now interrupt on change of state | 7 | 
        
            | Loss of Receive clock indication | 7 | 
        
            | Ability to monitor one DS0 channel in both the transmit and receive paths | 9 | 
        
            | Additional hardware signaling capability including: 
 
 
                Receive signaling re-insertion to a backplane multiframe sync
                Signaling freezing
                 | 10 | 
        
            | Per-channel code insertion in both transmit and receive paths | 11 | 
        
            | Per-channel loopback | 11 | 
        
            | Ability to pass the F-Bit position through the elastic stores in the 2.048 MHz backplane mode | 13 | 
        
            | HDLC controller 
 
 
                64-byte buffers
                Configurable for FDL or DS0 access
                 | 14 | 
        
            | Programmable inband code generation and detection | 16 | 
        
            | Interleaved PCM bus operation | 18 | 
        
            | TAG support | 19 | 
        
            | 3.3V operation with 5V tolerant I/O | 21 | 
    
Changes in Register Definitions
When implementing the new features of the DS21Q42, a priority was placed on preserving the
DS21Q41B's register map to facilitate code migration from existing DS21Q41B designs. This section highlights register additions and differences found in the DS21Q42.
Register Map Comparison
    
        
            | Address | R/W | DS21Q42 Register Name | DS21Q41B Register Name | 
        
            | 00 | R/W | FDL Control | Not Present | 
        
            | 01 | R/W | FDL Status | Not Present | 
        
            | 02 | R/W | FDL Interrupt Mask | Not Present | 
        
            | 03 | R/W | Receive Performance Report Message | Not Present | 
        
            | 04 | R/W | Receive Bit Oriented Code | Not Present | 
        
            | 05 | R | Receive FDL FIFO | Not Present | 
        
            | 06 | R/W | Transmit Performance Report Message | Not Present | 
        
            | 07 | R/W | Transmit Bit Oriented Code | Not Present | 
        
            | 08 | W | Transmit FDL FIFO | Not Present | 
        
            | 09 | R/W | Test Register | Not Present | 
        
            | 0A | R/W | Common Control 7 | Not Present | 
        
            | 0B | — | Not Present | Not Present | 
        
            | 0C | — | Not Present | Not Present | 
        
            | 0D | — | Not Present | Not Present | 
        
            | 0E | — | Not Present | Not Present | 
        
            | 0F | R | Device ID | Not Present | 
        
            | 10 | R/W | Receive Information 3 | Not Present | 
        
            | 11 | R/W | Common Control 4 | Not Present | 
        
            | 12 | R/W | In-Band Code Control | Not Present | 
        
            | 13 | R/W | Transmit Code Definition | Not Present | 
        
            | 14 | R/W | Receive Up Code Definition | Not Present | 
        
            | 15 | R/W | Receive Down Code Definition | Not Present | 
        
            | 16 | R/W | Transmit Channel Control 1 | Not Present | 
        
            | 17 | R/W | Transmit Channel Control 2 | Not Present | 
        
            | 18 | R/W | Transmit Channel Control 3 | Not Present | 
        
            | 19 | R/W | Common Control 5 | Not Present | 
        
            | 1A | R | Transmit DS0 Monitor | Not Present | 
        
            | 1B | R/W | Receive Channel Control 1 | Not Present | 
        
            | 1C | R/W | Receive Channel Control 2 | Not Present | 
        
            | 1D | R/W | Receive Channel Control 3 | Not Present | 
        
            | 1E | R/W | Common Control 6 | Not Present | 
        
            | 1F | R | Receive DS0 Monitor | Not Present | 
        
            | 20 | R/W | Status 1 | Same | 
        
            | 21 | R/W | Status 2 | Bit Difference | 
        
            | 22 | R/W | Receive Information 1 | Same | 
        
            | 23 | R | Line Code Violation Count 1 | Same | 
        
            | 24 | R | Line Code Violation Count 2 | Same | 
        
            | 25 | R | Path Code Violation Count 1 | Same | 
        
            | 26 | R | Path Code Violation Count 2 | Same | 
        
            | 27 | R | Multiframe Out of Sync Count 2 | Same | 
        
            | 28 | R | Receive FDL Register | Same | 
        
            | 29 | R/W | Receive FDL Match 1 | Same | 
        
            | 2A | R/W | Receive FDL Match 2 | Same | 
        
            | 2B | R/W | Receive Control 1 | Same | 
        
            | 2C | R/W | Receive Control 2 | Same | 
        
            | 2D | R/W | Receive Mark 1 | Same | 
        
            | 2E | R/W | Receive Mark 2 | Same | 
        
            | 2F | R/W | Receive Mark 3 | Same | 
        
            | 30 | R/W | Common Control 3 | Bit Difference | 
        
            | 31 | R/W | Receive Information 2 | Same | 
        
            | 32 | R/W | Transmit Channel Blocking 1 | Same | 
        
            | 33 | R/W | Transmit Channel Blocking 2 | Same | 
        
            | 34 | R/W | Transmit Channel Blocking 3 | Same | 
        
            | 35 | R/W | Transmit Control 1 | Same | 
        
            | 36 | R/W | Transmit Control 2 | Same | 
        
            | 37 | R/W | Common Control 1 | Same | 
        
            | 38 | R/W | Common Control 2 | Same | 
        
            | 39 | R/W | Transmit Transparency 1 | Same | 
        
            | 3A | R/W | Transmit Transparency 2 | Same | 
        
            | 3B | R/W | Transmit Transparency 3 | Same | 
        
            | 3C | R/W | Transmit Idle 1 | Same | 
        
            | 3D | R/W | Transmit Idle 2 | Same | 
        
            | 3E | R/W | Transmit Idle 3 | Same | 
        
            | 3F | R/W | Transmit Idle Definition | Same | 
        
            | 40 | R/W | Transmit Channel 9 | Not Present | 
        
            | 41 | R/W | Transmit Channel 10 | Not Present | 
        
            | 42 | R/W | Transmit Channel 11 | Not Present | 
        
            | 43 | R/W | Transmit Channel 12 | Not Present | 
        
            | 44 | R/W | Transmit Channel 13 | Not Present | 
        
            | 45 | R/W | Transmit Channel 14 | Not Present | 
        
            | 46 | R/W | Transmit Channel 15 | Not Present | 
        
            | 47 | R/W | Transmit Channel 16 | Not Present | 
        
            | 48 | R/W | Transmit Channel 17 | Not Present | 
        
            | 49 | R/W | Transmit Channel 18 | Not Present | 
        
            | 4A | R/W | Transmit Channel 19 | Not Present | 
        
            | 4B | R/W | Transmit Channel 20 | Not Present | 
        
            | 4C | R/W | Transmit Channel 21 | Not Present | 
        
            | 4D | R/W | Transmit Channel 22 | Not Present | 
        
            | 4E | R/W | Transmit Channel 23 | Not Present | 
        
            | 4F | R/W | Transmit Channel 24 | Not Present | 
        
            | 50 | R/W | Transmit Channel 1 | Not Present | 
        
            | 51 | R/W | Transmit Channel 2 | Not Present | 
        
            | 52 | R/W | Transmit Channel 3 | Not Present | 
        
            | 53 | R/W | Transmit Channel 4 | Not Present | 
        
            | 54 | R/W | Transmit Channel 5 | Not Present | 
        
            | 55 | R/W | Transmit Channel 6 | Not Present | 
        
            | 56 | R/W | Transmit Channel 7 | Not Present | 
        
            | 57 | R/W | Transmit Channel 8 | Not Present | 
        
            | 58 | R/W | Receive Channel 17 | Not Present | 
        
            | 59 | R/W | Receive Channel 18 | Not Present | 
        
            | 5A | R/W | Receive Channel 19 | Not Present | 
        
            | 5B | R/W | Receive Channel 20 | Not Present | 
        
            | 5C | R/W | Receive Channel 21 | Not Present | 
        
            | 5D | R/W | Receive Channel 22 | Not Present | 
        
            | 5E | R/W | Receive Channel 23 | Not Present | 
        
            | 5F | RW | Receive Channel 24 | Not Present | 
        
            | 60 | R | Receive Signaling 1 | Same | 
        
            | 61 | R | Receive Signaling 2 | Same | 
        
            | 62 | R | Receive Signaling 3 | Same | 
        
            | 63 | R | Receive Signaling 4 | Same | 
        
            | 64 | R | Receive Signaling 5 | Same | 
        
            | 65 | R | Receive Signaling 6 | Same | 
        
            | 66 | R | Receive Signaling 7 | Same | 
        
            | 67 | R | Receive Signaling 8 | Same | 
        
            | 68 | R | Receive Signaling 9 | Same | 
        
            | 69 | R | Receive Signaling 10 | Same | 
        
            | 6A | R | Receive Signaling 11 | Same | 
        
            | 6B | R | Receive Signaling 12 | Same | 
        
            | 6C | R/W | Receive Channel Blocking 1 | Same | 
        
            | 6D | R/W | Receive Channel Blocking 2 | Same | 
        
            | 6E | R/W | Receive Channel Blocking 3 | Same | 
        
            | 6F | R/W | Interrupt Mask 2 | Bit Difference | 
        
            | 70 | R/W | Transmit Signaling 1 | Same | 
        
            | 71 | R/W | Transmit Signaling 2 | Same | 
        
            | 72 | R/W | Transmit Signaling 3 | Same | 
        
            | 73 | R/W | Transmit Signaling 4 | Same | 
        
            | 74 | R/W | Transmit Signaling 5 | Same | 
        
            | 75 | R/W | Transmit Signaling 6 | Same | 
        
            | 76 | R/W | Transmit Signaling 7 | Same | 
        
            | 77 | R/W | Transmit Signaling 8 | Same | 
        
            | 78 | R/W | Transmit Signaling 9 | Same | 
        
            | 79 | R/W | Transmit Signaling 10 | Same | 
        
            | 7A | R/W | Transmit Signaling 11 | Same | 
        
            | 7B | R/W | Transmit Signaling 12 | Same | 
        
            | 7C | — | Not Present | Test Register | 
        
            | 7D | R/W | Test Register | Test Register | 
        
            | 7E | R/W | Transmit FDL Register | Same | 
        
            | 7F | R/W | Interrupt Mask Register 1 | Same | 
        
            | 80 | R/W | Receive Channel 1 | Not Present | 
        
            | 81 | R/W | Receive Channel 2 | Not Present | 
        
            | 82 | R/W | Receive Channel 3 | Not Present | 
        
            | 83 | R/W | Receive Channel 4 | Not Present | 
        
            | 84 | R/W | Receive Channel 5 | Not Present | 
        
            | 85 | R/W | Receive Channel 6 | Not Present | 
        
            | 86 | R/W | Receive Channel 7 | Not Present | 
        
            | 87 | R/W | Receive Channel 8 | Not Present | 
        
            | 88 | R/W | Receive Channel 9 | Not Present | 
        
            | 89 | R/W | Receive Channel 10 | Not Present | 
        
            | 8A | R/W | Receive Channel 11 | Not Present | 
        
            | 8B | R/W | Receive Channel 12 | Not Present | 
        
            | 8C | R/W | Receive Channel 13 | Not Present | 
        
            | 8D | R/W | Receive Channel 14 | Not Present | 
        
            | 8E | R/W | Receive Channel 15 | Not Present | 
        
            | 8F | R/W | Receive Channel 16 | Not Present | 
        
            | 90 | R/W | Receive HDLC DS0 Control Register 1 | Not Present | 
        
            | 91 | R/W | Receive HDLC DS0 Control Register 2 | Not Present | 
        
            | 92 | R/W | Transmit HDLC DS0 Control Register 1 | Not Present | 
        
            | 93 | R/W | Transmit HDLC DS0 Control Register 2 | Not Present | 
        
            | 94 | R/W | Interleave Bus Operation Register | Not Present | 
        
            | 95 | — | Not Present | Not Present | 
        
            | 96 | — | Not Present | Not Present | 
        
            | 97 | — | Not Present | Not Present | 
        
            | 98 | — | Not Present | Not Present | 
        
            | 99 | — | Not Present | Not Present | 
        
            | 9A | — | Not Present | Not Present | 
        
            | 9B | — | Not Present | Not Present | 
        
            | 9C | — | Not Present | Not Present | 
        
            | 9D | — | Not Present | Not Present | 
        
            | 9E | — | Not Present | Not Present | 
        
            | 9F | — | Not Present | Not Present | 
    
NOTE: Test Registers 1 and 2 are used only by the factory; these registers must be cleared (set to all zeros) on power up initialization to insure proper operation.
New Feature Register Usage
Highlights specific registers containing bit locations related to new features. Each item can be found in the
data sheet under the listed sections.
    Device Identification (section 6)
    
        
            | Register | Description | 
        
            | IDR | Device Identification Register | 
    
    Expanded Elastic Stores Reset Functions (section 6)
    
        
            | Register | Description | 
        
            | CCR5 | Common Control 5 | 
        
            | CCR6 | Common Control 6 | 
    
    Loss of Receive Clock (section 6)
    
        
            | Register | Description | 
        
            | RIR3 | Receive Information Register 3 | 
    
    Japanese CRC6 Mode (section 6)
    
        
            | Register | Description | 
        
            | CCR5 | Common Control 5 | 
        
            | CCR6 | Common Control 6 | 
    
    Interrupt on Change of State for RCL, RLOS, RRA, RAIS (section 7)
    
        
            | Register | Description | 
        
            | SR2 | Status Register 2 | 
        
            | IMR2 | Interrupt Mask Register 2 | 
    
    DS0 Monitoring (section 9)
    
        
            | Register | Description | 
        
            | CCR5 | Common Control 5 | 
        
            | CCR6 | Common Control 6 | 
        
            | TDS0M | Transmit DS0 Monitor | 
        
            | RDS0M | Receive DS0 Monitor | 
    
    Hardware Based Signaling (section 10.2)
    
        
            | Register | Description | 
        
            | CCR4 | Common Control 4 | 
    
    Per Channel Loopback (section 11)
    
        
            | Register | Description | 
        
            | CCR4 | Common Control 4 | 
        
            | TIR1-TIR3 | Transmit Idle | 
    
    Per Channel Code Generation (section 11)
    
        
            | Register | Description | 
        
            | TCC1-TCC3 | Transmit Channel Control 1-3 | 
        
            | TC1-TC24 | Transmit Channels 1-24 Codes | 
        
            | RCC1-RCC3 | Receive Channel Control 1-3 | 
        
            | RC1-RC24 | Receive Channels 1-24 Codes | 
    
    On Chip HDLC & BOC Controller For FDL Support (section 15.1)
    
        
            | Register | Description | 
        
            | TCR1 | Transmit Control Register 1 | 
        
            | FDLC | FDL Control | 
        
            | FDLS | FDL Status | 
        
            | FIMR | FDL Interrupt Mask | 
        
            | RPRM | Receive Performance Report Message | 
        
            | RBOC | Receive Bit Oriented Message | 
        
            | RFFR | Receive FDL FIFO | 
        
            | TPRM | Transmit Performance Report Message | 
        
            | TBOC | Transmit Bit Oriented Code | 
        
            | TFFR | Transmit FDL FIFO | 
        
            | RDC1 | Receive HDLC DS0 Control Register 1 | 
        
            | RDC2 | Receive HDLC DS0 Control Register 2 | 
        
            | TDC1 | Transmit HDLC DS0 Control Register 1 | 
        
            | TDC2 | Transmit HDLC DS0 Control Register 2 | 
    
    Programmable In-Band Code Generation & Detection (section 16)
    
        
            | Register | Description | 
        
            | CCR3 | Common Control 3 | 
        
            | IBCC | In-Band Code Control | 
        
            | TCD | Transmit Code Definition | 
        
            | RUPCD | Receive Up Code Definition | 
        
            | RDNCD | Receive Down Code Definition | 
        
            | SR1 | Status Register 1 | 
    
    Interleave Bus Operation (section 18)
    
        
            | Register | Description | 
        
            | IBO | Interleave Bus Operation Register | 
    
Bit Assignment Changes within Existing Registers
Highlights bit locations in the DS21Q42 which have changed from the DS21Q41B.
    
        
            | Register | Bit # | DS21Q42 Function
 | DS21Q41B Function
 | 
        
            | CCR3 | 0 | TESMDM | Not Assigned | 
        
            | CCR3 | 1 | TLOOP | TLU | 
        
            | CCR3 | 2 | ECUS | TLD | 
        
            |  |  |  |  | 
        
            | CCR3 | 6 | TCLKSRC | ESR | 
        
            | CCR3 | 7 | RESMDM | ESMDM | 
        
            |  |  |  |  | 
        
            | SR2 | 0 | RSC | LORC | 
        
            |  |  |  |  | 
        
            | IMR2 | 0 | RSC | LORC | 
    
Register Bit Moves
    
        
            | Register | DS21Q42 Function | DS21Q41B Function | 
        
            | ESR | CCR6 & CCR7 | CCR3 | 
        
            | LORC | RIR3.4 | SR2.0 | 
    
Changes in Device Pin Out
Package types
The DS21Q42 is offered in the same package as the DS21Q41B (128-pin 20 × 20 × 1.4 mm TQFP).
Values listed are for body dimensions.
Device Pin Differences
    
        
            | Pin | DS21Q42 | DS21Q41B | 
        
            | 9 | RSIG0 [RCHCLK0]
 | RCHCLK0 | 
        
            | 16 | SPARE [RMSYNC0]
 | RMSYNC0 | 
        
            | 18 | Active-Low JTRST [RLOS/LOTC0] | RLOS/LOTC0 | 
        
            | 34 | TSIG1 [TCHCLK1] | TCHCLK1 | 
        
            | 43 | RSIG1 [RCHCLK1] | RCHCLK1 | 
        
            | 46 | A7 | VSS | 
        
            | 47 | FMS | VDD | 
        
            | 50 | JTMS [RMSYNC1] | RMSYNC1 | 
        
            | 52 | JTCLK [RLOS/LOTC1] | RLOS/LOTC1 | 
        
            | 62 | Active-Low RD / (Active-Low RD) | Active-Low RD / (Active-Low RD) | 
        
            | 68 | TSIG2 [TCHCLK2] | TCHCLK2 | 
        
            | 77 | RSIG2 [RCHCLK2] | RCHCLK2 | 
        
            | 84 | JTDI [RMSYNC2] | RMSYNC2 | 
        
            | 86 | JTDO [RLOS/LOTC2] | RLOS/LOTC2 | 
        
            | 94 | TSIG3 [TCHCLK3] | TCHCLK3 | 
        
            | 103 | RSIG3 [RCHCLK3] | RCHCLK3 | 
        
            | 108 | 8MCLK [RMSYNC3] | RMSYNC3 | 
        
            | 112 | CLKSI [RLOS/LOTC3] | RLOS/LOTC3 | 
        
            | 128 | TSIG0 [TCHCLK0] | TCHCLK0 | 
    
NOTE: Brackets [ ] indicate pin function when the DS21Q42 is configured for emulation of the DS21Q41B, (FMS = 1).
Operating the DS21Q42 in DS21Q41B
Emulation Mode
The DS21Q42 is a superset of the DS21Q41B and can be configured to emulate the latter. This mode is
enabled by tying the Framer Mode Select (FMS) pin to VCC since the DS21Q42 supports an expanded
register set, the A7 address pin was added to the device. Although the DS21Q42 does not require the
functionality associated with the additional registers when in DS21Q41B emulation mode, the A7 pin must
be used. This is necessary because the device does not automatically clear its register space on power-up.
After the supplies are stable, each of four framers register space should be configured for operation by
writing to all of the internal registers. This can be accomplished in a two-pass approach on each framer.
    - Clear framers register space by writing 00h to the addresses 00h through BFh.
    
- Program required registers to achieve desired operating mode.