EBR Uses 16-Bit DAC

4096 Scan Lines with 5% Spacing-Error Allows High-Resolution, High-Speed Electron-Beam Recordings on Film

At CBS Laboratories, high-resolution electron-beam recording is accomplished by directing a controlled stream of electrons at a sensitive film in a vacuum. The electron beam is scanned horizontally, with stepwise vertical displacement of successive sweeps, and intensity modulation of the beam. Read full article