Versatile Monolithic V/f or I/f Converter

AD537 is Easy to Use, Works from Single Supply; Outputs to Beyond 100kHz; T/f Conversion Inherent

The AD537 is a self-contained monolithic voltage-to-frequency converter fabricated on a single 74 x 118 mil (1.9 x 3mm) silicon chip and mounted in a hermetically-sealed 14-pin ceramic dual in-line package (DIP). It contains an input amplifier, a precision oscillator system, a reference generator, and a high-current output stage. Read full article



作者

Dave-Kress-Blue

David Kress

David Kress拥有美国麻省理工学院的土木工程学士学位(BSCE)和硕士学位(MSCE)。他原先从事医疗电子设备设计工作,后于1972年加入ADI公司,担任IC设计师。 多年来,他从事过模拟芯片设计、晶圆制造工程、新产品开发和管理。多年来,David领导着ADI公司的技术支持团队,在2018年退休之前曾担任技术营销总监。

Barrie Gilbert

Barrie Gilbert

Barrie Gilbert, the first ADI Fellow, has “spent a lifetime in the pursuit of analog elegance.” He joined Analog Devices in 1972, was appointed ADI Fellow in 1979, and manages the Northwest Labs in Beaverton, Oregon. Barrie was born in Bournemouth, England, in 1937. Before joining ADI, he worked with first-generation transistors at SRDE in 1954, and at Mullard, Ltd.; later at Tektronix and Plessey Research Labs. Barrie is an IEEE Fellow (1984) and has received numerous awards. He has some 50 issued patents, has authored about 40 papers, is coauthor of several books, and is a reviewer for several journals. He was awarded an Honorary Doctorate of Engineering from Oregon State University in 1997.