In this circuit, the coupling time constant is increased by (1 + a). If R = 10MΩ, C = 1µF, a = 99, R1 = 100Ω, the RC of 10 seconds is increased to 1000s. Read full article
我们也为您准备了免费的《模拟对话》杂志印刷版本,准确填写信息后即可获得。
立即索取
In this circuit, the coupling time constant is increased by (1 + a). If R = 10MΩ, C = 1µF, a = 99, R1 = 100Ω, the RC of 10 seconds is increased to 1000s. Read full article