Advantages of 3-States in Synchro Conversion

Track the Input Signal Continuously without Opening the Loop; Digital Multiplexing is Sometimes Easier than Analog

Conventional tracking-type synchro-to-digital converters run into settling-time problems when the input angle has changed during an "INHIBIT." When the data is placed on three-state latches instead, the worst-case throughput delays can be as little as 30 nanoseconds. Read full article



作者

Generic_Author_image

Steve Bloom