ADI公司推出汽车行业首款用于量产电动汽车的无线电池管理系统

通用汽车的Ultium电池平台将使用ADI公司的无线电池管理系统

2020-09-14 - 中国,北京
  • Wireless Battery Management System

    Analog Devices, Inc. (Nasdaq: ADI) 宣布推出业内首款用于量产电动汽车的无线电池管理系统(无线BMS),使汽车制造商能够更加灵活地将电动汽车平台扩展至多种车型实现量产。作为首款用于量产电动汽车的无线电池管理系统,无线BMS将在通用汽车搭载Ultium电池平台的量产车辆中亮相。

    ADI公司的无线BMS免去了使用传统线束的必要,节省了高达90%的线束和高达15%的电池组体积,提高了设计灵活性和可制造性,同时不会影响电池使用寿命内的里程数和精度。

    ADI公司的无线BMS将电源、电池管理、射频通信和系统功能等所有集成电路、硬件和软件整合在单个系统级产品内,通过采用ADI公司经过验证的业内领先BMS电池电芯测量技术,支持ASIL-D安全性和模块级安全性。通过提高车辆使用寿命期间的精度,无线BMS系统可较大化单个电芯的能量利用率,从而实现优异的车辆续航里程,并支持安全且可持续的无钴电池化学材料,如磷酸铁锂(LFP)。

    ADI公司汽车事业部副总裁Patrick Morgan表示:"电池组从有线连接到无线连接的转变使汽车制造商能够将电动汽车平台扩展至多种车型,以满足消费者不断发展的需求。我们的无线BMS解决方案不仅可以简化制造流程,还可以根据无线数据构建新系统,从而加快整个行业向可持续未来的迈进。我们非常荣幸能够与通用汽车一起将这一突破性的系统创新推向市场。"

    附加的系统功能使电池能够测量和报告其自身性能,提升早期故障检测,并优化电池组装配。从电池组装到仓储和运输,再到安装、维护和梯次利用,在整个电池寿命周期中均可实现远程数据监测。

    ADI公司和通用汽车近期宣布建立合作关系,共同将无线BMS技术用于通用汽车的Ultium电池平台。ADI的无线BMS技术有助于将Ultium平台扩展到通用汽车的未来车型,包括不同子品牌和车型细分领域(从卡车到性能车等)。

    通用汽车全球电气化和电池系统执行总监Kent Helfrich表示:"我们非常高兴能够与ADI公司合作,共同将无线BMS技术用于生产,作为我们Ultium电池平台的组成部分。ADI公司的无线BMS技术可进一步推进我们车系的电气化发展,我们期待能与ADI公司继续合作,共同进行安全、质量和性能方面的创新。"

    欲了解有关ADI无线BMS的更多信息,请访问:www.analog.com/electrification

  • 关于ADI公司
    • Analog Devices (Nasdaq: ADI)是全球领先的高性能半导体公司,致力于解决艰巨的工程设计挑战。凭借杰出的检测、测量、电源、连接和解译技术,搭建连接现实世界和数字世界的智能化桥梁,从而帮助客户重新认识周围的世界。
      详情请浏览ADI官网 www.analog.com/cn 。


  • 通用汽车

    通用汽车(NYSE: GM)是一家全球性公司,致力于为人们提供更安全、美好和可持续的出行方式。通用汽车及其子公司和合资公司销售 雪佛兰别克GMC凯迪拉克霍顿宝骏 和 五菱 等品牌的汽车。欲了解更多通用汽车及其子公司(包括汽车安全与安保服务领域的全球领导者安吉星)详情,请访问http://www.gm.com

    This release may contain forward-looking statements intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, among other things, statements by Messrs. Helfrich and Morgan and other statements regarding the expected opportunities, utilization, benefits, cost savings, product and service offerings and developments relating to our wireless battery management system that are based on current expectations, beliefs, assumptions, estimates, forecasts, and projections about the industry and markets in which the companies operate. The statements contained in this release are not guarantees of future performance, are inherently uncertain, involve certain risks, uncertainties, and assumptions that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed in such forward-looking statements, and such statements should not be relied upon as representing Analog Devices' expectations or beliefs as of any date subsequent to the date of this press release. Important factors that could cause actual results to differ materially from the results described, implied or projected in any forward-looking statements are included as risk factors as described in the most recent filings of Analog Devices with the Securities and Exchange Commission. Analog Devices does not undertake any obligation to update forward-looking statements made by us.


  • 联络方式