Versatile Ring Tone Generator Finds Uses in Motor Drivers and Amplifiers

Sep 1 1999

Figure 1

   

Overview

The LT1684 was specifically designed for OEM telephone equipment. Its function is to interface between the digital control logic and the high voltage analog phone line. When used in the design of a phone system, the LT1684 allows software to control the frequency, voltage and cadence of the ring signal. Because of similarities of application to telephone systems, the LT1684 ring tone chip finds itself at home in motor drives, digital input amplified speakers, alarm systems and sine wave UPS systems.

Introducing the LT1684

The LT1684 provides the tool set to easily implement a digital, pulse width modulated (PWM) signal to DC-coupled voltage converter (at high currents), while providing isolation, switching frequency filtering and output protection. Figure 1 is a system-level diagram of the LT1684 in action. By controlling a pair of external MOSFETs, the LT1684 utilizes their inherent robustness while providing control of the output voltage and current. In its telecom application circuit, the LT1684 provides up to ±240V of smooth, clean output at up to 200mA of output current. Higher output voltages are obtained by cascoding MOSFETs, while higher currents are readily achieved by using the LT1166 MOSFET automatic bias generator chip as a companion.

Figure 1. The LT1684 uses differential pulse width modulation to provide isolation for digitally controlled analog power solutions.

The Circuit

Figure 2 is the schematic of the LT1684 implementing a digital-PWM-to-ringing-telephone converter. This is something like a high power, high voltage, isolated, output filtered D/A converter. Like its DAC counterpart, the LT1684 has a precision reference, switches and an output amplifier. Unlike its DAC counterpart, it includes post-conversion ripple filtering, isolation and a robust high voltage output.

Figure 2. Typical LT1684 digital-PWM-to-ringing-telephone converter application.

In addition to the isolation, filtering and amplification, the LT1684 provides the gate-bias control and gate voltage protection for the two external MOSFETs. Providing such a plethora of functions from a single, monolithic IC requires the use of a somewhat tricky circuit. This circuit is arrived at by applying a circuit transformation to a simple filter circuit. This transformation is performed on the basic 2nd order lowpass multiple feedback filter (MFB) circuit and ends up looking somewhat like the filter/amplifier shown in Figure 3. The filter/amplifier components in Figure 2 are R3–R5 and C3 and C4. Looking backwards through the circuit transformation, these components, in fact, form the 2nd order MFB filter shown in Figure 3. The values chosen for these components in Figure 2 implement a 2nd order Butterworth MFB lowpass filter with a cutoff frequency of 100Hz and a DC gain of 100. These were chosen to provide ±80V of output swing with PWM duty factors of 10% to 90%, while filtering the 10kHz PWM ripple to meet telephone specifications.

Figure 3. The basic 2nd order lowpass MFB filter, as implemented by the LT1684.

Stealing the LT1684 for Use In Other Applications

The LT1684, used as shown in Figure 1, outputs a ring signal that meets Belcore specification. This means we can ring a phone 22,000 feet away. The LT1684 fits another role, where 22,000 feet of separation would be a nice minimum. This is the application of the LT1684 in the scaleable power amplifier, as detailed in Figure 4. This amplifier can be used to drive motors, simulate the power company in sine wave UPS systems and operate large audio drivers. Because of its scaleable nature, this design can be used at any power level. The circuit in Figure 4 is shown implementing a 5000W bits-to-decibels converter. When this converter is implemented with the appropriate audio drivers and enclosures, the output sound pressure level can be significant—so significant, in fact, that the author suggests giving it a wide berth of at least 22,000 feet.

Figure 4. 5kW PWM-to-analog converter.

Analog Inputs Welcome

The scaleable amplification system detailed in Figure 4 can be driven with analog inputs while still maintaining full isolation. Such a system is detailed in Figure 5, where the analog input is filtered (to prevent ailiasing) and converted to PWM. Figure 5 goes on to show the use of an RS485 differential driver to drive a twisted pair line. The receiver end of the twisted pair line is terminated with a resistor and put across the isolation barrier. This provides very good ESD protection on both ends of the line.

Figure 5. A remote, isolated, analog input amplifier using a robust RS485 driver and a terminated, twisted-pair line.

Conclusion

The LT1684 is useful in a wide variety of applications. The LT1684 is a highly integrated solution for use in any system that requires digital control of high output voltage or high output power.

About the Authors

Dale Eagar
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Product Categories
Latest Media 25
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project