Home     Analog Devices     Feedback     Subscribe     Archives     Advanced Search      

Recent Feature Articles

The Basics of Video Decoders in Supervision and Inspection

Video cameras—which range from inexpensive, low-definition black-and-white closed-circuit television systems to state-of-the-art high-definition digital-video systems—are found in diverse applications including product inspection, traffic monitoring, and real-time face recognition. Dropping unneeded data and passing only the essential parts of the picture can simplify the video system—saving memory and computational cycles.

Detecting Human Falls with a 3-Axis Digital Accelerometer

Elderly individuals can suffer accidental falls due to weakness or dizziness. The initial injury can be further aggravated if treatment is not obtained within a short time. MEMS-based fall detectors can sense changes in body position by tracking acceleration, determine when an individual is falling, and issue an alert for assistance. This article describes the use of an ADXL345 three-axis digital accelerometer as a fall detector.

Digital Isolator Simplifies USB Isolation in Medical and Industrial Applications

Despite its low speed and point-to-point nature, RS-232 was tolerated in medical and industrial applications because it was universally available, well supported, and allowed easy implementation of the required isolation. The ADuM4160 digital isolator allows simple, inexpensive isolation of full- and low-speed USB peripherals—including the D+ and D– lines—increasing the usefulness of USB in medical and industrial applications.

“Rules of the Road” for High-Speed Differential ADC Drivers

Most modern high-performance ADCs use differential inputs to reject common-mode noise and interference, increase dynamic range by a factor of two, and improve overall performance. ADC drivers—circuits often specifically designed to provide differential signals—perform many important functions including amplitude scaling, single-ended-to-differential conversion, buffering, common-mode offset adjustment, and filtering.

PLC Evaluation Board Simplifies Design of Industrial Process-Control Systems

The applications for industrial process-control systems range from simple traffic control to complex electrical power grids, from environmental control systems to oil-refinery process control. The intelligence of these systems lies in their measurement and control units. The two most common computer-based systems to control machines and processes are programmable logic controllers and distributed control systems.

Analog Microcontroller Forms Heart of Low-Cost, High-Efficiency PA Monitor

Saving energy is crucial for efficient wireless network operation. Power amplifiers (PA), the core of base stations and repeaters, can account for more than half of their total power consumption. Monitoring and controlling the PA can: improve efficiency and reduce operating costs; maximize output power and achieve the highest possible linearity; and allow the system operator to discover problems and improve reliability.

Using MEMS Accelerometers as Acoustic Pickups in Musical Instruments

MEMS microphones have begun to dominate the broad consumer market, including cell phones, Bluetooth headsets, personal computers, and digital cameras. Now, key technologies used in MEMS accelerometers can bring a new dimension to acoustic transducers. Low-g accelerometers don't suffer from traditional feedback problems, and show clear potential as high-quality acoustic pickups for musical instruments.

Smart Metering Technology Promotes Energy Efficiency for a Greener World

We’re all familiar with the electricity meter in the garage or basement. We may even have looked at it once or twice to phone an up-to-date reading to the utility company in place of an estimate. Thanks to technology, a quiet revolution is taking place inside this innocuous looking meter. This article describes how automatic meter reading and the smart grid can help improve energy efficiency and reduce carbon emissions.

Analog Front End for Femto Base Stations Brings Wireless Connectivity Home

Imagine a device that can provide high-quality cellular reception within your home, allowing you and your family unlimited voice and data usage for a low monthly fee. A femto base station, usually referred to as a femtocell, provides all that and more. This small wireless device, which improves local wireless coverage when placed in a home or office, is poised to dramatically change the wireless infrastructure landscape.

Considering Multipliers, Part 1 [The Wit and Wisdom of Dr. Leif–7]

Multipliers exploiting translinear loops, current-mirrors, current conveyors, and linear gm cells continue to be indispensable more than sixty years since the very first fully monolithic ICs were fabricated in 1967. In this futuristic tale, Drs. Newton Leif and Niku Chen discuss multiplier topologies, uses, and history. Leif also provides some hints as to how neurons, which are translinear, behave exactly like bipolar junction transistors.

Design, Simulate, and Document Proprietary Wireless Systems

The broad acceptance of standards developed for short range wireless connectivity has been one of the notable features of the semiconductor market in the past few years. These standards include Bluetooth, various flavors of Wi-Fi, ZigBee, and new emerging standards, such as Wibree/Bluetooth ULP and Ultra Wideband. The available wireless standards are not always the best fit for the application’s requirements, however.

Maintaining Public Railways with Lower Cost and Improved Safety

A new, systematic maintenance approach now makes it possible to measure, locate, and fix rail- and tramway defects when they appear. Mature railway-engineering know-how and cutting edge technologies—including Blackfin processors and graphical system design techniques—combine to improve and optimize public transportation. This can result in longer operation lifetimes for rails, improving economy and reliability.

Impedance Measurement Monitors Blood Coagulation

Blood coagulation is a complex process by which clots are formed to end bleeding at an injured site. During heart-bypass surgery, blood is diverted to a heart-lung machine. An anticoagulant is administered during surgery—followed by a rapid reversal. This article describes a coagulation monitor that provides rapid, automated data—aiding patient safety, workflow, and decision making—and leading to improved outcomes.

Fingerprint Sensor and Blackfin Processor Enhance Biometric Identification

The need for effective, efficient security is manifest in today’s world. Individuals must be identified to allow or prohibit access to secure areas—or to enable them to use a computer. Biometric signatures identify individuals by measuring unique physical and behavioral characteristics using: a sensor, feature extraction, pattern matching, and decision making—allowing a user’s claimed identity to be authenticated or rejected.

Noise Figure and Logarithmic Amplifiers [The Wit and Wisdom of Dr. Leif—6]

Log amps are uniquely equipped as RF measurement elements at frequencies from near-dc up to 12 GHz because of their wide dynamic range, temperature stability, excellent log conformance, and ease of use—with measurements provided directly in decibels. Noise figure is a valuable metric when log amps are used in the signal path, as it indicates the system's ability to extract information in the presence of noise.

Understanding Hot-Swap Controllers: Hot-Swap Circuit Design Example

High-availability systems, such as servers, network switches, redundant-array-of-independent-disk (RAID) storage, and other forms of communications infrastructure must be designed for near-zero downtime throughout their useful life. Components that fail or need updating must be replaced without interrupting the rest of the system. This process, known as hot-swapping or hot-plugging, requires a hot-swap controller.

Discrete- and Integrated Control of Power Amplifiers in Base Stations

In wireless base stations, the power amplifier dominates the performance in terms of power dissipation, linearity, efficiency, and cost. Monitoring and controlling the PA makes it possible to maximize the output power while achieving optimum linearity and efficiency. This article discusses the elements of a monitoring-and-control solution for the PA using discrete components—and describes an integrated solution.

Cooking Inductively: ADI iCoupler Technology Isolates Hob and User Interface

Easy-to-use inductive cooking surfaces (hobs) are significantly safer, without flames or other direct heat sources on the hob. They have better overall performance, including faster heating time, and are gaining acceptance by consumers as they are becoming more affordable. Designing the circuitry that drives the inductive plate to heat metal pots requires an understanding of a wide variety of physical principles and techniques.

Analog/Digital-Converter Clock Optimization: A Test Engineering Perspective

The entire system-clock signal chain must be understood in order to achieve optimal performance from an A/D converter. It can be discouraging to find that a circuit's accuracy is clock-jitter limited, as this problem could have been prevented during the design phase. Decreased clock jitter can be achieved through frequency division, filtering, use of an improved clock source, and proper choice of auxiliary hardware.

High Side Current Sensing: Difference Amplifier vs. Current-Sense Amplifier

Accurate high-side current sensing is necessary in applications such as motor control, solenoid control, and power management. In these applications, monitoring the current on the high side permits improved diagnostic capabilities and maintains the integrity of the ground path by avoiding the introduction of shunt resistance. The sensing circuitry  must reject high common-mode voltages, while providing high gain and high accuracy.

Switching-Regulator Insights—Achieving Longer Battery Life in DSP Systems

Step-down dc-to-dc switching regulators efficiently derive a low voltage from a higher voltage, maintaining a constant output despite variations in supply voltage or load current. This article describes an architecture that provides good regulation, high efficiency, and fast response, showing both fixed-voltage operation and a resistor-programmable circuit that provides dynamic voltage scaling in DSP applications.

Faster Open-Loop Gain Measurements (Ask The Applications Engineer—38)

It is often desirable to measure the performance of a feedback network in a particular configuration so as to model the open-loop behavior. But this type of measurement is often challenging due to high gains, small input signals, and long settling times. This article shows you how to characterize the frequency response of the network rapidly and with minimal effort, using available tools and a small amount of special circuitry.

Phase Relations in Active Filters

In applications that use filters, the amplitude response is generally of greater interest than the phase response. When a filter is used inside a process control loop, however, the total phase shift is of concern, since it may affect loop stability. This article looks at first- and second-order filters, comparing phase response as a function of topology, order, and Q. Higher-order filters are treated as cascades of lower-order blocks.

Toward More-Compact Digital Microphones

As electret microphones become smaller, their element capacitance decreases. JFET preamps no longer suffice, as their relatively large input capacitance attenuates the signal from the microphone. Much can be gained by replacing JFET amplifiers with CMOS analog and digital circuitry, including easier gain setting, multiple functional modes, direct digital outputs, enhanced sound quality, and higher noise immunity.

Avoid Common Problems When Designing Amplifier Circuits

Modern op amps and in-amps provide great benefits to the designer, and a great many clever, useful, and tempting circuit applications have been published. But all too often, in one’s haste to assemble a circuit, some very basic issues are overlooked, leading to the circuit not functioning as expected—or perhaps at all. This article will discuss a few of the most common application problems and suggest practical solutions.

The AD9271—A Revolutionary Solution for Portable Ultrasound

Medical ultrasound systems, among the more complex signal processing devices in use today, are used for real-time detection of health problems and general diagnostic procedures. Slower than radar and faster than sonar, ultrasound systems have become increasingly portable, evolving from cart-based systems into palm-sized devices. This article discusses some of the necessary ingredients of compactness.

Reducing Ground Bounce in DC-to-DC Converters—Some Grounding Essentials

Electrical ground looks simple on a schematic, but circuit performance is dictated by the PCB layout. Ground-node analysis is difficult, especially for dc-to-dc converters, such as buck and boost circuits, which pound the ground node with large, fast-changing currents. When ground moves, performance suffers and the system radiates EMI. An understanding of ground noise can provide a sense for reducing the problem.

Low-Dropout Regulators (Ask The Applications Engineer—37)

Voltage regulators provide stable outputs independent of line voltage, load impedance, temperature, and time. Low-dropout regulators (LDOs) can maintain regulation with a small difference between supply voltage and load voltage. This article introduces basic topologies of LDOs, and provides tips for ensuring stable operation. It also discusses ADI's LDOs, which offer a flexible approach to maintaining dc- and dynamic stability.

Elements of Motion: 3D Sensors in Intuitive Game Design

Standard video game controllers limit intuitive play, requiring a player to learn specific control skills. The latest platforms add motion, enabling games that are both more fun and more intuitive. This article presents a foundation for using accelerometers in game controllers, including operating mechanisms, measurement techniques, and specific parameters that affect gaming performance, price, reliability, verification, and test.

High-Speed Time-Domain Measurements—Practical Tips for Improvement

Making accurate high-speed time domain measurements can be challenging, but a few tips and tricks, coupled with some good old-fashioned commonsense engineering, can help yield quick and accurate results. When choosing a scope and probe for high-speed measurement, first consider: signal amplitude, source impedance, rise time, and bandwidth. The type of probe and length of the ground lead are also important.

Wideband ADC Front-End Design: Amplifier Drive vs. Transformer Drive (Ask The Applications Engineer—36)

The circuitry ahead of a high-performance ADC is critical to achieving desired system performance. The optimal design depends on many factors, including the application, system partition, and ADC architecture. Amplifiers consume power and add noise, whereas transformers consume no power and add negligible noise. On the other hand, amplifiers maintain dc levels, provide easily adjustable gain, and have flatter response. 

Multichannel Power-Line Monitoring with Simultaneous-Sampling ADCs

The rapid expansion of the electric power industry has created a worldwide need to reinforce existing transmission and distribution networks and to construct new substations. Advances in microprocessor technology and the increasing cost of support staff are key drivers for power companies to design new automated high-voltage substations using high-accuracy integrated automation systems.

Digital Isolation: A Compact, Low-Cost Solution to Complex Design Problems

New isolation capabilitiesincluding integrated, isolated power and truly bidirectional isolation channels—are greatly simplifying the design of isolated systems. Fueled by a shift from LED-based optocouplers to chip-scale microtransformer technology that is compatible with standard CMOS processes, they fit more functionality into a single package. This article discusses two kinds of devices that embody these advances.

Lens Drivers Focus on Performance in High-Resolution Camera Modules

An Evolution of Resolution is driving the development of cell phone camera modules. Autofocus is now standard in high-resolution cameras, and features such as optical zoom, shutter control, and image stabilization are becoming common. These require the lens to move rapidly. The lens driver powers a motor to move the lens in response to digital signals. This article discusses three types of motors and how to drive them.

Capacitance Sensors for Human Interfaces to Electronic Equipment (Ask The Applications Engineer—35)

Mechanical buttons, switches, and jog wheels have long been used as interfaces between users and machines, but their many drawbacks have led designers to look for more reliable solutions. Capacitive sensors, which can be used in place of buttons, can also add versatility. Available ICs can measure the capacitance of up to 14 sensors, compensate for environmental changes, and provide a digital output.

Fast, Versatile Blackfin Processors Handle Advanced RFID Reader Apps

From inventory control to supermarket checkouts, RFID technology is transforming existing applications and enabling new ones. RFID readers detect tags and read the information they carry. Typically needing a signal processor to interface with ADCs and DACs and a network processor to communicate with servers, they can now use a Blackfin® processor to manage both signal conversion and network connectivity.

Precision Signal-Processing and Data-Conversion ICs for PLCs Now Have More Performance at Less Power, Size, and Cost

Programmable-logic controllers are compact computer-based electronic systems that use digital or analog I/O modules to control machines, processes, and other control modules. PLCs can receive (input) and transmit (output) various types of electrical signals to control and monitor many kinds of electromechanical systems.

Wideband A/D Converter Front-End Design Considerations

A factor often overlooked when using transformers in the front-end circuitry of high-speed A/D converters is that they are never ideal. Any imbalance introduced by the transformer delivers an imperfect signal to the ADC, causing overall performance to be worse than the ADC could otherwise provide. Read about the effects of input imbalances on ADC performance and circuitry that can help achieve better results.

Class D Audio Amplifiers: What, Why, and How

Class D amplifiers, first proposed in 1958, have become increasingly popular in recent years. What are class D amplifiers? How do they compare with other kinds of amplifiers? Why is class D of interest for audio? What is needed to make a good class D audio amplifier? What are the features of ADI's class D amplifier products? Find the answers to all these questions and more by reading this article.

Power Supply Management—Principles, Problems, and Parts

Determining whether a supply voltage is above a threshold or within an operating window—and powering supplies on or off in the correct sequence with respect to each other—is vital for safety, economy, durability, and proper operation of electronic systems. This article discusses how power supply designers are using flexible supply monitoring, sequencing, and adjustment circuits to manage their systems.

Design Your Own VoIP Solution with a Blackfin Processor—Add Enhancements Later

The age of voice-over-Internet-protocol is here, with packetized data streaming over low-cost Internet links. Designers must choose a cost-effective, easy to deploy, scalable platform that can implement a basic VoIP solution, while retaining plenty of capacity for value-added capabilities and services—like video, music, and imaging.

Wireless Short-Range Devices: Designing a Global License-Free System for Frequencies <1 GHz

Short-range radio transmitters can communicate without interfering with other radio equipment. Short-range devices (SRD) provide many different services—including home automation, keyless remote entry, and wireless video—typically using portions of the spectrum that allow license-free operation provided certain conditions are met.

ADC Input Noise: The Good, The Bad, and The Ugly. Is No Noise Good Noise?

All analog-to-digital converters (ADCs) have a certain amount of input-referred noise—modeled as a noise source connected in series with the input of a noise-free ADC. In most cases, less input noise is better; however there are some instances where input noise can actually be helpful in achieving higher resolution. Read this article to learn how some noise can be good noise.

Switching in USB Consumer Applications

The universal serial bus has become a dominant interface for rapidly transferring data between PCs and portable devices such as digital cameras, personal media players and cell phones. CMOS switches can be used for connecting and routing data lines in USB systems. Selecting suitable switches allows designers to enhance existing designs rather than developing new ones, significantly shortening design cycles.

A Reference Design for High-Performance, Low-Cost Weigh Scales

The accuracy required by weigh scales is not initially obvious. Their typical resolution is only 1:3,000 to 1:10,000, so a 12- to 14-bit ADC would seemingly be adequate. A closer examination shows that this is not case, however, and that a 20-bit ADC is really required. This article introduces weigh scale system specifications and design considerations, including noise, dynamic range, offset drift, gain drift, and filtering.

Using Dual-Axis Accelerometers to Protect Hard Disk Drives

The increasing use of hard disk drives in portable equipment has fueled the need to prevent their destruction when a product that contains one is accidentally dropped. This article describes a novel technique that calculates differential acceleration, thus allowing a dual-axis accelerometer to sense an impending collision in time to park the read/write head and protect the head and the platter from damage.

iCoupler® Digital Isolators Protect RS-232, RS-485, and CAN Buses in Industrial, Instrumentation, and Computer Applications

Serial communication buses are used to transmit data over various types of physical networks, with interconnected systems typically separated by long distances. Thus, galvanic isolation is often required to break ground loops, protect the system from high-voltage transients, reduce signal distortion, and to enhance physical safety.

A Practical Guide to High-Speed Printed-Circuit-Board Layout

Despite its critical nature in high-speed circuitry, PCB layout is often one of the last steps in the design process, with sloppy layouts sometimes causing circuit designs that look good “on paper” to render mediocre performance. This article addresses high-speed layout from a practical perspective, discussing topics that can improve circuit performance, reduce design time, and minimize time-consuming revisions. 

DDS Controls Waveforms in Test, Measurement, & Communications

Direct Digital Synthesizers can generate frequencies from a few hertz to greater than 400 MHz with less than 1 degree phase resolution. They can quickly hop from one frequency to another—in a phase-continuous manner—without settling anomalies. DDS-based waveform generation is used to locate resonant frequencies in industrial applications and as agile frequency sources in RF communication systems.

Encoder’s Spare Channel Embeds Whole-House Stereo Audio in Satellite Set-Top-Box Designs Stably and Cost-Effectively

The novel application of a phase-locked loop allows one channel of the AD71028 BTSC- (Broadcast Television Standards Committee) encoder to derive the primary channel’s master clock, while the other channel provides the Multichannel Television Sound (MTS) stereo-encoded output for satellite set-top boxes and receivers.

Which ADC Architecture Is Right For Your Application?

Selecting the proper ADC for a particular application can be a formidable task, considering the thousands of available converters. An understanding of three popular architectures—successive-approximation, sigma-delta, and pipelined—and their relationship to the data acquisition, precision measurement, audio, and high speed markets is a useful supplement to selection guides and search engines.

Pushing the State of the Art with Multichannel A/D Converters

The most demanding data-acquisition requirements surpass the performance levels provided by commercially available integrated-circuit ADCs. Innovative solutions that fulfill high-end data-acquisition system needs while awaiting the next performance breakthrough use signal averaging, for increased resolution without loss of speed—and time interleaving, to increase sampling rates without loss of resolution.

Transformer-Coupled Front-End for Wideband A/D Converters

ADCs are being used at ever higher frequencies, making receiver front-end design increasingly important. Many applications are moving to super-Nyquist sampling in order to eliminate a mix-down stage, but amplifier noise will degrade the signal-to-noise ratio at these frequencies. Transformers can be used to replace the amplifier, minimizing noise and providing good high-frequency coupling.   

A Smart Modem for Robust Wireless Data Transmission Over ISM Bands

Heavy usage of the license-free 2.4-GHz band—from microwave ovens, Bluetooth, WLAN 802.11b, and cordless phones—has increased interest in the lower-frequency ISM bands. The ADF7020 UHF transceiver and ADSP-BF531 Blackfin processor can implement a smart modem that has the ability to overcome interference from legacy systems and the flexibility required to deal with the lack of established standards.

Enhance Processor Performance in Open-Source Applications

Open-source algorithms are becoming a popular alternative to royalty-based code in embedded processing applications. Each compiler will exploit a given processor’s strengths at the expense of other inefficiencies, so developers must optimize the acquired code for the chosen processor. This article will explore the porting of open-source algorithms for music-, video-, and speech processing to Blackfin processors.

Blackfin Processor’s Parallel Peripheral Interface Simplifies LCD Connection in Portable Multimedia Applications

Low-power, fixed-point Blackfin processors now have the performance required to handle signal processing and control functions, while also driving the small liquid-crystal-displays used in many multimedia applications. Their parallel peripheral interface integrates LCD drive capability with high-performance media processing.

Support for the Designer—Improved ADI Website Helps You

If you are an old friend, perhaps you’ve already found that www.analog.com is friendlier than ever. If you are new to our website, Welcome! This article introduces our new Design Center, where you can find tools and utilities such as parametric searches, selection tables, signal chains, models, and Analog Wizards—all intended to help you quickly find and apply the best products for your design.

Designing Memory-Efficient, Real-Time Audio Systems With VisualAudio

Home theater and automotive audio systems continue to increase in complexity. VisualAudio™, a new software tool for designing and developing audio systems, provides a real-time-architecture that is especially well-suited to the challenges of audio product development. This article introduces VisualAudio, describing its framework, audio modules, and application to audio product development.

Wideband CMOS Switches (Ask the Applications Engineer—34)

Wideband CMOS switches are designed to meet the requirements of devices transmitting in the ISM (industrial, scientific, and medical) band (900 MHz and up). Their low insertion loss, high isolation between ports, low distortion, and low current consumption make them ideal for many high frequency applications that require low power consumption and the ability to handle transmitted power up to 16 dBm.

JPEG 2000 Image Compression

The JPEG 2000 standard defines a new image-coding scheme using state-of-the-art compression techniques based on wavelet technology. Its architecture is useful for many applications, including Internet image distribution, security systems, digital photography, and medical imaging. This article highlights some of its benefits.

All About Direct Digital Synthesis (Ask the Applications Engineer—33)

Direct digital synthesis (DDS) is a method of producing an analog waveform—usually a sine wave—by generating a time-varying signal in digital form and then performing a digital-to-analog conversion. Because operations within DDS devices are primarily digital, they can offer fast switching between output frequencies, fine frequency resolution, and operation over a broad spectrum of frequencies.

Adjustable Cable Equalizer Combines Wideband Differential Receiver with Analog Switches

Category-5 unshielded twisted-pair cable, like any transmission medium, suffers from dispersion and high-frequency signal loss. This article presents an equalizer that compensates Cat‑5 cable at frequencies to 100 MHz and lengths to 1000 feet, making it suitable for KVM networking and high-resolution video transmission.

Practical Techniques to Avoid Instability Due to Capacitive Loading (Ask the Applications Engineer—32)

Capacitive loading of amplifiers reduces bandwidth and slew rate, and introduces a phase lag in the feedback loop that can cause instability. ADI has published a lot of information on dealing with capacitive loading and other stability issues in books, earlier issues of Analog Dialogue, and some design tools. Here's a refresher course.

Bridge-Type Sensor Measurements are Enhanced by Autozeroed Instrumentation Amplifiers with Digitally Programmable Gain and Offset

This article introduces the AD8555, which simplifies bridge measurement systems by integrating a zero-drift instrumentation amplifier with programmable gain, programmable output offset, fault detection, output clamping, and low-pass filtering, thus providing the complete signal conditioning path between a sensor and an ADC.

Current Measurement in Solenoids for Automotive Control Systems

Linear solenoids operate pistons and valves to accurately control fluid pressure or flow in automotive transmissions. Connected in feedback loops and powered by PWM signals, their position can be determined by measuring their current. This article shows several methods of using an AD8200 to measure solenoid current.

Use of Video Technology to Improve Automotive Safety Becomes More Feasible with Blackfin Processors

Processors control almost every function in today's automobiles, including climate control, engine control, and entertainment. Now, the increasing performance-to-cost ratio of signal processors is leading to their use in the safety subsystem. Blackfin media processors can help to make video-based automotive safety a reality.

Why and How to Control Fan Speed for Cooling Electronic Equipment

Compact electrical fans are cheap and have been used for cooling electronic equipment for more than half a century. The technology for controlling these fans has evolved significantly, enabling lower power, quieter systems to be designed. This article suggests some useful approaches to efficient heat removal.

Mixed-Signal Control Circuits Use Microcontroller for Flexibility in Implementing PID Algorithms

Proportional-Integral-Derivative (PID) algorithms are commonly used to provide accurate, stable process control. Systems typically require an ADC to measure the process variable, a DAC to manipulate the physical input, and a digital controller. This article shows how a MicroConverter® can simplify the system implementation.

Closed-Loop Control of Variable Optical Attenuators with Logarithmic Analog Processing

Translinear log-amps simplify VOA absorbance measurements by providing a linear-in-dB relationship between the input photo-current and resulting output voltage, thus eliminating the division and exponentiation processes that would be required with classical architectures using transimpedance amplifiers.

ECG Front-End Design is Simplified with MicroConverter®

This article provides an overview of a traditional analog ECG system, then proposes a simpler circuit that uses a MicroConverter®—a “system on a chip” that combines an A/D converter, microcontroller, and flash memory—to flexibly perform analog-to-digital conversion, digital filtering, and digital amplification.

Fast-Locking, High-Sensitivity Tuned-IF Radio Receiver Achieved with a 7-GHz Synthesizer

To improve sensitivity and selectivity in modern radios, phase noise and reference spurs must be minimized, and lock time must be reduced. The circuit outlined in this article uses an ADF4107 7-GHz PLL synthesizer in a tuned-IF architecture to improve local oscillator (LO) performance with respect to these parameters.

How to Save Power in Battery Applications Using the Power-Down Mode in an ADC

Minimizing the current drawn by system components can extend battery life—a critical concern in battery-powered applications. Most ADCs provide a power-down mode, but the technique used to place them into the power-down state—and its effectiveness—differ from part to part. This article describes some novel methods.

Advanced Digital Post-Processing Techniques Enhance Performance in Time-Interleaved ADC Systems

This article details the matching requirements for 12- and 14-bit time-interleaved ADC systems, discusses the idea of advanced digital post-processing techniques as an enabling technology, and introduces the AD12400, a device employing the most promising performance to date.

Dynamic Memory Allocation Optimizes Integration of Blackfin® Processor Software

Blackfin’s memory is versatile and easy to use in many applications, but in some applications, such as embedded cell phone systems, memory allocation can be difficult for any embedded processor. This article introduces ADIalloc, a dynamic memory allocation tool designed to deal with this challenge.

Solving Power-Management Problems with a Single Chip that Handles up to 7 Channels of Sequencing, Monitoring, and Supervision

Systems with multiple supply voltages have become common, so sequencing and supervision of their supplies has grown in importance. The ADM1060 simplifies this task by providing multiple supply supervisors, sequencing logic, and output drivers, and is easily programmed using an intuitive graphical user interface.

Compact Web-Manufacturing Process Defect Detection System Uses a Camera and ADI Blackfin Processor

One aim of industrial machine vision is to develop electronic systems to replace human vision in industrial quality control. This article describes a new integrated environment—intended for real-time defect detection—that eliminates the need for an external frame grabber and associated host computer peripherals.

Amplifiers as Comparators? (Ask the Applications Engineer--31)

In principle, any high-gain amplifier can be used as a comparator, but as usual, "the devil is in the details". This article helps designers to understand the basic differences between amplifiers and comparators, allowing them to determine when an amplifier can be used to improve precision, reduce cost, or save space.

New iMEMS Angular Rate-Sensing Gyroscope

With full-scale ranges of 150°/s and 300°/s, the new ADXRS150 and ADXRS300 represent a quantum jump in gyro technology. The first commercially available surface-micromachined angular rate sensors with integrated electronics, they are smaller—with lower power consumption, and better immunity to shock and vibration—than any gyros having comparable functionality.

Getting 14-Bit Performance from a 32-Channel 14-Bit String DAC

The AD5532 32-channel, 14-bit voltage output D/A converter can be used in DAC mode or Infinite Sample-and-Hold mode. The DACs have 14-bit monotonicity, but only ±0.39% integral nonlinearity. This article shows how the DACs can be calibrated to provide 14-bit performance.

Glueless, Hot-Swappable CompactFlash™ Interface

CompactFlash cards are used in MP3 players, digital cameras, handheld PCs, and many other electronic devices, and can be used for nonvolatile storage and transfer of music, pictures, and data. This article describes a simple interface between the ADSP-2191M digital signal processor and a CompactFlash card.  

High-Speed Op Amp Drives a 16-Bit, 1-MSPS Differential-Input A/D Converter

High-resolution A/D converters usually require input buffer amplifiers because they present both dc- and high-frequency dynamic loads to the source that is driving them. To maintain system accuracy, the settling time, noise, and total harmonic distortion of the driver must be considerably better than that of the ADC itself. This is a significant challenge in systems employing fast 16- or 18-bit successive-approximation ADCs.

Bus Switches for Speed, Safety, and Efficiency: What they are, what you should know about them

Bus switches are characterized by sub-nanosecond propagation delay and fast switching, and are designed for connecting to high-speed digital buses. They are ideally suited for voltage translation, hot swapping, hot plug, bus- or capacitance isolation, and many other applications. The key features that make them suitable for so many different applications include low on-resistance, low capacitance, and low propagation delay. 

Detecting Fast RF Bursts Using Log Amps

Monolithic log amps can handle signals with dynamic ranges up to 100 dB, and can respond to RF bursts as short as a few tens of nanoseconds. When demodulating log amps are used to detect fast RF bursts, however, strange tails sometimes appear at the output when the burst shuts off. This article explains the cause of these tails and offers suggestions on how to eliminate them.

Single-Chip Digitally Controlled Data-Acquisition as Core of Reliable DWDM Communication Systems

Optical communication systems use ADCs and DACs in control loops for the thermoelectric cooler (TEC), laser diode driver (LDD), and avalanche-photodiode (APD) monitoring and biasing circuitry. Dedicated control loops are used for driving the pump laser, reading its power level, adjusting the extinction ratio and average power in the transmit laser diode, and maintaining the laser diode at a stable temperature. This article describes a control system that has a MicroConverter™ at its heart.

Dynamic Power Management Optimizes Performance vs. Power in Embedded Applications of Blackfin™ DSPs

Consumer products employing multimedia embedded processors require complex computational abilities and high clock rates, but also low power consumption. Performance vs. power must be optimized for the specific application. A strategic power management approach is achievable with the inherent dynamic power management capabilities of the Blackfin DSP family.

Mirrors with Integrated Position-Sense Electronics for Optical-Switching Applications

Signal paths using all-optical switches will be required for 40-Gbit telecommunication systems. ADI's integrated optical micro-electromechanical system (optical iMEMS) technology combines mirrors, high-voltage CMOS for electrostatic deflection, and low-voltage CMOS for on-chip capacitive position-sensing. This technology could drastically lower the cost of all-optical switching systems.

How Ultrasound System Considerations Influence Front-End Component Choice

Medical ultrasound machines are among the most complex signal processing machines in use today, and thus present many trade-offs in implementation due to physics, cost and performance requirements. An overview of the system is presented in order to provide an understanding of the front-end IC functions and desired performance levels, especially for the low-noise amplifier, time-gain control, and A/D converters.

PLL Synthesizers (Ask the Applications Engineer--30)

What is a PLL synthesizer? What are the key performance parameters? How do I choose external components? Why are phase noise and lock time important, and how do I optimize them? Adrian Fox provides answers to these questions, and presents new ADI PLLs and simulation tools.

Versatile Mixed-Signal Front Ends Speed Customized Design of Wireline Broadband Modems and Home Networks

"No-new-wire" wireline technologies, as well as DSL and cable, require mixed-signal interfacing between transmission medium (power line, cable, twisted pair) and the digital baseband processors and controllers. A new family of mixed-signal front-ends (MxFE™ integrated circuits) provide the compact electronics to bridge this gap flexibly with high performance at low cost (AD9875/AD9876).

Interfacing a Blackfin DSP to High-Speed Converters for Wireless Applications

A new generation of fast, low-power, programmable general-purpose signal processors—ADI's Blackfin™ family—is allowing designers to avoid the costs of custom digital hardware. Soon-to-be-released new family members will enable a wide range of wireless applications. But an early member of the Blackfin family can be applied to outpace existing approaches—even though this DSP does not have a "wireless-ready" interface.

X-Amp™, A New 45-dB, 500-MHz Variable-Gain Amplifier (VGA), Simplifies Adaptive Receiver Designs

The AD8367 is a wideband, variable-gain amplifier with gain (in dB) accurately proportional to the control voltage. An on-chip square-law detector allows it to be used directly in automatic gain control (AGC), to maintain a preset rms output amplitude, irrespective of the input amplitude and waveshape, with a minimum of external components.

SigmaDSP™ Digital Audio Processing

SigmaDSP processors, such as the new AD1954, are fully integrated in both hardware and software to provide low-cost, zero-hassle, fully configurable processing of digital audio signals from sources such as CDs, DVD-Audio, SACD, and MP3, and deliver stereo and subwoofer analog signals via D/A converters with 112-dB signal-to-noise ratio.

Copyright 1995- Analog Devices, Inc. All rights reserved.