![]() |
|||
![]() |
![]() |
![]() |
![]() |
|
Volume 36, Number 2, March-April, 2002
Versatile Mixed-Signal Front Ends Speed Customized Design of Wireline Broadband Modems and INTRODUCTION
Figure 1. Home-networking/broadband access configuration. A variety of technologies have been developed to address high-speed communication between home computers and peripheral devicesand to interface to the hub (or gateway) for broadband access. Until recently, Ethernet has been the most viable method for providing networking within the home. The attractiveness of Ethernet has been the availability of inexpensive network interface cards based on proven technology. However, Ethernet suffers from one main disadvantagethe requirement of having Category 5 (CAT5) cable wired throughout the home. This almost always means the homeowner must run new wiresa cumbersome and potentially expensive solution. Wireless LAN provides an alternative to Ethernet that doesnt require installation of new wires. Despite the convenience of a wireless solution, it has achieved limited success due to higher cost, potential insecurity, multiple competing standards, lack of interoperability, and interference/robustness concerns. Recent advancements in the wireless standards within IEEE 802.11 and the emergence of the WiFi consortium have increased the prospects for wireless home networking. Nevertheless, the scarcity of frequency spectrum and the ubiquity of potent interfererssuch as microwave ovens, garage door openers, etc.will continue to pose numerous challenges to a wireless home network, including increased cost. The newer preferred wireline technologies are those that require no new wire; they offer the homeowner a potentially better way of establishing a home network by avoiding the burden of installing new cabling, while providing comparable performance to that of Ethernet at an affordable price. The two choices for operating over the installed infrastructure involve either telephone- or the power-line wiring. Until recently, utilizing this existing home wiring for broadband networking was impossible due to very poor channel quality. However, cost-effective broadband home networking is now a reality because of advances in signal-processing techniques, lowered costs resulting from persistent reduction of silicon fabrication geometries, and performance improvements in high-speed mixed-signal circuitry. The Home Phone Networking Alliance (HPNA) standard provides the framework for phone-line networking and allows data rates of up to 10 Mbits/s. And the HomePlug standard describes the specifications for implementing a power-line network system with data rates comparable to those of HPNA. These wireline home networking technologies, together with high-speed access technologies like DSL and cable, require mixed-signal interfacing between the transmission medium (power line, cable, twisted pair) and the digital baseband processors and controllers. Analog Devices has developed a family of monolithic mixed-signal front-end (MxFE) integrated circuits (ICs) to bridge this gap (see Analog Dialogue Volume 35, Number 1, January-February, 2001 article, AD9873 Mixed-Signal (MxFE) Front-End for Broadband Digital Set-Top Boxes). The recently introduced AD9875 and AD9876 MxFE devices, to be discussed in this article, were developed and aimed specifically at broadband home-networking and broadband-access applications, both of which require high data rates or signal bandwidth up to 25 MHz and impose similar demands in functionality, performance, and cost. Given their flexibility, these parts can be used in modems for both home networking (HomePlug, HPNA) and high-speed data access (VDSL, power line). Developed for large volume, cost-sensitive, consumer-class applications, they offer exceptional value to providers of system solutions. Figure 2 depicts the versatile role played by the MxFE chip. Its receive (Rx) circuitry accepts the (analog-domain) signals from the transmission medium, once they have been appropriately interfaced, and provides analog signal conditioning and A/D conversion to produce multiplexed digital signals that can be dealt with by the digital physical layer (PHY) and/or media access controller (MAC). It also accepts digital data from these entities, processes it and converts it to analogand outputs this transmit (Tx) signal to the media interface. The device design is based on the objective of optimizing system performanceirrespective of the analog or digital nature of its I/Oas implemented in ADIs smart-partitioning methodology (see Appendix).
Figure 2. Typical wireline network node. Figure 2 represents a typical wireline network node. The MxFE function may be connected to the wireline medium passively through a hybrid transformer block, or actively, with an amplifier on the receive side and a driver on the transmit side. On the digital side, the MxFE device needs to interface with the PHY and the MAC, which reside on a separate chip. Critically important factors for the designer of MxFE circuitry for the home networking and high-speed access markets are performance, time to market, and low cost. In this type of emerging broadband communication application, discrete analog components can be prohibitively expensive, power-hungry, and demanding of board space. The combination of cost, performance, size, and power dissipation made possible by integrating the difficult mixed-signal, analog, digital, and signal processing functions on a single chipsuch as the AD9875/AD9876makes complex consumer-market communication products feasible. In fact, by implementing their intellectual property and design expertise in a digital gate array or ASIC, in conjunction with these devices, design engineers can develop new products and prototypes faster than ever to capitalize on rapidly changing markets. Figure 3 shows a block diagram of the AD9875/AD9876 mixed-signal front-end converter for broadband modems. On the analog side, the AD9875 and AD9876 combine the ADC, DAC, clock generation, programmable-gain amplification, and analog and digital filtering circuitry to provide a level of integration and performance usually implemented with discrete solutions costing significantly more. The ADC uses a pipelined multistage architecture to achieve high sample rates while consuming low power. In the AD9875, the receive path provides 9.5 ENOB at 32 MSPS and 8.6 ENOB at 50 MSPS. Comparable numbers for the AD9876 are 10.2 ENOB @ 32 MSPS and 9.3 ENOB @ 50 MSPS. The DACs in each device are, respectively, 10- and 12-bit interpolating TxDAC™ circuits. On the digital side, the DAC inputs and ADC outputs are available on separate ports to accommodate both full-duplex and half-duplex operations. Each converters port is multiplexed into high- and low nybbles to reduce the number of package pins. [A 10-bit half-duplex device, the AD9875-HD, available in summer 2002, will connect seamlessly to currently available HomePlug-compliant physical-layer digital ASICs that support multiplexed transmit and receive data ports.]
Figure 3. AD9875/6 block diagram. The availability of low-cost, flexible, high-performance, off-the-shelf mixed-signal front-ends, such as these, with optimized functionality for broadband modem design using a variety of modulation formatsincluding OFDMsimplifies the ASIC design, specification, and testing process for both vendor and OEM and can substantially cut time to market. The unique features of the AD9875/AD9876 make these parts ideal for phone and power line networking as well as some xDSL applications. Broadband wireline modems The main function of the transmit path is to send the signal onto the line with sufficient fidelity to reach the far end of the wire with a high-enough signal-to-noise ratio (SNR) to allow faithful decoding at the receiver end. Invariably, the transmitter must also do this while conforming to a spectral mask to ensure that the modem does not cause excessive noise outside its channel bandwidth. Meeting the requirements of a power spectral-density (PSD) mask usually drives the design and performance requirements of the transmit path components. The two converter parameters that get the most attention are the number of bits and the sampling rate. For the DAC, the number of bits required will depend on the desired SNR, the signals peak-to-average ratio (PAR) and the ratio of the signal bandwidth to the sample rate. For a given SNR requirement, higher-precision converters are required as signal bandwidths and PARs increase. Often the most demanding DAC performance parameter turns out to be its spurious-free dynamic range (SFDR). The spurs generated by the non-ideal DAC transfer function may show up anywhere in the spectrum. If the magnitude of the spurs are high and fall close to the signal band, they may be impossible to filter adequately. The DACs SFDR performance must be able to meet the system linearity requirements. The AD9875/AD9876 incorporates a 10-/12-bit DAC and makes use of interpolation filters to oversample the input data. Oversampling, because it moves DAC image frequencies away from the frequency of the desired signal, may result in substantially simpler external analog filter requirements, which translate into lower complexity and cost. Ideally, the driver will be able to provide the transmit-path gain and deliver the required output power while maintaining the DAC linearity performance. In cases where the DACs available peak output power is not sufficient, AD832x cable drivers or AD8xxx DSL drivers could provide the interface to the wire. To deliver high peak-output signal with low distortion requires high voltage rails and high bias currents in the amplifiers output stage, which conflicts with the need for low power consumption and CMOS integration. The method of coupling the modems analog front-end to the line depends on whether the type of modulation/demodulation (modem) is time-domain duplex (TDD) or frequency-domain duplex (FDD). A TDD modem will normally employ a simple transformer coupling to the line and a switch that connects either the transmitter or receiver to the transformer. The main concern is that the switching and settling times, when the connections are made, meet the system requirements. An FDD modem will normally employ a hybrid to connect the modems analog front-end to the line. A hybrid is required because the modem can be transmitting large signals while the receiver is listening to greatly attenuated signalswhich can be orders of magnitude smaller. In order to limit the amount of signal coupling from the transmitter to the receiver, some type of line matching, cancellation circuitry, and filtering is used. The AD9875/AD9876 integrates a low-pass analog receive filter (LPF in Figure 3) with variable cutoff to provide for various signal bandwidth requirements. The effectiveness with which the receiver maintains the SNR of the incoming signal within the receive channel bandwidth will be the most important determinant of the modems raw data rate. The SNR of the receive signal over the signal bandwidth, determined by the channel; puts a fundamental limit on the amount of data the channel will carry. Any degradation beyond this in the circuitry between the line interface and the digital output samples is considered implementation noise and is determined by the quality of the receiver. It is the receivers job to eliminate out-of-band channel noise and compensate for signal attenuation, then digitize the analog signal for further digital signal processing. The out-of-band noise and interference on the line reduce the receiver SNR in two ways. First, the noise present may be folded back into the signal band of interest by the sampling process, raising the existing noise floor. Second, if the noise and interference are orders of magnitude greater than the desired signal, this will reduce the gain that can be applied to the signal to compensate for signal attenuationagain resulting in lower SNR. Effective filtering is essential to reduce these effects. In order to optimize noise- and distortion performance, a variable-gain amplifier is implemented on-chip. This function is shared by a continuous-time programmable gain stage (CPGA in Figure 3) and a discrete-time switched programmable gain stage (SPGA), sandwiching the LPF. Following the SVGA, a 12-/10-bit ADC digitizes the signal with sampling rates up to 50 MHz. Several auxiliary function are also present on-chip. Two phase-locked-loop (PLL) blocks, a voltage-regulator control circuit, and a serial-port interface help reduce external component count and optimize performance. Phone-line networking
Power-line and VDSL modems AD9875/AD9876 Key Features, Specifications, and Performance
AD9875/AD9876 performance was characterized over the 40° to +85°C extended industrial temperature range. The following two graphs show the transmit-path performance in multi-tone applications of these parts and illustrate their exceptional linearity. Figure 6 shows intermodulation-distortion of the AD9876; under the indicated conditions, it is less than 80 dB. Figure 7 shows the multi-tone power ratio of the transmit path: about 55 dB when transmitting 70 tones in the 4.5 to 20.7-MHz frequency range, corresponding to the HomePlug frequency band.
Figure 6. Dual-tone spectral plot of AD9876's 12-bit DAC @ fDATA = 50 MSPS,
Figure 7. In-band multi-tone spectral plot of AD9876's 12-bit DAC @ fDATA = 50 MSPS, The AD9876 12-bit ADCs performance meets the requirements for two-band VDSL and has been designed into system solutions for that application and for power line access modems. Figure 8 is a plot of THD as a function of ADC sampling rate for a 5-MHz sinusoidal input.
Figure 8. AD9876 12-bit ADC THD performance vs. fADC @ fIN = 5 MHz. The Rx LPF of the MxFE device has two frequency settings, one with a center frequency of about 10.8 MHz, the other at about 26 MHz. The filter transfer function is similar to that of a fourth-order Butterworth. The filters have a self-tuning feature that corrects for variation in device elements from part to part and for temperature drift. The center frequency can be adjusted over a 20% range if different cutoff frequencies are desired. Figure 9 shows LPF performance with the lower cutoff frequency selected.
Figure 9. AD9876 Rx LPF frequency response, low fC.
The AD9875/6 evaluation board (Figure 10), with its software, allows users to easily program and quickly evaluate the device for a specific modem application. The evaluation board provides connector access to the devices digital transmit and receive portswhich are buffered for reliable data transmission. The on-chip configuration registers can be programmed through the use of a PC serial port, which connects directly to a connector on the evaluation board; and the PC-resident evaluation-board software provides for a simple means of configuring the MxFE operation. The analog output from the DAC, and the analog input to the ADC circuitry can be accessed through SMA connectors or pin headers on the evaluation board. The jumper programmable interface configurations allow several different circuit options to suit different testing methods. An on-board digital loopback feature allows the ADC and DAC to be tested simultaneously with the use of a signal source and spectrum analyzer. Also available is a daughter card, which can provide a phone line compatible interface to the MxFE device. The AD9875-EB software provides a graphical user interface for easy programming and querying of the AD9875 registers. Three programming windows are available. The direct-register-access window allows AD9875 write- and readback in decimal, binary or hexadecimal data formats. The register-map window provides easy, function oriented programming of the AD9875 registers. This window displays graphically all of the MxFE functions on the screen. The advanced-register-access window allows programming of sequences of register accesses. Figure 10. AD9875/6 evaluation setup. Availability APPENDIX Besides its performance and cost advantages, smart partitioning provides a logical place for the division of labor in developing complete physical-layer solutions. Companies whose core competencies are in the development of communications systems and algorithms can concentrate on those aspects of the digital design and capitalize on their differentiating technology. They can rest assured that their combined analog and mixed-signal solution is at the state of the art by partnering with a leader in the field, such as Analog Devices. [Return to text] |
||||||||