![]() |
|||
![]() |
![]() |
![]() |
![]() |
|
Volume 35, Number 3, June-July, 2001
High Performance Narrowband Receiver Design Simplified by Mobile radios are used for public safety and emergency servicessuch as police, fire and ambulanceas well as for private services, such as fleet management. Increasingly, in order to provide enhanced services, along with improved spectral efficiency and coverage, the design of these radios has moved from traditional analog-based modulation schemessuch as FM and PMto digital modulation approaches. Receivers for these radios must be capable of accurately digitizing a low-level, high-frequency signal in the presence of large interfering signals. In radios using some narrowband mobile standards, interfering signals can be 70 dB greater than the desired channel, with frequency offsets as small as 25 kHz. Since these systems usually aren't cellular, the geographical coverage range of mobile radios is also an important featurethey must possess excellent sensitivity to recover low-level signals originating from subscribers at the fringe of the coverage range. As a further complication, these radios are often portable with high rates of usage; they demand low power consumption using smaller, longer-lived batteries. As an aid to equipment designers, Analog Devices has made avahe AD9870 IF Digitizing Subsystem, an IC designed to meet the demanding requirements of mobile radio and similar narrowband radio applications with superheterodyne architectures employing analog and/or digital modulation schemes. The AD9870 integrates the entire IF strip with minimal external components. It can accept an IF signal at frequencies as high as 300 MHz, with bandwidths up to 150 kHz, and provides a serial data output containing 16-bit I and Q data, which can then be demodulated with a host processor. The AD9870 is intended for both base stations and subscriber units, combining the dynamic range required by base stations with the low power consumption needed by portable radios.The big problem in all receivers is dynamic range
Figure 1. The "Big Problem" in all receivers is dynamic range! Assume for the moment that the only signal present in the spectrum is the "small target signal." The minimum detectable signal, or sensitivity, will be determined by the signal bandwidth (B), the receiver's detection threshold, (SNRMIN), the receiver's noise figure, (NF), and inherent thermal noise limitations (kTB). At a temperature of 290 K, the sensitivity can be estimated with the following equation: Sensitivity = SNRMIN + 10log(B)+NF+(-174 dBm/Hz) Here are some of the potential noise sources: Low-frequency 1/f noise becomes an issue if insufficient gain is applied to the target signal prior to down-conversion to frequencies below the 1/f corner of the process technology. DC components caused by offsets and 2nd-order distortion can also be problematic. A large interferer can have its energy spread over a broad range of frequencies by the phase noise of the receiver's LO, through a process known as"reciprocal mixing." The larger the interferer and the closer it is to the target signal, the more likely that the target signal will be corrupted by this noise transfer mechanism. Also, if this interferer is large enough to induce nonlinearities in the receiver's front-end circuitry, it is possible for a spurious component to mix back into the target signal's passband. The "half-IF" problem is a specific case afflicting receivers with poor second-order linearity, in which an interferer falling halfway between the LO and the target signal generates a second-order component, which mixes with the LO's 2nd harmonic to generate a spur falling on the target signal. The IIP2 specification of a receiver allows a receiver designer to quantify the "half-IF" spur. The difference, or Two large interferers at equally spaced frequency offsets (i.e., f0 + Superheterodyne architecture
Figure 2. Typical superheterodyne architecture for a digital receiver. Prior to RF-to-IF down-conversion, a band-select filter (duplexer) and/or image reject filter selects the entire RF band within which the target signal operates. The low-noise amplifier (LNA), which provides amplification of the intended RF band prior to down-conversion, is critical in determining the receiver's sensitivity. The down-converted IF spectrum following the RF mixer often contains an array of signals of varying strengths in addition to the target signal. Channel selection and amplification occurs at IF: the target signal is selected from among the other signals via one or more crystal or SAW-type passive filters. After filtering, the target signal undergoes further amplification, with its signal strength stabilized at a preset level by an AGC loop to optimize the quadrature demodulation process. In many digital receivers, an IF analog quadrature modulator separates the IF signal into its quadrature baseband I and Q components, which are then digitized by a dual ADC. In such cases, the modulation accuracy of the demodulated signal is quite sensitive to analog offsets, quadrature LO mismatch, and I/Q gain mismatch in the quadrature modulator and dual ADC.
AD9870 architecture
Figure 3. The AD9870 simplifies the digital receiver while enhancing performance. The AD9870 differs from the typical superheterodyne architecture by employing a wide-dynamic-range bandpass sigma-delta ADC to sample a 2nd-IF signal, along with any neighboring interferers. The demodulation of the target IF signal is performed with digital accuracy and stability, while the intrusive nearby interferers can be suppressed via digital filtering. Figure 4 shows a functional block diagram of the AD9870. Functioning similarly to the RF portion of the superheterodyne architecture, an LNA and mixer are used to amplify and down-convert the target signal centered at the 1st-intermediate frequency to a lower 2nd IF suitable for digitization by the bandpass ADC.
Figure 4. Functional block diagram of the AD9870 shows the level of integration. The LNA and mixer provide approximately 10.5 dB of gain, while preserving system dynamic range with an input noise figure of 9 dB and 3rd-order intercept of 0 dBm. The high input impedance (360 ohms) simplifies interfacing to crystal or SAW filters. An on-chip LO PLL synthesizer can be used in conjunction with an external loop filter and VCO to generate a tunable LO frequency. The 2nd-IF signal is centered at exactly 1/8th the bandpass ADC sample rate (i.e., Embedded in the AAF is a variable-gain amplifier (VGA), which provides up to 26 dB of gain range (Figure 5). The VGA gain, which extends the dynamic range of the AD9870, can be programmed either directly or controlled by an automatic gain-control (AGC) loop. The AGC loop is typically invoked under strong signal conditions to prevent "overloading" or clipping of the A/D converter by maintaining a programmable fixed signal level at the ADC input. The AD9870 implements the AGC function with a highly effective hybrid approach, as shown in Figure 5: the analog and digital domains work together in signal estimation and control.
Figure 5. A "hybrid" AGC control loop extends the dynamic range of the AD9870. In situations where a strong target signal or interferer falls within the bandwidth of the first-stage decimate-by-20 digital filter, the signal is estimated digitally and compared to a programmed reference level (AGCR). The difference between the two levels is fed to a digital integrator, which updates a control DAC to adjust the analog voltage of the VGA. Since a strong interferer falling outside of the passband of the 1st-stage digital filter can not be accurately estimated, an analog loop based on a simple differential comparator monitors the input to the ADC and assumes control of the loop during any overrange condition, to reduce the VGA gain. An external capacitor is used to smooth the transitions of the DAC, with a time constant established by its capacitance and the internal source resistance of the DAC. The R-C cutoff frequency is typically set well outside the control system's loop bandwidth to ensure continual digital control of the loop dynamics. The control loop bandwidth is digitally programmable with attack- and decay times variable over a wide range and the ability to react to any overload condition. The instantaneous dynamic range of any narrow-band receiver signal chain containing a VGA is dependent on the specific gain setting of the VGA, since the ratio of noise that is contributed by each stage in the signal path to the "overall" input-referred noise decreases as the gain of the preceding stage increases. This implies that input noise described by its noise figure, NF, is typically dominated by the first few stages (i.e., LNA and mixer), and noise sources at the end of the signal chain (i.e. the ADC) have minimal effect upon the system's NF, provided that there is sufficient gain between these blocks.
Figure 6. Dynamic range of AD9870 depends on VGA setting. In the case of the AD9870, the VGA's gain is nominally adjustable over a 25-dB range . Figure 6 shows how the AD9870's noise figure is impacted by the VGA gain setting as a target signal's (or interferer's) input power is increased from 85 to 23 dBm. Under small-signal conditions, the VGA is set to max gain; the AD9870's noise figure is set by the LNA/mixer as well as the VGA's input noise. However, as the signal power is increased, it reaches a point (depending on the AGC reference level) at which the VGA's gain begins to decrease to prevent ADC clipping. At this point, the VGA gain is reduced, dB for dB, as the signal power is further increased. Also, in this region, the input signal level to the ADC remains constant and the noise of the ADC begins to dominate, so that the system's NF degrades also at a 1-dB-per-dB rate. As the signal power continues to increase, a point is reached (i.e., 26 dBm) at which the gain of the VGA is set to its absolute minimum and further increases in signal level are seen at the ADC input until clipping occurs (i.e.,The "heart" of the AD9870that makes a low 2nd-IF digitization approach feasible and practical in an IC intended for radio systems requiring high dynamic range with minimal power consumptionis its bandpass sigma-delta ADC (Figure 7). This ADC, together with the back-end digital decimation filters, achieves nearly 14.5-ENOB performance within a 10-kHz bandwidth, while sampling a signal centered at frequencies as high as 2.25 MHz. It achieves these specifications while drawing a mere 13 mA from a 3.0-V power supply.
Figure 7. Multi-bit 4th-order bandpass The sigma-delta ADC is based on a 4th-order switched-capacitor , multi-bit modulator consisting of two cascaded resonators that provide two complex pairs of zeros in the noise transfer function (NTF), falling near CLK/8. The location of these complex zeros at the 2nd-IF frequency, along with the multibit feedback path, help ensure a low noise floor in a narrow region (±3.3% of CLK/8) around the 2nd-IF frequency. The digital output data from the ADC is fed into the digital signal-processing section of the AD9870 (Figure 8). This section consists of an CLK/8 complex (or quadrature) demodulator, followed by three linear-phase FIR filters. The complex demodulator separates the target 2nd-IF signal, centered at CLK/8, into its I/Q components prior to filtering.
Figure 8. Digital quadrature demodulation, followed by programmable Availability Prices, where indicated here, are recommended resale prices (U.S. Dollars) FOB U.S.A. Prices are subject to change without notice. For specific price quotations, get in touch with our sales offices or distributors. |