|
Go to Previous Page: Contents
Go to Next Page: Single- and dual- axis micromachined accelerometers (ADXL150, ADXL250)
Editor's Notes
THIRTY YEARS OF ANALOG DIALOGUE

In Volume 15 1 (1981), in celebration of 15 years in print, we listed the first 15 years of Analog Dialogue cover features. At that time, we wrote: . . . will mark the 15th year of publication of this journal, and the 13th year of our stewardship. While adding a copy of the [most recent] issue to our bulging binder, we nostalgically
turned the pages of issues long forgotten. The amount of technological progress reported in them surprised even us. Before the list expands beyond the capacity of this column, we thought you might be interested in seeing a roll of just the cover stories alone, though much significant progress never attained the cover. In this spirit, in celebration of our 30th year in print (and 28th of stewardship), here are the second 15 years of cover themes:
| 1981 |
15 2 |
D/A converters for graphic displays |
| 1982 | 16 1 | High performance hybrid circuit isolation amp (AD293) |
| 16 2 | Dual monolithic multiplying DACs (AD7528) |
| 16 3 | Monolithic instrumentation amplifier (AD524) |
| and thermocouple preamp (AD594) |
| 1983 | 17 1 | CMOS ICs for digital signal processing |
| 17 2 | Quad CMOS DAC with buffered voltage outputs |
| 1984 | 18 1 | Amplifier noise basics revisited |
| 18 2 | Monolithic V out µP compatible 12 bit DAC (AD667) |
| 18 3 | An intelligent vision system for industrial image analysis |
| 1985 | 19 1 | Multifunction analog IC computes y(z/x)m, etc. (AD538) |
| 1986 | 20 1 | Low cost, high performance, compact iso amps (AD202/4) |
| 20 2 | Fast, flexible CMOS DSP µP (ADSP 2100) |
| 1987 | 24 1 | Monolithic process control transmitters (AD693) |
| 21 2 | Complete 8 bit 400 ksps analog I/O (AD7569) |
| 1988 | 22 1 | Chipset for 50 Mbit/s digital data recovery (AD890/891) |
| 22 2 | 200 MSPS 8 bit IC ADC with 250 MHz BW (AD770) |
| 1989 | 23 1 | Isolated sensor to serial with a screwdriver (6B Series) |
| 23 2 | Single chip DSP microcomputer (ADSP 2101) |
| 23 3 | DC 120 MHz IC log ampaccurate compression (AD640) |
| 23 4 | Pin electronics for high speed ATE (AD1315/1521/22) |
| 1990 | 24 1 | Monolithic 75 MSPS 10 bit flash converter (AD9060) |
| 24 2 | Mixed signal processor: DSP/ADC/DAC (ADSP 21msp50) |
| 24 3 | RAM DAC upgrade enhances VGA graphics (AD7148) |
| 1991 | 25 1 | Pro Logic decoder: Dolby Surround Sound (SSM2125) |
| 25 2 | ADSP 21020 floating point high speed DSP |
| 1992 | 26 1 | Mixed signal chips drive digital radio (AD7001/7002) |
| 26 2 | Wideband linear in dB VCA (AD600/602) |
| 1993 | 27 1 | Fast precise 155 Mbps fiberoptic timing recovery (AD802) |
| 27 2 | Single chip micromachined accelerometer (ADXL50) |
| 1994 | 28 1 | Dual setpoint single chip temperature controller (TMP01) |
| 28 2 | Complete, low distortion 500 MHz IC mixer (AD831) |
| 28 3 | SHARC Floating point DSP: tops in memory, performance |
| 1995 | 29 1 | Integrated stereo codecs for multimedia (AD1843/1845) |
| 29 2 | Meeting the challenges of high speed |
| 29 3 | Considerations in low power, single supply system design |
| 1996 | 30 1 | Read channel processor uses PRML with MR heads |
| 30 2 | DSP based chip set for ac motor control (ADMC201) |
| 30 3 | CMOS DACs optimized for transmit path (AD976x family) |
| 30 4 | Dual axis accelerometer (ADXL250) |
Dan.Sheingold@analog.com
THE AUTHORS
 |
Howard Samuels is
a Product Development Engineer in ADIs Micromachined Products Division in Wilmington, MA. He joined Analog after graduating from Carnegie Mellon University in 1982 with a BS in EE and Applied Mathematics. He holds several patents and has published articles in trade magazines.
Howard has designed signal conditioners and isolators, including the AD210 3 port isolator. When not at work, he enjoys caring for and taking pictures of his new baby. |
 |
Matt Smith is a Senior Applications Engineer at our Limerick, Ireland, facility. He is responsible for Interface and Supervisory products. He holds a B.Eng from the University of Limerick. His leisure interests include playing squash, motor maintenance and more recently, woodworking. |
 |
Bill Slattery has marketing responsibility for products of the Digital Video Group at ADIs Limerick facility, including video DACs, RAM DACs, and video encoders & decoders. Earlier, he worked as a Senior Engineer in the Applications Group in Limerick. Bill has a BSc (Eng) degree from the University of Dublin (Trinity College) and an MBA from the University of Limerick. A licensed private pilot, he enjoys flying his airplane. |
 |
Jürgen Kühnel is a Senior Marketing Engineer for Power Management products, located in Munich. Since joining ADI in 1984, he has had various roles in Sales and Marketing in Central Europe. His Dipl. Ing. is from the Technische Fachhochschule in Berlin, and he worked for several years as a system designer in medical and chemical instrumentation. In his spare time he likes riding on two wheels (powered or not) and designing electronic systems for his model railroad. |
Dave Robertson is a design engineer in the Analog Devices High-Speed Converter group in Wilmington, MA. His photo and a brief biography appeared in Analog Dialogue 30-3.
Erik Barnes is an Applications Engineer for ADIs High Speed Converter Group in Wilmington, MA. His photo and a brief biography appeared in Analog Dialogue 30-3.
Go to Previous Page: Contents
Go to Next Page: Single- and dual- axis micromachined accelerometers (ADXL150, ADXL250)
|