|
Considerations In Designing Single Supply, Low-Power Systems Part II: Battery Powered Systemsby Steve GuintaPart I of this two-part series (Designs using ac line power) appeared in the last issue of Analog Dialogue (29-3). In it, we discussed the implications and performance tradeoffs in converting to a single-supply system using conventional (i.e., non-single supply characterized) active devices, such as op amps, A/D and D/A converters, etc., then further described several new product families and processes from Analog Devices that provided single-supply operation without the limitations on speed and dynamic range of conventional devices. We continue here with the considerations involved in design for low-power operation, particularly for portable and remote applications with batteries.
BATTERY-POWERED SYSTEMSIn a battery-powered system, time is the critical parameter. Unlike ac-powered systems, where supply voltage varies within a specified range and the availability of rated current is unlimited in duration, a battery can only supply power for a finite length of time before it requires recharging or replacement. In addition, as the battery discharges, the greater the current drain, the greater the drop in battery voltage (or supply rail) (Figure 1).
Figure 1. Cell discharge as a function of current dis-charge rate.] The key to designing an efficient battery-operated system, then, is (a) to maximize battery life by minimizing the current drawn by the circuit, especially the continuous "quiescent current"; and (b) if necessary, to maintain the voltage supplied to the load at a constant level during discharge by using some form of regulating circuit between the battery and the load. For example, a battery with a capacity of 100 mA-hour powering a circuit that draws 1 mA will operate for approximately 100 hours before recharging or 9 replacement is required. If this quiescent current is reduced to 100 mA, the battery life ideally increases to about 1,000 hours. Before designing a battery-operated system, it is important to understand the environment, requirements, and operating conditions under which the system will be used; this will allow the designer to determine what type of battery should be used (for example, primary or secondary), and how often the batteries would need to be replaced or recharged. For example, systems such as portable industrial data loggers or emergency medical monitors often can be recharged overnight (or when not in use), and so a secondary, or rechargeable, battery could be used. On the other hand, such low-power, battery-powered equipment as remote weather stations, seismic data recorders, or signalling beacons might be required to operate for weeks or even months without battery replacement or recharging; for such applications, a "throwaway" primary-type battery might be chosen. Regulating the battery output: A regulator between the battery and the load keeps the supply rail at constant voltage during battery discharge. This can be important for several reasons:
For example, most precision op amps exhibit a power supply rejection (PSR) at DC of the order of 120 to 100 dB. This is equivalent to 1 to 10 microvolts per volt of supply change. If the supply (battery) voltage were to drop from 5.0 V to 3.0 V, then the shift in input offset voltage would be
For a supply rejection of 100 dB (to 0.001%), this would equate to an offset change of 20 µV. This could represent a substantial number of degrees in a temperature monitoring system using sensitive B, R, and S type thermocouples, with temperature sensitivities of the order of 10 µV/°C or less. Figure 2. Voltage regulator and effect of battery discharge.
Figure 2. Voltage regulator and effect of battery discharge. Some designers may use the supply rail as the reference for analog-to-digital and/or digital-to-analog converters. Unless the measurement is ratiometric, the use of raw battery output as a voltage reference can lead to accuracy problems. For example, a two-volt shift in battery voltage can cause a 40% drop in the scale factor of a data converter. An n-bit A/D or D/A converter has an LSB (least-significant bit) weight of V(REF)/2 n . Comparing 5 V with V of supply voltage, used as a reference: 2exp(n) 5 V 3 V 2exp(-12) 1.22 µV 732 µV 2exp(-16) 76 µV 46 µV Voltage regulator devices, such as the REF19x series, are useful in stabilizing supply or reference voltage. They will maintain their output voltage at a constant level until the regulator reaches its "drop-out" voltage, i.e., the value at which the regulator can no longer hold its output constant (Figure 2). The use of a regulator does require somewhat higher battery voltage, but a type with low dropout voltage can minimize the use additional cells. For example, the 3-V REF193's dropout voltage ranges from 0.8 V with 10-mA load to 0.3 V with minimal load. Extending Battery Life: Three ways to extend battery operation are: (1) Minimize the quiescent current if continuous operation is needed; (2) Pulse the load on and off so that the battery operates on lower duty cycle; and (3) Power down the circuit when not in use.
|
|