With the exception of the Supervisor Parametric Search, the following stand-alone tools generate a power supply design complete with a schematic, bill of materials, and performance specifications including efficiency based on the user's preference for size, efficiency, and cost.
- ADI Power Management Tools (Size: 220 MB)
WARNING!!! The above ZIP files is very large! It contains all of the tools listed below for all of the parts listed below.
- ADI Power Discovery Tool (Version: 0.17 Size: 7.37 MB)
This Excel tool offers selection tables for most subcategories, and a parametric search for some subcategories. The subcategories with a parametric search have either lots of parts, lots of models, lots of features, or a combination of the above. The parametric search helps you reduce the solution set to those parts meeting your needs.
- ADI Linear Regulator Design Tool and Parametric Search (Version: 2.14 Size: 6.22 MB)
ADP120, ADP121, ADP122, ADP123, ADP124, ADP125, ADP130, ADP150, ADP151, ADP160, ADP161, ADP162, ADP163, ADP170, ADP171, ADP172, ADP220, ADP221, ADP223, ADP224, ADP225, ADP320, ADP322, ADP323, ADP1706, ADP1707, ADP1708, ADP1710, ADP1711, ADP1712, ADP1713, ADP1714, ADP1715, ADP1716, ADP1720, ADP1740, ADP1741, ADP1752, ADP1753, ADP1754, ADP1755, ADP2140, ADP3300, ADP3301, ADP3303, ADP3309, ADP3330, ADP3331, ADP3333, ADP3334, ADP3335, ADP3336, ADP3338, ADP3339, ADP3367, ADP667, ADP7102, ADP7104, ADP7182
- ADP161x Boost Regulator Design Tool (Version: 1.14 Size: 15.8 MB)
ADP1612, ADP1613, ADP1614
- ADP161x SEPIC-Cuk Design Tool (Version: 1.15 Size: 9.20 MB)
ADP1612, ADP1613, ADP1614
- ADP161x Coupled-SEPIC Design Tool (Version: 1.41 Size: 8.27 MB)
ADP1612, ADP1613, ADP1614
- ADP1621 Boost Regulator Design Tool (Version: 1.34 Size: 5.00 MB)
ADP1621
- ADP1621 Cuk Design Tool (Version: 1.31 Size: 5.30 MB)
ADP1621
- ADP1621 Coupled-SEPIC Design Tool (Version: 1.33 Size: 5.71 MB)
ADP1621
- ADP182x Buck Designer Tool (Version: 2.27 Size: 26.5 MB)
ADP1821, ADP1822, ADP1823, ADP1828, ADP1829
- ADP1850-77 Buck Designer Tool (Version: 4.3 Size: 23.9 MB)
ADP1850, ADP1877
- ADP1851_53 Buck Designer Tool (Version: 1.40 Size: 18.8 MB)
ADP1851, ADP1853
- ADP1864 Buck Controller Design Tool (Version: 1.31 Size: 15.5 MB)
ADP1864
- ADP187x Buck Designer Tool (Version: 1.12 Size: 16.4 MB)
ADP1870, ADP1871, ADP1872, ADP1873, ADP1874, ADP1875, ADP1878, ADP1879 [Does not include the ADP1877]
- ADP2114/16 Dual Buck Regulator Design Tool (Version: 1.8 Size: 7.07 MB)
ADP2114, ADP2116
- ADP21xx Buck Regulator Design Tool (Version: 2.13 Size: 8.56 MB)
ADP2105, ADP2106, ADP2107, ADP2108, ADP2109, ADP2118, ADP2119, ADP2120, ADP2138, ADP2139, ADP2164
- ADP230x Buck Regulator Design Tool (Version: 1.9 Size: 10.2 MB)
ADP2300, ADP2301, ADP2302, ADP2303
- ADP230x Inverting Buck-Boost Regulator Design Tool (Version: 1.9 Size: 6.35 MB)
ADP2300, ADP2301, ADP2302, ADP2303
- ADP232x Buck Regulator Design Tool (Version: 4.3 Size: 6.59 MB)
ADP2323, ADP2325
- ADP237x Buck Regulator Design Tool (Version: 1.21 Size: 5.79 MB)
ADP2370, ADP2371
- ADP238x Buck Regulator Design Tool (Version: 2.11 Size: 7.37 MB)
ADP2380, ADP2381, ADP2384, ADP2386
- ADP238x Inverting Buck-Boost Regulator Design Tool (Version: 1.23 Size: 6.24 MB)
ADP2380, ADP2380, ADP2384, ADP2386
- ADP244x Buck Regulator Design Tool (Version: 1.36 Size: 5.13 MB)
ADP2441, ADP2442
- ADP2503/4 Buck Boost Regulator Design Tool (Version: 1.25 Size: 4.18 MB)
ADP2503, ADP2504
- ADP3050 Buck Regulator Design Tool (Version: 1.27 Size: 8.41 MB)
ADP3050
- ADP505x Buck Regulator Design Tool (Version: 0.64 Size: 7.51 MB)
ADP5050, ADP5051, ADP5052, ADP5053
- ADI Supervisor Parametric Search and Cross-Reference v. 2010B
ADM1184, ADM1232, ADM12914, ADM13305, ADM13307, ADM1810, ADM1811, ADM1812, ADM1813, ADM1815, ADM1816, ADM1817, ADM1818, ADM2914, ADM6305, ADM6306, ADM6315, ADM6316, ADM6317, ADM6318, ADM6319, ADM6320, ADM6321, ADM6322, ADM6326, ADM6328, ADM6339, ADM6346, ADM6348, ADM6384, ADM6710, ADM6711, ADM6713, ADM6821, ADM6822, ADM6823, ADM6824, ADM6825, ADM690, ADM690A, ADM691, ADM691A, ADM692, ADM692A, ADM693, ADM693A, ADM694, ADM695, ADM696, ADM697, ADM698, ADM699, ADM705, ADM705, ADM706, ADM706, ADM707, ADM707, ADM708, ADM708, ADM709, ADM800, ADM802, ADM803, ADM805, ADM809, ADM810, ADM811, ADM812, ADM823, ADM824, ADM825, ADM8616, ADM8617, ADM8690, ADM8691, ADM8692, ADM8693, ADM8694, ADM8695, ADM8696, ADM8697, ADM8698, ADM8699, ADM9264, ADM9690
IMPORTANT: You must enable macros when Microsoft Excel asks you as the file is being opened.
The same tools (ZIP files) are available from ADIsimPower or Supervisor Parametric Search.
Note: Microsoft Excel is dependent on the language setting Microsoft Windows for the indication of a decimal point. Issues may arise when some of these files are read/run in Excel of another language that does not use decimal point notation (such as "2.7") and uses instead decimal comma notation (such as "2,7"). The the temporary workaround is to change the language of Microsoft Windows to English. [Control Panel->Region and Language->Format]. The specific error comes from the Excel Rank command that is used by just a few tools and that does not gracefully handle decimal notation of the opposite sort suddenly in a "smart" Microsoft Excel format conversion to the regional language when opened.