Sensor-Based Intelligent Data Acquisition for STD Bus

Signal Conditioning, A/D Conversion, Pre-processing with RTI-1270 Subsystem; From Sensor Screw-Terminals to the Data Bus via Memory Mapping—at Low Cost

The STD bus is one of the most popular microcomputer buses; it is supported by more than 100 manufacturers, and the number of STD-bus applications is growing at a rate of about 35% per year. The reasons are the usual ones—low cost, compatibility with a wide range of processors and supporting hardware, flexible modular configuration, and a positive-feedback "bandwagon" effect: success breeds success. Read full article



Frank Melanson


John Mills