AN-1317: Rolling Data Buffer on the ADF7024

Introduction

When the ADF7024 receives a packet, it stores the data in a linear sequence in the packet RAM. Prior to transmission, the data to be transmitted is written to the packet RAM in a linear sequence. This functionality is described in the ADF7024 Reference Manual, UG-698. (The ADF7024 Reference Manual, UG-698, is included in the ADF7024 design resource package, which is available for download on the ADF7024 product page.) The ADF7024 packet RAM is 240 bytes long. If the packet length is greater than 240 bytes, additional measures are required. This application note describes a method for handling longer packet lengths on the ADF7024, up to a maximum length of 65,535 bytes, via a rolling buffer mechanism. This method reuses and renames several registers of the ADF7024.

Tx/Rx Rolling Data Buffer

In rolling buffer mode, packet RAM locations Address 0x020 to Address 0x0FF are available for packet data. Packet RAM memory locations Address 0x000 to Address 0x01F are allocated for use by the ADF7024 and must not be used for packet data. When rolling buffer mode is not enabled, Address 0x000 to Address 0x00F are allocated for use by the ADF7024, and Address 0x010 to Address 0x0FF are available for packet data.

Rolling Buffer Registers

The registers to enable and configure the rolling buffer mode are outlined in Table 1. When the rolling buffer is enabled via the PKT_TESTMODES register (Address 0x139), the RADIO_ PROFILE_18 register to the RADIO_PROFILE_21 register (Address 0x134 to Address 0x137) take on the rolling buffer control mechanism and no longer form part of the radio profile.

Table 1. Configuration Registers Used by the Rolling Data Buffer Mode in Tx and Rx
Address
(Hex)
Register Name with Rolling Buffer Mode
Disabled (Normal Operation)
Register Name with Rolling Buffer
Mode Enabled
Description
0x124 PKT_TX_BASE_ADR PKT_TX_BASE_ADR Start address in the packet RAM for the
transmit buffer.
0x125 PKT_RX_BASE_ADR PKT_RX_BASE_ADR Start address in the packet RAM for the
receive buffer.
0x134
RADIO_PROFILE_18 BB_RX_BUFFER_SIGNAL Location in the packet RAM for the
receive buffer nearly full signal.
0x135 RADIO_PROFILE_19 BB_RX_BUFFER_SIZE Receive buffer size in bytes.
0x136 RADIO_PROFILE_20 BB_TX_BUFFER_SIGNAL Location in the packet RAM for the
transmit buffer nearly full signal.
0x137 RADIO_PROFILE_21 BB_TX_BUFFER_SIZE Transmit buffer size in bytes.
0x139 PKT_TESTMODES PKT_TESTMODES Enable/disable the transmit and receive
rolling buffer mode. See Table 3.

Rolling Buffer Interrupts

Use the interrupts defined in Table 2 for rolling buffer operation. The normal operation of the INTERRUPT_SWM_ RSSI_DET interrupt is not available when rolling buffer mode is enabled because this interrupt is replaced with the INTERRUPT_ BUFFER_FULL interrupt. When rolling buffer mode is disabled, the INTERRUPT_SWM_RSSI_DET interrupt is again available and operates as described in the ADF7024 Reference Manual, UG-698. (The ADF7024 Reference Manual, UG-698, is included in the ADF7024 design resource package, which is available for download on the ADF7024 product page.)

Table 2. Interrupts for Rolling Buffer Operation
Address Bit Interrupt Name in Normal
Operation
Interrupt Name with Rolling Buffer
Mode Enabled
Description
INTERRUPT_MASK_0,
Address 0x100 and
INTERRUPT_SOURCE_0,
Address 0x336
6 INTERRUPT_SWM_RSSI_DET  INTERRUPT_BUFFER_FULL Asserted in the INTERRUPT_
SOURCE_0 register when the
receive or transmit buffer is full.
To enable this interrupt source
and to mirror the interrupt on
the IRQ_GP3 pin, set this bit to
Logic 1 in the INTERRUPT_
MASK_0 register.
5 Reserved INTERRUPT_BUFFER_ALMOST_FULL Asserted in the INTERRUPT_
SOURCE_0 register when the
receive or transmit buffer is
almost full. To enable this
interrupt source and to mirror
the interrupt on the IRQ_
GP3 pin, set this bit to Logic 1 in
the INTERRUPT_MASK_0 register.
 Table 3. Address 0x139: PKT_TESTMODES for Use with Rolling Buffer
Bit Bit Name in Normal
Operation
Bit Name with Rolling Buffer Mode
Enabled
Description
5 Reserved ROLLING_BUFFER_PACKET_RX 1 is enable receive rolling buffer. 0 is normal operation.
4 Reserved PAYLOAD_ONLY_PACKET_TX 1 is enable transmit payload only rolling buffer. 0 is
normal operation.
 Table 4. Maximum Packet Length Control
Address
(Hex)
Name in Normal
Operation
Name with Rolling Buffer Mode
Enabled
Description
0x014 Available for packet data TRX_BYTE_LOW Bits[7:0] of MAX_ROLLING_BUFFER_LEN[15:0], the
lower byte of the packet length control register.
0x015 Available for packet data TRX_BYTE_HIGH Bits[15:8] of MAX_ROLLING_BUFFER_LEN[15:0],
the upper byte of the packet length control
register.

Rolling Buffer: Transmit Mode

Set Bit 4 of the PKT_TESTMODES register (Address 0x139) to 1 to enable only the payload rolling buffer in transmit mode. This mode allows the user to transmit a packet of up to 65,535 bytes long using a custom packet structure. The maximum transmit length is programmable up to 0xFFFF by setting the MAX_ ROLLING_BUFFER_LEN[15:0] value as defined in Table 4, which is defined locally in the packet RAM in the rolling buffer mode.

The number and type of preamble, sync, payload, and cyclic redundancy check (CRC) are no longer bounded by the ADF7024; instead, the ADF7024 transmits what is placed in the transmit buffer. In this mode, the data in the transmit buffer is sent over the air until the MAX_ROLLING_BUFFER_LEN[15:0] number of bytes are sent, or a command is issued

In transmit mode, the start of the rolling buffer in the packet RAM is set by the PKT_TX_BASE_ADR register. The size of the buffer is set by the BB_TX_BUFFER_SIZE register. The buffer size must not exceed the available packet RAM.

Set the value in the BB_TX_BUFFER_SIGNAL register so that an INTERRUPT_BUFFER_ALMOST_FULL interrupt is generated prior to the transmission of all the data in the buffer. Typically, the BB_TX_BUFFER_SIGNAL register is set so that the interrupt is asserted when half the data in the buffer is transmitted.

When an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted, the host processor writes new data to the packet RAM, starting at the address value PKT_TX_BASE_ADR and ending at the address value, PKT_TX_BASE_ADR + BB_TX_ BUFFER_SIGNAL.

When the data in the last byte of the transmit buffer is transmitted, the ADF7024 continues transmitting, starting with the data pointed to by the PKT_TX_BASE_ADR register. If enabled, an INTERRUPT_BUFFER_FULL interrupt is asserted when the last byte in the buffer is transmitted.

When an INTERRUPT_BUFFER_FULL interrupt is asserted, the host processor must write new data to the packet RAM, starting at the address value, PKT_TX_BASE_ADR + BB_TX_ BUFFER_SIGNAL + 1, and finishing at the address value, PKT_TX_BASE_ADR + BB_TX_BUFFER_SIZE.

Transmission of data continues until the MAX_ROLLING_ BUFFER_LEN[15:0] number of bytes are sent (TX_EOF), or the user issues the CMD_PHY_ON command.

Figure

Figure 1. Rolling Buffer in Transmit Mode.

Rolling Buffer: Receive Mode

Set Bit 5 of the PKT_TESTMODES register (Address 0x139) to 1 to enable the rolling buffer in receive mode. The ADF7024 can receive packet lengths up to 216 − 1 bytes long (65,535 bytes) via the rolling buffer mechanism. The maximum packet length is programmable up to 0xFFFF by setting the MAX_ROLLING_ BUFFER_LEN[15:0] value as defined in Table 4.

When Bit 5 of the PKT_TESTMODES register (Address 0x139) is set and the sync word is received, the packet handler uses the rolling buffer to capture the remainder of the packet.

In receive mode, the PKT_RX_BASE_ADR register sets the address pointer for the start of the rolling buffer in the packet RAM. Set the size of the buffer using the BB_RX_BUFFER_ SIZE register. The buffer size must not exceed the available packet RAM size. When the value in the BB_RX_BUFFER_ SIZE register is added to the address in the PKT_RX_BASE_ ADR register, it must not exceed 0x0FF.

Set the value in the BB_RX_BUFFER_SIGNAL register so that an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted prior to the buffer being filled by the received data. Typically, the BB_RX_BUFFER_SIGNAL register is set so the interrupt is asserted when half the buffer is filled with received data.

When an INTERRUPT_BUFFER_ALMOST_FULL interrupt is asserted, the host processor reads the data from the packet RAM, starting at the address value PKT_RX_BASE_ADR and ending at the address value, PKT_RX_BASE_ADR + BB_RX_ BUFFER_SIGNAL.

When the last byte of the receive buffer is filled, the ADF7024 continues to write the received data, starting at the address value PKT_RX_BASE_ADR. If enabled, an INTERRUPT_BUFFER_ FULL interrupt is asserted when the buffer is filled.

When an INTERRUPT_BUFFER_FULL interrupt is asserted, the host processor must read the data from the packet RAM, starting at the address value, PKT_RX_BASE_ADR + BB_RX_ BUFFER_SIGNAL + 1, and ending at the address value, PKT_RX_BASE_ADR + BB_RX_BUFFER_SIZE.

Reception of data continues until the length programmed in the MAX_ROLLING_BUFFER_LEN[15:0] value is achieved (RX_EOF), or the host processor issues the CMD_PHY_ON command.

Note that it is up to the host processor to detect the end of the payload and perform an error checking operation on the data, such as CRC.

Figure

Figure 2. Rolling Buffer in Receive Mode.

Authors

Generic_Author_image

Liam O'Hora

Generic_Author_image

Conor O'Mahony

Conor O'Mahony leads the battery insights product line at Analog Devices, developing advanced battery intelligence solutions for automotive and energy storage applications. Over his career at Analog Devices, he has held a variety of engineering and leadership roles spanning wireless technology and battery management systems. Conor holds a B.E.E. from University College Cork and an M.Eng. from Dublin City University.