Press Release

Contact Linda Kincaid

Analog Devices’ 12-bit 10.25-GSPS Radio Frequency ADC Sets New Performance Benchmarks for Instrumentation and Defense

May 21 2018 - Norwood, MA
  • Analog Devices, Inc. (ADI) today introduced a radio frequency (RF) analog-to-digital converter (ADC) that delivers industry leading speed and bandwidth. The new AD9213 features higher parametric performance, greater Nyquist bandwidth, and RF sampling capabilities at higher analog input frequencies than conventional RF ADCs, allowing for the digitization of RF signals up to 7 GHz. The AD9213 enables the next generation of software defined systems in aerospace and defense, instrumentation and communications, driving greater system integration, lower costs, reduced power consumption, and decreased size, weight, and power (SWaP). Additionally, the high sample rate and integrated post processing enable further performance gains in narrow-band applications. ADI will demonstrate the AD9213 in booth #1725 at the 2018 International Microwave Symposium (IMS) taking place June 10-15 in Philadelphia, Pennsylvania.



    The AD9213 provides aerospace and defense customers with greater flexibility and the ability to process larger sections of spectrum in electronic surveillance and countermeasures applications, as well as increased resolution and longer range in RADAR designs. The device helps electronic test and measurement manufacturers (ETM) create greater product differentiation and new levels of performance in time-domain applications, such as digital oscilloscopes and spectroscopy/chemical analysis. The wider Nyquist bandwidth allows satellite communications customers to deliver products with increased bandwidth. In addition, wide input bandwidths combined with high sample rates enable new wideband digital pre-distortion architectures in wireless communications applications.


    AD9213 Product Highlights:


    • 2.5 times sampling compared to other similar devices
    • Greater system dynamic range for better discrimination between signals
    • Superior noise performance over a wide signal bandwidth
    • Enhanced multi-chip synchronization for phased array applications
    • Increased temporal resolution (higher sample rate)

    Pricing and Availability
    Product Sample Availability Full Production Price Each Per 1,000 Packaging
    AD9213 Now February 2019 $3,652.49 192-lead BGA
  • About Analog Devices
  • Analog Devices (Nasdaq: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/

  • Editor's Contact Information
Stay Informed