Press Release

Contact Linda Kincaid

Analog Devices’ Integrated, Isolated Power Controller Series Reduces Design Complexity and Improves System Reliability

Mar 23 2017 - Norwood, MA
  • ADP107x-RGB-300x300-Title-WebAnalog Devices, Inc. (ADI), today announced a series of three isolated pulse width modulation (PWM) controllers with integrated 5 kV isolation enabled by ADI’s award-winning iCoupler® technology. The ADP1071-1 and ADP1071-2 are isolated synchronous flyback controllers and the ADP1074 is an isolated synchronous active clamp forward controller. By integrating multiple functions such as overvoltage protection (OVP), output tracking, and light load mode for greater energy efficiency and SR Drivers, which ordinarily need several discrete components, board space is reduced by as much as 35% and system reliability greatly improved when compared to traditional approaches using optocouplers. The new PWM controllers are designed for isolated DC/DC power supplies for use in universal input off-line, industrial, or telecom power supplies. Another important feature includes secondary side communication using PGOOD to eliminate the typical isolation barrier constraints while reducing external component count.


    The new devices offer a unique combination of a primary and secondary side controller with iCoupler isolation technology in a single easy-to-use package with true secondary side sensing providing all the benefits of primary and secondary side controllers in one combination. The iCoupler technology also provides high bandwidth for excellent transient response with over five times improvement and over 20% reduced output capacitance.


    About the ADP1071-1 and ADP1071-2 PWM Controllers
    The ADP1071-1 and ADP1071-2 are PWM current mode fixed frequency synchronous flyback controllers designed for isolated DC/DC power supplies. ADI’s proprietary iCoupler technology is integrated in the PWM controllers, replacing the bulky signal transformers and optocouplers while reducing system design complexity, cost component count, and improving overall system reliability. With the integrated isolation and drivers on both the primary and secondary side, the PWM controllers offer a compact system level design that yields higher efficiency than a diode rectified flyback converter at heavy loads. The ADP1071-1 accommodates high voltage applications (≥60V) and the ADP1071-2 accommodates low voltage applications (≤60V). The ADP1071-1 and ADP1071-2 are ideally suited for isolated DC/DC or AC/DC power conversion, small cell, PoE powered devices, and enterprise switches/routers used in telecom and industrial applications.


    About the ADP1074 PWM Controller
    The ADP1074 is a current mode fixed frequency active-clamp synchronous forward controller also designed for isolated DC/DC power supplies. ADI’s iCoupler technology is integrated in the ADP1074 to replace the bulky signal transformers and optocouplers that transmit signals over the isolation boundary. With the integrated isolators and MOSFET drivers on both the primary and secondary side, the ADP1074 offers a compact system-level design and yields a higher efficiency than a non-synchronous forward converter at heavy loads. This device reduces system design complexity, cost, and component count while improving overall system reliability. The ADP1074 is ideally suited for isolated DC/DC power conversion in many applications including intermediate bus voltage generation, base station and antenna RF power, small cell, PoE powered devices, enterprise switches/routers, core/edge/metro/optical routing, and power modules used in telecom and industrial equipment.


    Availability and Packaging

    Part Number Availability Package Description
    ADP1071-1 October 2017 16-Lead SOIC wide body package Flyback controller with integrated isolation and SR drive with light load mode
    ADP1071-2 October 2017 16-Lead SOIC wide body package Flyback controller with integrated isolation and SR drive
    ADP1074 July 2017 24-Lead SOIC wide body package Forward controller with integrated isolation and SR drive
  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • iCoupler and EngineerZone are registered trademarks of Analog Devices, Inc.


    Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/analog-dialogue

  • Editor's Contact Information
Stay Informed