Press Release

Contact Linda Kincaid

Analog Devices’ Industrial Inertial Measurement Units Improve Navigation and Reliability in Autonomous Machines

Nov 8 2017 - Norwood, MA
  • ADIS16470Analog Devices, Inc. (ADI) today announced a series of five high-performance inertial measurement units (IMUs) that address the navigation- and safety-related needs of industrial applications in several emerging markets, while also reducing their system complexity and cost. The ADIS16470, ADIS16475 and ADIS16477 IMUs deliver exceptional performance improvements in smallest size with standard surface mount assembly. The three different models are optimized to provide a range of performance, cost, and application-suitability needs. The ADIS16465 and ADIS16467 IMUs offer similar performance advantages in a more ruggedized enclosure option. Together, these product advancements bring a previously unavailable performance-for-cost ratio to unmanned aerial vehicle (UAV) applications where designers have previously struggled with costly, risky, and sub-par performance solutions from integrating consumer grade sensors, which also fell short of reliability goals. These new IMUs bring the same benefits to Autonomous Machine applications in fields such as Smart Agriculture where the demands of such rugged equipment previously forced a choice between cost-challenged, highest-grade sensors or performance-limited commercial sensors.



    All of the IMUs provide six degree-of-freedom (DoF) sensing via triple-axis MEMS-based accelerometers and gyroscopes, and are focused on the demands of the Industrial "Internet of Moving Things" and its need for precise geolocation. Their performance allows systems to characterize motion accurately despite turbulence, vibration, wind, temperature, and other environmental disturbances, resulting in more-accurate navigation and guidance, and/or instrument stabilization.

    Leveraging three decades of experience in inertial sensor design, Analog Devices has engineered an unparalleled combination of reliable high performance, and size/cost effectiveness. With industry leading performance, system designers are now able to rely more heavily on these high-grade sensors versus a previous need to attempt performance boosting via added test, components, calibration, or software aids. The ADIS1646x and ADIS1647x IMUs are specifically designed to reject what are otherwise significant error sources, such as ‘g’-influence, cross-axis sensitivity, and temperature and mechanical stress related drifts.


    Key Product Specifications
    Product DoF Gyro Range °/sec Gyro Noise °/sec/√Hz rms Gyro in-run Stability o/hr Accel Range g Accel Noise μg/√Hz rms Accel in-run Stability μg Oper Temp Range °C
    ADIS16470 6 2000 0.008 8 40 100 13 -25 to 85
    ADIS16475/65 6 125/500/2000 0.003 2 8 23 3.6 -40 to 105
    ADIS16477/67 6 125/500/2000 0.003 2 40 100 13 -40 to 105

    Pricing and Availability
    Product Production Availability Price Each per 1,000 Packaging
    ADIS16470 Now $149 11x15x11 BGA
    ADIS16475/7 Now $365 11x15x11 BGA
    ADIS16465/7 End Nov 2017 $385 22x22x9 Module

    The new IMUs are supported by the EVAL-ADIS2Z, a PC-based tool for evaluation which enables basic demonstration, individual register access, and high-speed data capture, as well as the breakout boards that simplify connecting ADIS16xxx IMU products to development platforms.



  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • EngineerZone is a registered trademark of Analog Devices, Inc.

    Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/analog-dialogue/

  • Editor's Contact Information
Stay Informed