Press Release

Contact Joe Dussi

Robust iCoupler® Digital Isolators Improve Signal Reliability to Guarantee Safe System Functionality in Noisy Environments

Analog Devices, Inc. today introduced the industry’s most robust digital isolator series with the best combination of signal reliability, safety and performance.

Oct 29 2015 - Norwood, MA
  • ADUM140Analog Devices, Inc. today introduced the industry’s most robust digital isolator series with the best combination of signal reliability, safety and performance. Based on ADI’s patented iCoupler® digital isolation technology, the new isolator devices ensure safe system performance for applications operating in noisy, harsh and unpredictable healthcare and industrial environments.



    Advances in healthcare technology are pushing design boundaries by requiring wired patient monitors to function continuously during defibrillation. These high-voltage transients put a great burden on designing a dependable, connected medical system. To protect data signals in this unpredictable environment, the new iCoupler digital isolators feature the highest in industry surge protection tested at 16 kVpk and withstand voltage ratings up to 5 kVrms. And unlike other digital isolators, ADI’s new, robust iCoupler digital isolators can replace bulky optocouplers in harsh medical environments with a more compact solution.


    Precision robotic arms operate in unforgiving industrial factory floor environments. Modern high-speed communications used in factory automation must be isolated from electrical noise caused by arc welding and other equipment in order to avoid signal interference. ADI’s iCoupler digital isolators provide high noise immunity and surpass previous digital isolator options to ensure signal integrity. ADI’s isolation components provide outstanding performance and proven galvanic isolation with more than 1.4 billion channels shipped and growing. By combining high-speed CMOS and monolithic air core transformer technology and an on-off-keying (OOK) architecture, the new digital isolators offer the highest available noise immunity, lowest EMI and highest surge capability for broad market appeal. Multiple products are in production today with versions in different packages and channel counts forthcoming.


    Robust iCoupler Digital Isolator Key Features:

    • Safest: 16 kVpk basic and 10-kV reinforced surge protection ratings,
      5 KVrms withstand, 600 Vrms working voltage
    • Fastest: 150 Mbps throughput, 13 ns max propagation delay, 100 kV/µs CMTI
    • Widest supply range: 1.7 V to 5.5 V
    • Versatile: 1 to 4 input channels, choice of default state, and input/output disable, pin compatible to prior generations

    Pricing and Availability
    Product Availability Withstand Voltage (KV) Total Channels Price Each per 1,000 Packaging
    ADuM110 Now 3.0 1 $1.29 8ld SOIC_N
    ADuM13x Now 3.75 3 $1.72 16ld SOIC_W
    ADuM13x Nov 2015 3.0 3 $1.72 16ld SOIC_N
    ADuM14x Now 3.75 4 $2.18 16ld SOIC_W
    ADuM14x Nov 2015 3.0 4 $2.18 16ld SOIC_N
    ADuM23x Now 5.0 3 $2.47 16ld SOIC_W
    ADuM24x Now 5.0 4 $3.15 16ld SOIC_W

  • About Analog Devices
  • Analog Devices designs and manufactures semiconductor products and solutions. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure and connect. Visit http://www.analog.com
  • iCoupler® is a registered trademark of Analog Devices, Inc.


    EngineerZone is a registered trademark of Analog Devices, Inc.


    Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/

  • Editor's Contact Information
Stay Informed