Reduce the Chances of Human Error: Part 2, Super Amps and Filters for Analog Interface

Mar 8 2011

Read other articles in this series.

Abstract

A common view holds that digital circuits just work naturally, but analog circuits are hard to implement. There is truth to that old belief—analog interface is an expert subject that requires training. It is, moreover, always better to avoid an issue than to try to solve it later. This is precisely why we should take advantage of some basic concepts that experienced analog engineers perform as a reflex. This application note provides some basic reminders and concepts about amplifiers and filters for you to consider during a design.

Introduction

As children we learned to share and in that process we learned about portions. Many parents taught this to children by having one child cut the pie or cake and then letting another child pick the piece first. We can be sure that great care was used to make the pieces all the same size.

We are reminded of a good lesson in life, "It's the ratio that counts." We use ratios in everyday life when we compare distances between different routes or the taste of two foods. (Yes, mom's cooking was better, or maybe we were too young to know any difference?).

Moving from children, pies, and cakes to analog engineering design, we realize that ratios—the relative amount, proportion, percentage, share, part, and fraction—are all important measurements in analog design. When we ignore these ratios and relationships, we introduce human error into what must be a precise process. This application note shares some analog concepts about amplifiers and filters that will help reduce the chances of "human" error and improve the analog design.

Considerations for Signal to Noise (SNR)

Crosstalk and signal to noise (SNR) are expressed as ratios, a proportion of good to bad. How does one improve the SNR of a signal? If a particular circuit contributes considerable noise, we have two basic options: first, reduce the noise somehow, or second, increase the amplitude of the good signal before it goes through the stage. Figure 1 illustrates the concept.

Figure 1. Power-supply noise is added to the signal.

Figure 1. Power-supply noise is added to the signal.

In application note 4992, "Reduce the Chances of Human Error: Part 1, Power and Ground," we concentrated on power noise, ground, and layout. In this companion article we examine how to control noise in the signal path. We discuss the characteristics of the signal and noise as we proceed through the various circuit stages.

Is the major noise source harmonics of a switching power supply? If the power-supply noise is 50kHz and higher and if our wanted signal is 1kHz, then filtering may be feasible. If we will be going into an ADC next, the anti-aliasing filter may help.

Reducing Noise

What possibilities does an experienced circuit designer evaluate? The simplest fix is to amplify the signal before the noise is added. Yes, straightforward enough, but unfortunately this solution most often cannot be used because the incoming signal already has noise present. So now we get creative and consider how to separate the signal from noise? Can we use highpass, lowpass, or bandpass filters? Can we discriminate on the basis of amplitude, limiting, noise blanking, or coring? Can we use preemphasis before the noise is introduced and deemphasis after to increase SNR? Can we discriminate on the basis of time, i.e., sample at a minimum noise level or interference time? Can we time average, or if the signal is repetitive, can we sum cycles or average in two, three, or more dimensions?

Turning from component functions, think about the system as a whole. What are the system goals? How will the system be used? How will the human senses interact with the information provided by the system? In short, consider all the information that we can muster.

The above set of questions reflects considerable design experience and knowledge. This is precisely why smart companies hire experienced engineers and mentor the new engineers to build a solid design team.

We can use an example to illustrate the thinking and development process. The first observation finds that the system has a high-gain operational amplifier at its input. The op amp feeds an analog-to-digital converter (ADC). Occasionally a large noise pulse appears on the signal and this causes the op amp to saturate. The op amp recovery time might be as long as milliseconds or seconds. How will we approach the issue? Since every case will be different, we will just ask questions and point out possible solutions.

First, gather data to try to understand what is happening. Can we fix the source? No. So we decide that the noise spike is unavoidable. What do we know about its risetime amplitude and duration? If the spike is very fast and narrow and our wanted signal is relatively slow, can we separate them by filtering? Can we detect the spike and open a series switch to blank out the spike from the main path? Could we add a pair of diodes like an electrostatic discharge (ESD) structure to clip any signal that goes above VCC or below ground? Can we learn from application note 4344, "Rail Splitter, from Abraham Lincoln to Virtual Ground?" In Figure 2 of that application note we create a voltage between VCC and ground at the average signal level of the wanted signal. If the series resistor was replaced with a pair of back-to-back diodes (Figure 2), the signal spike would be limited to the voltage ±0.6V for silicon diodes (red dashed lines) and ~±0.3V for Schottky diodes (green dashed lines). The reverse recovery time for silicon diodes can be between one hundreds and several hundreds of nanoseconds. Schottky diodes have a switching time of ~100ps for the small signal diodes but, because of their operating physics, do not have a reverse recovery time. The diodes can also be placed in the op amp feedback loop to reduce gain during the spike. Figure 3 shows the effect of limiting.

Figure 2. Replacing a series resistor with a pair of back-to-back diodes.

Figure 2. Replacing a series resistor with a pair of back-to-back diodes.

Figure 3. Diode limiter effect, ±0.3V Schottky, ±0.6V silicon.

Figure 3. Diode limiter effect, ±0.3V Schottky, ±0.6V silicon.

Figure 3 may help relieve op amp saturation and recovery time, but is it enough? We could add circuits to blank out the noise pulse as in Figure 4.

Figure 4. Noise pulse blanking.

Figure 4. Noise pulse blanking.

The block diagram of the blanking circuit is Figure 5.

Figure 5. Noise-blanking block diagram.

Figure 5. Noise-blanking block diagram.

From the basic concept of blanking in Figure 5, more elegance can be added. The input buffer may not be needed if the source is low impedance. R1 and R2 set a DC value as shown in application note 4344, "Rail Splitter, from Abraham Lincoln to Virtual Ground," mentioned above. Alternatively, the input signal could be AC coupled to this same voltage or the input signal could be averaged over the long term to produce this voltage. The main signal path is from the input buffer through a RC delay, the mux, buffer, and lowpass filter to the ADC. The MAX11203 ADC has four general-purpose input or output (GPIO) ports controlled by the SPI interface. The GPIO is set so that the AIN1of the MAX313 multiplexor is on and AIN2 is off. We highpass or differentiate the noise pulse. The dual or window comparator output will be active while the noise pulse exceeds 0.3V in either the positive or negative direction. The XOR gated inverts the logic to the mux, thereby turning off the main path and switching on the DC voltage. The RC delay also delays the main path long enough for the comparator path to change state. If the RC delay degrades the signal bandwidth too much, an LC delay line can be substituted.

The input buffer of Figure 5 could use a MAX4209 instrument amplifier which has incredibly low offset drift despite its high gain. Application note 4179, "Autozero Noise Filtering Improves Instrumentation Amplifier Output," explains why.

The filter just before the ADC in Figure 5 can control signal bandwidth to meet Nyquist anti-aliasing, reduce noise, or soften the residual blanking glitch. The following application notes will provide advice and ideas:

Application note 4617, "ADC Input Translator," uses resistor-dividers to scale the differential inputs and a stable voltage reference to offset the inputs. This circuit design enables an ADC with a 0V to 5V input range (e.g., the MAX1402) to accept inputs in the range +10.5V to -10.5V.

Calibration ideas using digital-to-analog converters (DACs) and potentiometers are covered in application notes 4494, "Methods for Calibrating Gain Error in Data-Converter Systems," and 818, "Digital Adjustment of DC-DC Converter Output Voltage in Portable Applications." The digital-output voltage-adjustment methods are performed with DAC, a trim pot (digital potentiometer), and PWM output of a microprocessor. Application note 4704, "Introduction to Electronic Calibration and Methods for Correcting Manufacturing Tolerances in Industrial Equipment Designs," includes a discussion of the DS4303 infinite sample-and-hold to capture a DC Voltage. Other application notes about digital pots include:

Analog I/O, interface circuits and digital-port signal protection ideas are discussed in the following application notes:

Maxim has watchdog circuits which ensure that microprocessor-controlled devices react in a known manner if the processor loses control. The following application notes offer ideas for using watchdogs: 4558, "Simple Latching Watchdog Timer," and 4229, "Comparison of Internal and External Watchdog Timers."

Microprocessor-controlled system clocks typically are of two types: system clocks controlling computing functions in orderly ways, and real time clocks (RTCs) or clocks that relate to human time concepts. Computer clocks operate like soldiers marching in cadence. This can result in interference products that may not meet regulatory requirements. Clock-generator spread-spectrum techniques to reduce this interference are discussed in these notes: 2863, "The Effects of Adjusting the DS1086L's Dither Span and Dither Frequency on EMC Measurements," and 3512, "Automotive Applications for Silicon Spread-Spectrum Oscillators." RTC ideas are found at "Reduce the Chances of Human Error: Part 1, Power and Ground".

Conclusion

Noise and interference control is different in every circuit and system. Thankfully, the laws of physics prevail and engineers must work hard to silence noise. This discussion has tried to help designers anticipate noise and interference issues before the design starts and during the design. After the product is in production, the options for correction are severely limited.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

MAX4506
PRODUCTION

Fault-Protected, High-Voltage Signal-Line Protectors

MAX3226
PRODUCTION

1µA Supply Current, 1Mbps, 3.0V to 5.5V, RS-232 Transceivers with AutoShutdown Plus

MAX1490E
RECOMMENDED FOR NEW DESIGNS

±15kV ESD-Protected, Isolated RS-485/RS-422 Data Interfaces

MAX274

4th- and 8th-Order, Continuous-Time Active Filters

MAX275

4th- and 8th-Order, Continuous-Time Active Filters

MAX4568 PRODUCTION

±15kV ESD-Protected, Low-Voltage, SPDT/SPST, CMOS Analog Switches

MAX4640 Obsolete

±15kV ESD-Protected, Low-Voltage, Quad, SPST, CMOS Analog Switches

MAX4630 PRODUCTION

±15kV ESD-Protected, Low-Voltage, Quad, SPST, CMOS Analog Switches

MAX321 PRODUCTION

Precision, Dual Supply, SPST, Analog CMOS Switches

MAX4575 PRODUCTION

±15kV ESD-Protected, Low-Voltage, Dual, SPST, CMOS Analog Switches

MAX4551 PRODUCTION

±15kV ESD-Protected, Quad, Low-Voltage, SPST Analog Switches

MAX4558 PRODUCTION

±15kV ESD-Protected, Low-Voltage, CMOS Analog Multiplexers Switches

DS1086 PRODUCTION

Spread-Spectrum EconOscillator

DS1087L PRODUCTION

3.3V Spread-Spectrum EconOscillator

DS1086L PRODUCTION

3.3V Spread-Spectrum EconOscillator

DS1085 PRODUCTION

EconOscillator Frequency Synthesizer

DS1089L PRODUCTION

3.3V Center Spread-Spectrum EconOscillator™

MAX7375 PRODUCTION

3-Pin Silicon Oscillator

DS1094L PRODUCTION

Multiphase Spread-Spectrum EconOscillator

DS1090 PRODUCTION

Low-Frequency, Spread-Spectrum EconOscillator

MAX4167 PRODUCTION

High-Output-Drive, Precision, Low-Power, Single-Supply, Rail-to-Rail I/O Op Amps with Shutdown

MAX516 PRODUCTION

Quad Comparator with Programmable Threshold

MAX4209 PRODUCTION

Ultra-Low Offset/Drift, Precision Instrumentation Amplifiers with REF Buffer

MAX4238 PRODUCTION

Ultra-Low Offset/Drift, Low-Noise, Precision SOT23 Amplifiers

MAX4232 PRODUCTION

High-Output-Drive, 10MHz, 10V/µs, Rail-to-Rail I/O Op Amps with Shutdown in SC70

MAX5898 NOT RECOMMENDED FOR NEW DESIGNS

16-Bit, 500Msps, Interpolating and Modulating Dual DAC with Interleaved LVDS Inputs

MAX5874 PRODUCTION

14-Bit, 200Msps, High-Dynamic-Performance, Dual DAC with CMOS Inputs

MAX5384 PRODUCTION

Low-Cost, Low-Power, 8-Bit DACs with 3-Wire Serial Interface in SOT23

DS1851 NOT RECOMMENDED FOR NEW DESIGNS

Dual Temperature-Controlled NV Digital-to-Analog Converters

MAX5116 PRODUCTION

Nonvolatile, Quad, 8-Bit DACs with 2-Wire Serial Interface

MAX5105 PRODUCTION

Nonvolatile, Quad, 8-Bit DACs

MAX5893 LAST TIME BUY

12-Bit, 500Msps Interpolating and Modulating Dual DAC with CMOS Inputs

MAX5877 PRODUCTION

14-Bit, 250Msps, High-Dynamic-Performance, Dual DAC with LVDS Inputs

MAX5363 PRODUCTION

Low-Cost, Low-Power, 6-Bit DACs with 3-Wire Serial Interface in SOT23

MAX5115

Nonvolatile, Quad, 8-Bit DACs with 2-Wire Serial Interface

MAX5547

Dual, 10-Bit, Current-Sink Output DAC

MAX5876 RECOMMENDED FOR NEW DESIGNS

12-Bit, 250Msps, High-Dynamic-Performance, Dual DAC with LVDS Inputs

MAX5550 PRODUCTION

Dual, 10-Bit, Programmable, 30mA High-Output-Current DAC

MAX5364

Low-Cost, Low-Power, 6-Bit DACs with 3-Wire Serial Interface in SOT23

MAX5895 LAST TIME BUY

16-Bit, 500Msps Interpolating and Modulating Dual DAC with CMOS Inputs

MAX5381 PRODUCTION

Low-Cost, Low-Power, 8-Bit DACs with 2-Wire Serial Interface in SOT23

MAX5106 PRODUCTION

Nonvolatile, Quad, 8-Bit DACs

MAX5774 PRODUCTION

32-Channel, 14-Bit, Voltage-Output DACs with Serial Interface

MAX5878 PRODUCTION

16-Bit, 250Msps, High-Dynamic-Performance, Dual DAC with LVDS Inputs

MAX5894 Obsolete

14-Bit, 500Msps, Interpolating and Modulating Dual DAC with CMOS Inputs

MAX5380 PRODUCTION

Low-Cost, Low-Power, 8-Bit DACs with 2-Wire Serial Interface in SOT23

MAX5109

Nonvolatile, Dual, 8-Bit DACs with 2-Wire Serial Interface

MAX5383 PRODUCTION

Low-Cost, Low-Power, 8-Bit DACs with 3-Wire Serial Interface in SOT23

MAX5873 PRODUCTION

12-Bit, 200Msps, High-Dynamic-Performance, Dual DAC with CMOS Inputs

MAX5355 PRODUCTION

10-Bit Voltage-Output DACs in 8-Pin µMAX

MAX5875 PRODUCTION

16-Bit, 200Msps, High-Dynamic-Performance, Dual DAC with CMOS Inputs

MAX5361 PRODUCTION

Low-Cost, Low-Power 6-Bit DACs with 2-Wire Serial Interface in SOT23 Package

MAX1215

1.8V, 12-Bit, 250Msps ADC for Broadband Applications

MAX1214

1.8V, 12-Bit, 210Msps ADC for Broadband Applications

MAX1402 PRODUCTION

+5V, 18-Bit, Low-Power, Multichannel, Oversampling (Sigma-Delta) ADC

MAX12555 PRODUCTION

14-Bit, 95Msps, 3.3V ADC

MAX12528

Dual, 80Msps, 12-Bit, IF/Baseband ADC

MAX12558

Dual, 80Msps, 14-Bit, IF/Baseband ADC

MAX12557 PRODUCTION

Dual, 65Msps, 14-Bit, IF/Baseband ADC

MAX1213

1.8V, 12-Bit, 170Msps ADC for Broadband Applications

MAX19586 Obsolete

High-Dynamic-Range, 16-Bit, 80Msps ADC with -82dBFS Noise Floor

MAX12553 Obsolete

14-Bit, 65Msps, 3.3V ADC

MAX1067 PRODUCTION

Multichannel, 14-Bit, 200ksps Analog-to-Digital Converters

MAX12527 PRODUCTION

Dual, 65Msps, 12-Bit, IF/Baseband ADC

MAX5481 PRODUCTION

10-Bit, Nonvolatile, Linear-Taper Digital Potentiometers

MAX5457 PRODUCTION

Stereo Audio Taper Potentiometers with Pushbutton Interface

MAX5460 PRODUCTION

32-Tap FleaPoT™, 2-Wire Digital Potentiometers

DS3906 PRODUCTION

Triple NV Low Step Size Variable Resistor Plus Memory

MAX5422 PRODUCTION

256-Tap, Nonvolatile, SPI-Interface, Digital Potentiometers

MAX5456 PRODUCTION

Stereo Audio Taper Potentiometers with Pushbutton Interface

DS1848 NOT RECOMMENDED FOR NEW DESIGNS

Dual Temperature-Controlled NV Variable Resistor & Memory

MAX5429 PRODUCTION

32-Tap, One-Time Programmable, Linear-Taper Digital Potentiometers

MAX5400 PRODUCTION

256-Tap SOT-PoT, Low-Drift Digital Potentiometers in SOT23

MAX5491 PRODUCTION

Precision-Matched Resistor-Divider in SOT23

MAX5463 PRODUCTION

32-Tap FleaPoT™, 2-Wire Digital Potentiometers

MAX5437 PRODUCTION

±15V, 128-Tap, Low-Drift Digital Potentiometers

MAX5160 PRODUCTION

Low-Power Digital Potentiometers

MAX5477 PRODUCTION

Dual, 256-Tap, Nonvolatile, I²C-Interface, Digital Potentiometers

DS3930 PRODUCTION

Hex Nonvolatile Potentiometer with I/O and Memory

MAX5402 PRODUCTION

256-Tap, µPoT Low-Drift, Digital Potentiometer

MAX5490 PRODUCTION

100kΩ Precision-Matched Resistor-Divider in SOT23

MAX5466 PRODUCTION

32-Tap FleaPoT™, 2-Wire Digital Potentiometers

DS1804 PRODUCTION

Nonvolatile Trimmer Potentiometer

DS3502 PRODUCTION

High-Voltage NV I²C Potentiometer

MAX5401 PRODUCTION

256-Tap SOT-PoT, Low-Drift Digital Potentiometers in SOT23

MAX5439 PRODUCTION

±15V, 128-Tap, Low-Drift Digital Potentiometers

DS3904 PRODUCTION

Triple, 128-Position, Nonvolatile, Variable, Digital Resistor/Switch

DS1847 NOT RECOMMENDED FOR NEW DESIGNS

Dual Temperature-Controlled NV Variable Resistor

MAX5428 PRODUCTION

32-Tap, One-Time Programmable, Linear-Taper Digital Potentiometers

MAX5492 PRODUCTION

10kΩ Precision-Matched Resistor-Divider in SOT23

DS3903 PRODUCTION

Triple 128-Position Nonvolatile Digital Potentiometer

MAX5427 PRODUCTION

32-Tap, One-Time Programmable, Linear-Taper Digital Potentiometers

MAX7412 PRODUCTION

5th Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7401 PRODUCTION

8th-Order, Lowpass, Bessel, Switched-Capacitor Filters

MAX7415 PRODUCTION

5th Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7404 PRODUCTION

8th-Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7414 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7403 PRODUCTION

8th-Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7420 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7405 PRODUCTION

8th-Order, Lowpass, Bessel, Switched-Capacitor Filters

MAX7419 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7421 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7411 PRODUCTION

5th Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7408 PRODUCTION

5th Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7400 PRODUCTION

8th-Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7418 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7410 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7407 PRODUCTION

8th-Order, Lowpass, Elliptic, Switched-Capacitor Filters

MAX7491 PRODUCTION

Dual Universal Switched-Capacitor Filters

MAX7413 PRODUCTION

5th-Order, Lowpass, Switched-Capacitor Filters

MAX7490 PRODUCTION

Dual Universal Switched-Capacitor Filters

MAX6241 PRODUCTION

Low-Noise, Precision, +2.5V/+4.096V/+5V Voltage References

MAX6350 PRODUCTION

1ppm/°C, Low-Noise, +2.5V/+4.096V/+5V Voltage References

MAX674 PRODUCTION

+10V Precision Voltage Reference

MAX6173 PRODUCTION

High-Precision Voltage References with Temperature Sensor

MAX6160 PRODUCTION

SOT23, Low-Cost, Low-Dropout, 3-Terminal Voltage References

MAX6325 PRODUCTION

1ppm/°C, Low-Noise, +2.5V/+4.096V/+5V Voltage References

MAX6175 PRODUCTION

High-Precision Voltage References with Temperature Sensor

MAX6143 PRODUCTION

High-Precision Voltage Reference with Temperature Sensor

MAX6341 PRODUCTION

1ppm/°C, Low-Noise, +2.5V/+4.096V/+5V Voltage References

MAX6174 PRODUCTION

High-Precision Voltage References with Temperature Sensor

MAX6220 PRODUCTION

Low-Noise, Precision, +2.5V/+4.096V/+5V Voltage Reference

REF02 NOT RECOMMENDED FOR NEW DESIGNS

+5V, +10V Precision Voltage References

MAX675 PRODUCTION

Precision, +5V Voltage Reference, Replaced MAX673

MAX6250 PRODUCTION

Low-Noise, Precision, +2.5V/+4.096V/+5V Voltage References

MAX6177 PRODUCTION

High-Precision Voltage References with Temperature Sensor

REF01 NOT RECOMMENDED FOR NEW DESIGNS

+5V, +10V Precision Voltage References

MAX6176 PRODUCTION

High-Precision Voltage References with Temperature Sensor

MAX6225 PRODUCTION

Low-Noise, Precision, +2.5V/+4.096V/+5V Voltage References

DS4303 PRODUCTION

Electronically Programmable Voltage Reference

MAX1553 PRODUCTION

High-Efficiency, 40V Step-Up Converters for 2 to 10 White LEDs

MAX6752 PRODUCTION

µP Reset Circuits with Capacitor-Adjustable Reset/Watchdog Timeout Delay

MAX6749 PRODUCTION

µP Reset Circuits with Capacitor-Adjustable Reset/Watchdog Timeout Delay

MAX253 PRODUCTION

1W Primary-Side Transformer H-Bridge Driver for Isolated Supplies

DS1267

±5V Dual Digital Potentiometer Chip

MAX9206 PRODUCTION

10-Bit Bus LVDS Deserializers

MAX9205 PRODUCTION

10-Bit Bus LVDS Serializers

MAX9208 PRODUCTION

10-Bit Bus LVDS Deserializers

MAX9207

10-Bit Bus LVDS Serializers

MAX483E PRODUCTION

±15kV ESD-Protected, Slew-Rate-Limited, Low-Power, RS-485/RS-422 Transceivers

MAX487E PRODUCTION

±15kV ESD-Protected, Slew-Rate-Limited, Low-Power, RS-485/RS-422 Transceivers

MAX3485 PRODUCTION

3.3V Powered, 10Mbps and Slew-Rate Limited, True RS-485/RS-422 Transceivers

MAX3244E PRODUCTION

±15kV ESD-Protected, 1µA, 1Mbps, 3.0V to 5.5V, RS-232 Transceivers with AutoShutdown Plus

MAX3228

+2.5V to +5.5V RS-232 Tranceivers in UCSP

MAX488 PRODUCTION

Low-Power, Slew-Rate-Limited RS-485/RS-422 Transceivers

MAX3083 PRODUCTION

Fail-Safe, High-Speed (10Mbps), Slew-Rate-Limited RS-485/RS-422 Transceivers

MAX3313E PRODUCTION

±15kV ESD-Protected, 460kbps, 1µA, RS-232-Compatible Transceivers in µMAX

MAX3388E PRODUCTION

2.5V, ±15kV ESD-Protected RS-232 Transceivers for PDAs and Cell Phones

MAX3443E PRODUCTION

±15kV ESD-Protected, ±60V Fault-Protected, 10Mbps, Fail-Safe RS-485/J1708 Transceivers

MAX491E PRODUCTION

±15kV ESD-Protected, Slew-Rate-Limited, Low-Power, RS-485/RS-422 Transceivers

MAX3483E PRODUCTION

3.3V Powered, ±15kV ESD-Protected, 12Mbps, Slew-Rate-Limited True RS-485/RS-422 Transceivers

MAX3490 PRODUCTION

3.3V Powered, 10Mbps and Slew-Rate Limited, True RS-485/RS-422 Transceivers

MAX3088 PRODUCTION

Fail-Safe, High-Speed (10Mbps), Slew-Rate-Limited RS-485/RS-422 Transceivers

MAX3225E RECOMMENDED FOR NEW DESIGNS

±15kV ESD-Protected, 1µA, 1Mbps, 3.0V to 5.5V, RS-232 Transceivers with AutoShutdown Plus

MAX485E PRODUCTION

±15kV ESD-Protected, Slew-Rate-Limited, Low-Power, RS-485/RS-422 Transceivers

MAX1480E RECOMMENDED FOR NEW DESIGNS

±15kV ESD-Protected, Isolated RS-485/RS-422 Data Interfaces

MAX3311E PRODUCTION

±15kV ESD-Protected, 460kbps, 1µA, RS-232-Compatible Transceivers in µMAX

MAX3080 PRODUCTION

Fail-Safe, High-Speed (10Mbps), Slew-Rate-Limited RS-485/RS-422 Transceivers

MAX3190E

±15kV ESD-Protected, 460kbps, RS-232 Transmitters in SOT23-6

MAX3245E PRODUCTION

±15kV ESD-Protected, 1µA, 1Mbps, 3.0V to 5.5V, RS-232 Transceivers with AutoShutdown Plus

MAX1488E PRODUCTION

±15kV ESD-Protected, Quad, Low-Power RS-232 Line Driver

MAX3188

1Mbps, 1µA RS-232 Transmitters in SOT23-6

MAX3387E PRODUCTION

3V, ±15kV ESD-Protected, AutoShutdown Plus RS-232 Transceiver for PDAs and Cell Phones

MAX3223E PRODUCTION

±15kV ESD-Protected, 1µA, 3.0V to 5.5V, 250kbps, RS-232 Transceivers with AutoShutdown

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project