Обзор

Ресурсы проектирования

Design & Integration Files

  • Schematic
  • Bill of Materials
  • Gerber Files
  • PADS Layout Files
  • Assembly Drawing
Загрузить файлы проектов 1253 kB

Оценочные платы

Буква "Z" в наименовании компонента указывает на соответствие требованиям RoHS. Отмеченные платы нужны для оценки данной схемы

  • EVAL-CN0357-PMDZ ($95.00) Single-Supply, Toxic Gas Detector, Using an Electrochemical Sensor with Programmable Gain TIA
  • EVAL-SDP-CB1Z ($99.00) Eval Control Board
  • SDP-PMD-IB1Z ($55.00) PMOD to SDP Interposer Board
Проверка наличия и приобретение

Особенности и преимущества

  • Complete electrochemical sensor 
  • Low power 
  • Single Supply

Circuit Function & Benefits

The circuit shown in Figure 1 is a single-supply, low noise, portable gas detector, using an electrochemical sensor. The Alphasense CO-AX carbon monoxide sensor is used in this example.

Electrochemical sensors offer several advantages for instruments that detect or measure the concentration of many toxic gases. Most sensors are gas specific and have usable resolutions under one part per million (ppm) of gas concentration.

The circuit shown in Figure 1 uses the ADA4528-2, dual auto zero amplifier, which has a maximum offset voltage of 2.5 μV at room temperature and an industry leading 5.6 μV/√Hz of voltage noise density. In addition, the AD5270-20 programmable rheostat is used rather than a fixed transimpedance resistor, allowing for rapid prototyping of different gas sensor systems, without changing the bill of materials.

The ADR3412 precision, low noise, micropower reference establishes the 1.2 V common-mode, pseudo ground reference voltage with 0.1% accuracy and 8 ppm/°C drift.

For applications where measuring fractions of ppm gas concentration is important, using the ADA4528-2 and the ADR3412 makes the circuit performance suitable for interfacing with a 16-bit ADC, such as the AD7790


Figure 1. Low Noise Gas Detector Circuit (Simplified Schematic: all Connections and Decoupling not Shown)

Описание схемы

Figure 2 shows a simplified schematic of an electrochemical sensor measurement circuit. Electrochemical sensors work by allowing gas to diffuse into the sensor through a membrane and by interacting with the working electrode (WE). The sensor reference electrode (RE) provides feedback to Amplifier U2-A, which maintains a constant potential with the WE terminal by varying the voltage at the counter electrode (CE). The direction of the current at the WE terminal depends on whether the reaction occurring within the sensor is oxidation or reduction. In the case of a carbon monoxide sensor, oxidation takes place; therefore, the current flows into the working electrode, which requires the counter electrode to be at a negative voltage (typically 300 mV to 400 mV) with respect to the working electrode. The op amp driving the CE terminal should have an output voltage range of approximately ±1 V with respect to VREF to provide sufficient headroom for operation with different types of sensors (Alphasense Application Note AAN-105-03, Designing a Potentiostatic Circuit, Alphasense, Ltd.). 


Figure 2. Simplified Electrochemical Sensor Circuit 
 
The current into the WE terminal is less than 100 nA per ppm of gas concentration; therefore, converting this current into an output voltage requires a transimpedance amplifier with a very low input bias current. The ADA4528-2 op amp has CMOS inputs with a maximum input bias current of 220 pA at room temperature, making it a very good fit for this application.

The ADR3412 establishes the pseudo ground reference for the circuit, which allows for single-supply operation while consuming very little quiescent current (100 μA maximum).

Amplifier U2-A sinks enough current from the CE terminal to maintain a 0 V potential between the WE terminal and the RE terminal on the sensor. The RE terminal is connected to the inverting input of Amplifier U2-A; therefore, no current flows in or out of it. This means that the current comes from the WE terminal and it changes linearly with gas concentration. Transimpedance Amplifier U2-B converts the sensor current into a voltage proportional to the gas concentration.

The sensor selected for this circuit is an Alphasense CO-AX carbon monoxide sensor. Table 1 shows the typical specifications associated with carbon monoxide sensors of this general type.

Warning: carbon monoxide is a toxic gas, and concentrations higher than 250 ppm can be dangerous; therefore, take extreme care when testing this circuit. 

Table 1. Typical Carbon Monoxide Sensor Specifications 

Parameter Value
Sensitivity 55 nA/ppm to 100 nA/ppm (65 nA/ppm typical)
Response Time (t90 from 0 ppm to 400 ppm CO) <30 seconds
Range (ppm) CO, Guaranteed Performance) 0 ppm to 2,000 ppm
Overrange Limit (Specifications Not Guaranteed) 4,000 ppm

The output voltage of the transimpedance amplifier is

CN0357_Image1

where IWE is the current into the WE terminal, and RF is the transimpedance feedback resistor (shown as the AD5270-20 U3-B rheostat in Figure 1).

The maximum response of the CO-AX sensor is 100 nA/ppm, and its maximum input range is 2000 ppm of carbon monoxide. These values result in a maximum output current of 200 μA and a maximum output voltage determined by the transimpedance resistor, as shown in Equation 2.

CN0357_Image2

Applying 1.2 V to VREF of the AD7790 allows a usable range of ±1.2 V at the output of the transimpedance amplifier, U2-B. Selecting a 6.0 kΩ resistor for the transimpedance feedback resistor gives a maximum output voltage of 2.4 V.

Equation 3 shows the circuit output voltage as a function of ppm of carbon monoxide, using the typical response of the sensor of 65 nA/ppm.

CN0357_Image3

The AD5270-20 has a nominal resistance value of 20 kΩ. There are 1024 resistance positions, resulting in resistance step sizes of 19.5 Ω. The 5 ppm/°C resistance temperature coefficient of the AD5270-20 is better than that of most discrete resistors, and its 1 μA of supply current is a very small contributor to the overall power consumption of the system.

Resistor R4 keeps the noise gain at a reasonable level. Selecting the value of this resistor is a compromise between the magnitude of the noise gain and the sensor settling time errors, when exposed to high concentrations of gas. For the example shown in Equation 4, R4 = 33 Ω, which results in a noise gain of 183.

CN0357_Image4

The input noise of the transimpedance amplifier appears at the output, amplified by the noise gain. For this circuit, only low frequency noise is of interest because the frequency of operation of the sensor is very low. The ADA4528-2 has a 0.1 Hz to 10 Hz input voltage noise of 97 nV p-p; therefore, the noise at the output is 18 μV p-p, as shown in Equation 5.

CN0357_Image5

Because this is a very low frequency 1/f noise, the noise is very hard to filter. However, because the sensor response is also very slow, it is possible to use a very low frequency, low-pass filter (R5 and C6) with a cutoff frequency of 0.16 Hz. Even with such a low frequency filter, its effect on the sensor response time is negligible, when compared to the 30 second response time of the sensor.

The noise free code resolution of the system is determined from the peak-to-peak output noise. The maximum output of the ADA4528-2 is 2.4 V, so the noise free number of counts is

CN0357_Image6

The noise free code resolution becomes

CN0357_Image7

To take advantage of the entire ADC range available (±1.2 V), the AD8500 micropower, rail-to-rail input/output amplifier is chosen to drive the input of the AD7790. If the entire range is not necessary, the AD8500 can be removed and the internal buffer of the AD7790 can be used in its place.

One important characteristic of electrochemical sensors is their very long time constant. When first powered up, it can take several minutes for the output to settle to its final value. When exposed to a midscale step in concentration of the target gas, the time required for the sensor output to reach 90% of its final value can be in the order of 25 seconds to 40 seconds. If the voltage between the RE terminal and the WE terminal has a sudden change in magnitude, it can take several minutes for the output current of the sensor to settle. This long time constant also applies when cycling power to the sensor. To avoid very long start-up times, P-channel JFET Q1 shorts the RE terminal to the WE terminal when the supply voltage drops below the gate-to-source threshold voltage (~2.0 V) of the JFET. 

Основные варианты исполнения

Electrochemical sensors operate with very small amounts of current, making them well suited for portable, battery-powered instruments. If lower power is required, the ADA4505-2 amplifier has a maximum input bias current of 2 pA and consumes only 10 μA per amplifier. However, the noise of the ADA4505-2 is greater than that of the ADA4528-2.

The ADR291 precision voltage reference consumes only 12 μA and can be substituted for the ADR3412, if lower power is required.

More information can be found in Circuit Note CN-0234.

Оценивание характеристик и тестирование схем

The circuit shown in Figure 1 uses the EVAL-CN0357-PMDZ circuit evaluation board, the PMD-SDP-IB1Z interposer board, and the EVAL-SDP-CB1Z system demonstration platform (SDP-B) controller board. In addition, the EVAL-CN0357-PMDZ comes in a Pmod form factor, making it possible to connect the board to any Pmod controller board, allowing for rapid prototyping.

The CN-0357 Evaluation Software communicates with the SDP board to capture data from the EVAL-CN0357-PMDZ circuit evaluation board.


Equipment Needed

The following equipment is needed for evaluating the CN-0357 circuit: 

  • PC with USB port and Windows® XP, or Windows Vista (32-bit), or Windows 7 (32-bit) 
  • EVAL-CN0357-PMDZ evaluation board 
  • PMD-SDP-IB1Z interposer Board 
  • EVAL-SDP-CB1Z controller board 
  • CN-0357 Evaluation Software 
  • Calibration gas (less than 250 ppm) 
  • EVAL-CFTL-6V-PWRZ or equivalent 6 VDC power supply 


Getting Started

Load the evaluation software by placing the CN-0357 Evaluation Software CD into the CD drive of the PC. Using My Computer, locate the drive that contains the evaluation software CD and run the setup.exe. Follow the on screen prompts for installing and using the evaluation software.



Functional Block Diagram

A functional block diagram of the test setup is shown in Figure 3. There is a complete schematic of the evaluation board contained in the CN-0357 Design Support Package, including printouts of the gerber files, as well as a bill of materials. 

Figure 3.

Figure 3. Test Setup Functional Block Diagram 
 

Setup

Connect the electrochemical sensor to the socket on the EVAL-CN0357-PMDZ circuit evaluation board.

Connect the EVAL-CN0357-PMDZ to the interposer board and ensure that the jumper on the interposer board selects +3.3 V as the configuration. Next, connect the SDP-B board to the interposer board and apply power to the interposer board via the DC barrel jack.

Connect the USB cable supplied with the SDP-B board to the USB port on the PC and to the SDP-B board.

The software can communicate with the SDP board if the Analog Devices System Development Platform driver appears in the Device Manager. When USB communications are established, the SDP board can now send, receive, and capture serial data from the EVAL-CN0357-PMDZ circuit evaluation board.


Test

Navigate to the installation location of the CN-0357 Evaluation Software and open the CN0357.exe file. (The file should be located in a folder named Analog Devices in the start menu of the operating system.)

When the application opens, the software automatically connects to the SDP-B board. If multiple SDP-B controller boards are connected, the selected board will have a light emitting diode (LED) blinking.

The CN-0357 Evaluation Software User Guide contains information and details regarding how to use the evaluation software for data capture.

The input signal for this board is gas concentration; therefore, a calibration gas source is required. When testing with carbon monoxide, consider that 250 ppm is the maximum short term exposure limit.

The software is designed to be used with any electrochemical sensor, so it is important to input the correct specifications for the chosen sensor. 

The maximum sensor sensitivity and sensor range are needed to calculate and set the resistance of the AD5270-20 digital rheostat. This value is a signed value. Positive values are used to describe sensors than sink current, whereas negative values are used to describe sensors that source current.

The typical sensor sensitivity is used to calculate the system conversion coefficient of ppm/mV.

Pressing the Run button begins acquisition of concentration data at 1 second intervals.

Figure 4 shows the circuit response after rapidly removing the sensor from the 175 ppm CO atmosphere and is a better representation of circuit performance.

A photo of the EVAL-CN0357-PMDZ board is shown in Figure 5. 

Figure 4.

Figure 4. Response to a 175 ppm to 0 ppm Step of Carbon Monoxide 
 


Figure 5.

Образцы

Образцы

Продукт

Описание

Доступный продукт
Модели для образца

AD5270 1024-Position, 1% Resistor Tolerance Error, SPI Interface and 50-TP Memory Digital Rheostat

AD5270BCPZ-100-RL7

AD5270BCPZ-20-RL7

AD5270BRMZ-100

AD5270BRMZ-20

AD5270BRMZ-50

AD7790 Одноканальный 16-разрядный сигма-дельта АЦП с крайне низким энергопотреблением

AD7790BRMZ

AD8500 Micropower Precision CMOS Operational Amplifier

AD8500AKSZ-REEL7

ADA4528-2 Precision, Ultralow Noise, RRIO, Zero-Drift Dual Op Amp

ADA4528-2ACPZ-R7

ADA4528-2ARMZ

ADA4528-2TCPZ-EP

Функционирование раздела Покупка возможно только в полной версии сайта
Оценочные платы Цена указана за одну единицу.
Назад
Проверить наличие
Цены указаны за одну штуку, в долларах США, на условиях ФОБ. Являются рекомендованными розничными ценами в США, приведены только для примерного расчета и могут меняться. Международные цены могут отличаться на величину местных пошлин, налогов, сборов и курсов валют.