Thermistor

Thermistors are resistors made from metal oxides, whose resistance changes with temperature. Thermistors are the cheapest temperature sensor you can buy: they are common in consumer-grade applications. Thermistors are highly nonlinear. They are typically available from -40° to 150°C, with best accuracy between 0° to 100°C, although some specialized versions have wider temperature ranges.

Using Custom Thermistors with the Temp-to-Bits Family

Using Custom Thermistors with the Temp-to-Bits Family

This article focuses on custom thermistors and two ways of configuring the converter.

Read Custom Thermistors Article

This Should Work: Thermistor Senses Liquid Levels

This Should Work: Thermistor Senses Liquid Levels

In precision temperature measurement applications using thermistors, RTDs, or other resistive temperature sensors, care must be taken to avoid errors due to self-heating of the sensor by the excitation current.

Learn More

Сигнальные цепочки

(1)

Нажмите на компонент в таблице ниже

Reference Designs

Featured Products