What’s the big deal about ABSOLUTE MAXIMUM RATINGS?

Вопрос:

“Is it alright to exceed just one of the parameters in the ABSOLUTE MAXIMUM RATINGS table, by just a little bit?”

RAQ:  Issue 50

Ответ:

While the answer may seem obvious to many, it does bear some discussion…oh, by the way, the answer is NO!

The majority of information contained within the pages of most datasheets is "typical" data. The performance shown in the graphs, tables and plots is predictable and easy to replicate in new designs, as long as the recommended operating conditions are adhered to. You’ll also find minimums and maximums. These limits, specified by the manufacturer, are guaranteed by design or through exhaustive testing and yield analysis. The datasheet also has a section titled ABSOLUTE MAXIMUM RATINGS (ABS). This section deals with the ABSOLUTE MAXIMUM RATINGS a device can tolerate, but NOT operate at. Like fire, its best to keep your distance from the ABS limits; if you don’t, you could get burned!

I'm not typing ABSOLUTE MAXIMUM RATINGS in capital letters here for dramatic effect (well, maybe a little bit), but this is actually how it appears in the datasheet. The ABSOLUTE MAXIMUM RATINGS table is spelled with all capital letters because it’s extremely important. The following statement spells out the implications of ABSOLUTE MAXIMUM RATINGS. It can be found directly beneath the ABS table in our datasheets.

"Stresses above those listed under Absolute Maximum Ratings may cause permanent damage to the device. This is a stress rating only; functional operation of the device at these or any other conditions above those indicated in the operational section of this specification is not implied. Exposure to absolute maximum rating conditions for extended periods may affect device reliability."

I think the statement is pretty clear, but I'll restate it just to make sure. The device is NOT designed to work at the values contained in the ABSOLUTE MAXIMUM RATINGS table. If you operate at or above the ABSOLUTE MAXIMUM RATINGS, there's a very, very good chance you will permanently damage the device!

Friends, take my advice and steer well clear of danger and peril by avoiding close contact with ABSOLUTE MAXIMUM RATINGS when designing any circuit or system. A good general engineering practice is to build margin into your designs. Resist the temptation to operate near the very edge of a device's ABS ratings; it's never a good idea and usually leads to problems down the road, especially when it comes to reliability.


Design Tools:

Diff Amp Calculator

Об авторах

John Ardizzoni

John Ardizzoni

John started at Analog Devices in 2002, as an Application Engineer in the High Speed Amplifier group. Prior to joining Analog Devices John worked for IBM, in RFIC applications and at M/A-COM for 20 years. John is also co-author of Analog Devices Rarely Asked Questions (RAQ's) column. John has over 30 years experience in the electronics industry, and has authored numerous articles and design ideas.