What’s the (Converter) Frequency Kenneth?

Вопрос:

How Do I Design a Converter Front-end without Compromising the Performance?

RAQ:  Issue 49

Ответ:

Designers that employ a converter for high-frequency sampling have to face many challenges. Designing a front-end isn't simple, but the following comments can guide the designer to a solution.

Baseband applications require bandwidth from dc or the low MHz to the Nyquist frequency of the converter. In terms of relative bandwidth, this implies about 100 MHz or less. These designs can employ either an amplifier or a transformer (balun).

Narrowband applications (narrow being relative to the ADC's full Nyquist bandwidth) usually operate at high intermediate frequencies (IF). They typically use only 5 to 20 MHz of bandwidth in the 2nd or 3rd Nyquist zone, with a center frequency ≥190 MHz. The design only needs a portion of the Nyquist bandwidth, but the unused bandwidth is often needed to implement an anti aliasing filter. A transformer or balun is typically used for these applications, but an amplifier can be used if its performance is adequate at these frequencies.

Wideband designs need it all, with the user taking as much as the converter will supply. These designs have the widest bandwidth, making the frontend design the most challenging of the three types. These applications require bandwidth from dc or low MHz to several GHz. Currently, these designs typically employ a wideband balun, but amplifiers are catching up in bandwidth and performance.

After choosing the converter, choose the front-end amplifier (active) or transformer (passive). The tradeoffs between the two are many and depend on the application, but can be distilled to a few points. Amplifiers add noise, require a power supply, and burn power, but they are not gain bandwidth dependent like a transformer. Also, they have better gain flatness within the pass band region. Transformers are passive, so they don't add noise or burn power, but their asymmetrical behavior can cause spurious issues. Transformers are not ideal devices; if not used properly their parasitics can undermine any design, particularly at higher frequencies (>100 MHz).

Hopefully, this advice will keep the design on track. For additional information, please refer to the references or send me an email.

Об авторах

Rob Reeder

Rob Reeder

Rob Reeder was a senior system application engineer with Analog Devices Inc. in the High Speed Converter and RF Applications Group in Greensboro, NC. He has published numerous papers on converter interfaces, converter testing, and analog signal chain design for a variety of applications. Formerly, Rob was an applications engineer for the Aerospace and Defense Group for five years focusing on a variety of radar, EW, and instrumentation applications, and he was part of the high speed converter product line for nine years. His prior experience also includes test development and analog design engineer for the Multichip Products Group at ADI, designing analog signal chain modules for space, military, and high reliability applications for five years. Rob received his M.S.E.E. and B.S.E.E. degrees from Northern Illinois University in DeKalb, Ill., in 1998 and 1996, respectively.