0 to 88.5 dB in 1.5-dB Steps

AD7110 Digitally Controlled CMOS Attenuator; Has Low: Noise, Distortion, Power-Consumption, and Cost

The AD7110 is basically a 2-quadrant multiplying CMOS d/a converter. It has an internal digital decoder, which produces an antilogarithmic transfer function between the binary value of the 6-bit digital input and the analog output current. Read full article



Об авторах

Generic_Author_image

Steve Stephenson