/***************************************************************************//** * @file adt7420.c * @brief Implementation of ADT7420 Driver. * @author DBogdan (dragos.bogdan@analog.com) ******************************************************************************** * Copyright 2012(c) Analog Devices, Inc. * * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * - Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * - Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in * the documentation and/or other materials provided with the * distribution. * - Neither the name of Analog Devices, Inc. nor the names of its * contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * - The use of this software may or may not infringe the patent rights * of one or more patent holders. This license does not release you * from the requirement that you obtain separate licenses from these * patent holders to use this software. * - Use of the software either in source or binary form, must be run * on or directly connected to an Analog Devices Inc. component. * * THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, * MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. * IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. *******************************************************************************/ /******************************************************************************/ /***************************** Include Files **********************************/ /******************************************************************************/ #include <stdint.h> #include <stdlib.h> #include "platform_drivers.h" #include "adt7420.h" /***************************************************************************//** * @brief Reads the value of a register. * * @param dev - The device structure. * @param register_address - Address of the register. * * @return register_value - Value of the register. *******************************************************************************/ uint8_t adt7420_get_register_value(struct adt7420_dev *dev, uint8_t register_address) { uint8_t register_value = 0; i2c_write(dev->i2c_desc, ®ister_address, 1, 0); i2c_read(dev->i2c_desc, ®ister_value, 1, 1); return register_value; } /***************************************************************************//** * @brief Sets the value of a register. * * @param dev - The device structure. * @param register_address - Address of the register. * @param register_value - Value of the register. * * @return None. *******************************************************************************/ void adt7420_set_register_value(struct adt7420_dev *dev, uint8_t register_address, uint8_t register_value) { uint8_t data_buffer[2] = {0, 0}; data_buffer[0] = register_address; data_buffer[1] = register_value; i2c_write(dev->i2c_desc, data_buffer, 2, 1); } /***************************************************************************//** * @brief Initializes the communication peripheral and checks if the device is * present. * * @param device - The device structure. * @param init_param - The structure that contains the device initial * parameters. * * @return status - The result of the initialization procedure. * Example: -1 - I2C peripheral was not initialized or the * device is not present. * 0 - I2C peripheral was initialized and the * device is present. *******************************************************************************/ int32_t adt7420_init(struct adt7420_dev **device, struct adt7420_init_param init_param) { struct adt7420_dev *dev; int32_t status; uint8_t test = 0; dev = (struct adt7420_dev *)malloc(sizeof(*dev)); if (!dev) return -1; /* I2C */ status = i2c_init(&dev->i2c_desc, init_param.i2c_init); /* Device Settings */ dev->resolution_setting = init_param.resolution_setting; test = adt7420_get_register_value(dev, ADT7420_REG_ID); if(test != ADT7420_DEFAULT_ID) status = -1; *device = dev; return status; } /***************************************************************************//** * @brief Free the resources allocated by adt7420_init(). * * @param dev - The device structure. * * @return ret - The result of the remove procedure. *******************************************************************************/ int32_t adt7420_remove(struct adt7420_dev *dev) { int32_t ret; ret = i2c_remove(dev->i2c_desc); free(dev); return ret; } /***************************************************************************//** * @brief Resets the ADT7420. * The ADT7420 does not respond to I2C bus commands while the default * values upload (approximately 200 us). * * @param dev - The device structure. * * @return None. *******************************************************************************/ void adt7420_reset(struct adt7420_dev *dev) { uint8_t register_address = ADT7420_REG_RESET; i2c_write(dev->i2c_desc, ®ister_address, 1, 1); dev->resolution_setting = 0; } /***************************************************************************//** * @brief Sets the operational mode for ADT7420. * * @param dev - The device structure. * @param mode - Operation mode. * Example: ADT7420_OP_MODE_CONT_CONV - continuous conversion; * ADT7420_OP_MODE_ONE_SHOT - one shot; * ADT7420_OP_MODE_1_SPS - 1 SPS mode; * ADT7420_OP_MODE_SHUTDOWN - shutdown. * * @return None. *******************************************************************************/ void adt7420_set_operation_mode(struct adt7420_dev *dev, uint8_t mode) { uint8_t register_value = 0; register_value = adt7420_get_register_value(dev, ADT7420_REG_CONFIG); register_value &= ~ADT7420_CONFIG_OP_MODE(ADT7420_OP_MODE_SHUTDOWN); register_value |= ADT7420_CONFIG_OP_MODE(mode); adt7420_set_register_value(dev, ADT7420_REG_CONFIG, register_value); } /***************************************************************************//** * @brief Sets the resolution for ADT7420. * * @param dev - The device structure. * @param resolution - Resolution. * Example: 0 - 13-bit resolution; * 1 - 16-bit resolution. * * @return None. *******************************************************************************/ void adt7420_set_resolution(struct adt7420_dev *dev, uint8_t resolution) { uint8_t register_value = 0; register_value = adt7420_get_register_value(dev, ADT7420_REG_CONFIG); register_value &= ~ADT7420_CONFIG_RESOLUTION; register_value |= (resolution * ADT7420_CONFIG_RESOLUTION); adt7420_set_register_value(dev, ADT7420_REG_CONFIG, register_value); dev->resolution_setting = resolution; } /***************************************************************************//** * @brief Reads the temperature data and converts it to Celsius degrees. * * @param dev - The device structure. * * @return temperature - Temperature in degrees Celsius. *******************************************************************************/ float adt7420_get_temperature(struct adt7420_dev *dev) { uint8_t msb_temp = 0; uint8_t lsb_temp = 0; uint16_t temp = 0; float temp_c = 0; msb_temp = adt7420_get_register_value(dev, ADT7420_REG_TEMP_MSB); lsb_temp = adt7420_get_register_value(dev, ADT7420_REG_TEMP_LSB); temp = ((uint16_t)msb_temp << 8) + lsb_temp; if(dev->resolution_setting) { if(temp & 0x8000) /*! Negative temperature */ temp_c = (float)((int32_t)temp - 65536) / 128; else /*! Positive temperature */ temp_c = (float)temp / 128; } else { temp >>= 3; if(temp & 0x1000) /*! Negative temperature */ temp_c = (float)((int32_t)temp - 8192) / 16; else /*! Positive temperature */ temp_c = (float)temp / 16; } return temp_c; }