![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
Variables | |
| char | demo_name [] = "DC934" |
| Demo Board Name stored in QuikEval EEPROM. More... | |
| const uint8_t | address_map [3] = {LTC2607_DAC_A, LTC2607_DAC_B, LTC2607_ALL_DACS} |
| Look-up table for DAC_A, DAC_B, or both command byte option. More... | |
| static int8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static uint32_t | startMinutes = 10*60 + 24 |
| static float | MY_LSB = 7.65841584E-5 |
| static float | MY_OFF = 0.0012425743 |
|
static |
Definition at line 90 of file vmClock.ino.
|
static |
Initialize Linduino.
Definition at line 76 of file vmClock.ino.
| const uint8_t address_map[3] = {LTC2607_DAC_A, LTC2607_DAC_B, LTC2607_ALL_DACS} |
Look-up table for DAC_A, DAC_B, or both command byte option.
Definition at line 66 of file vmClock.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 68 of file vmClock.ino.
| char demo_name[] = "DC934" |
Demo Board Name stored in QuikEval EEPROM.
Definition at line 64 of file vmClock.ino.
|
static |
Definition at line 72 of file vmClock.ino.
|
static |
Definition at line 73 of file vmClock.ino.
|
static |
Definition at line 70 of file vmClock.ino.