![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1962C Demonstration Board LTC3880, LTC2974, LTC2977: Power Management Solution for Application Processors. More...
Linear Technology DC1962C Demonstration Board LTC3880, LTC2974, LTC2977: Power Management Solution for Application Processors.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator.
http://www.linear.com/product/LTC3880
http://www.linear.com/product/LTC2974
http://www.linear.com/product/LTC2977
http://www.linear.com/demo/DC1962C
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file ultra_fix.ino.
Go to the source code of this file.
Functions | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Initialize Linduino. More... | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_warning_prompt () |
| Prints a warning if the demo board is not detected. More... | |
Macros | |
| #define | LTC3880_I2C_ADDRESS 0x30 |
| #define | LTC2974_I2C_ADDRESS 0x32 |
| #define | LTC2977_I2C_ADDRESS 0x33 |
Variables | |
| static uint8_t | ltc3880_i2c_address |
| static uint8_t | ltc2974_i2c_address |
| static uint8_t | ltc2977_i2c_address |
| static uint8_t | ltc_i2c_addresses [3] |
| static LT_SMBus * | smbus = new LT_SMBusNoPec() |
| static LT_PMBus * | pmbus = new LT_PMBus(smbus) |
|
static |
|
static |
|
static |
Prints the title block when program first starts.
Definition at line 202 of file ultra_fix.ino.
|
static |
Prints a warning if the demo board is not detected.
Definition at line 232 of file ultra_fix.ino.
|
static |
| #define LTC2974_I2C_ADDRESS 0x32 |
Definition at line 70 of file ultra_fix.ino.
| #define LTC2977_I2C_ADDRESS 0x33 |
Definition at line 71 of file ultra_fix.ino.
| #define LTC3880_I2C_ADDRESS 0x30 |
Definition at line 69 of file ultra_fix.ino.
|
static |
Definition at line 75 of file ultra_fix.ino.
|
static |
Definition at line 76 of file ultra_fix.ino.
|
static |
Definition at line 74 of file ultra_fix.ino.
|
static |
Definition at line 77 of file ultra_fix.ino.
Definition at line 79 of file ultra_fix.ino.
|
static |
Definition at line 78 of file ultra_fix.ino.